Offshore Wind: Nexans Advances Dieppe–Le Tréport Cable Connection
Interconnection
31 July 2025
3 min
A large ship with yellow cranes and orange buoys in calm waters near the shore.

Nexans has completed a key phase in the grid connection of the Dieppe–Le Tréport offshore wind farm for client RTE (Réseau de Transport d’Électricité). This milestone brings France one step closer to delivering a new large-scale renewable energy from offshore to shore.

A High-Precision Offshore Operation

Awarded in March 2022, the contract covers the full turnkey delivery of export cables—offshore and onshore—for one of France’s largest offshore wind projects. Nexans is responsible for the design, engineering, manufacturing, installation, and protection of the 225 kV power cables, as well as long-term inspection, maintenance, and repair (IMR) services.

The wind farm, located in the English Channel, will generate up to 496 MW of renewable electricity—enough to supply approximately 850,000 people. It will play a key role in France’s broader goals for energy transition and independence.

The recent installation campaign, completed this spring, involved more than 100 personnel and 15 different vessels throughout the various phases of the offshore operation. The work was led by Nexans’ cable-laying vessel CS Skagerrak and required tight coordination between offshore and onshore teams.

Key steps in the operation included:

  • Preparation of the cable route and subsea nearshore trenches
  • Floating of the export cable into position using temporary cable floats, guided towards shore by several powerful work boats maneuvering the cable in strong tidal currents
  • Pulling the cable ashore through a pre-installed duct to the transition joint bay
  • Removing the floats while ensuring position alignment with a pre-dug subsea trench
  • Laying the cable into the pre-defined route, avoiding subsea obstacles such as large sand dunes and potential unexploded ordinances from WW2
  • Backfilling of nearshore trenches and burial of the offshore cable into the seabed by means of jet trenching and mechanical trenching machines

Delivering Value – Technically and Locally

The grid connection consists of two 23-kilometre subsea cables and a 3-kilometre long onshore section. Nexans also provides future value through its IMR services, ensuring the long-term reliability and performance of the infrastructure.

The last outstanding phase of the project, planned for August this year, is the final pull-in and connection of the export cables to the offshore substation, followed by the commissioning, completing the export cable link between the offshore wind farm and the French electric grid.

Enabling Offshore Wind at Scale

As Europe accelerates its energy transition, large-scale offshore wind projects like Dieppe–Le Tréport are becoming essential building blocks. Nexans is proud to contribute to this transformation by delivering resilient, high-voltage cable systems that help electrify the future—safely, reliably, and sustainably.

Construction site with excavators and workers near chalk cliffs
Construction site with machinery and workers laying a large pipe, surrounded by safety cones.
Construction site with workers handling machinery and materials.
Civil engineering site with workers overseeing equipment and materials in a trench.
Marine operation with vessels and a large ship in the sea, featuring orange barriers.
View of fishing boats in the water with a distant offshore platform and floating markers
Crew members working on a floating barrier in calm waters with boats nearby and cliffs in the background.
View of a large ship with orange booms and smaller boats in a calm sea
A vibrant seascape showing boats and a large ship involved in marine operations.
Two small boats navigating a clear blue waterway with mooring buoys.
Two boats engaged in marine operations, with orange buoyancy aids visible on the water.
Aerial view of fishing boats connected to an offshore platform, with calm turquoise waters.
Aerial view of several boats on calm water with floating buoys.

Latest news

Electrician cutting a cable

CSR

15 October 2026

Nexans and Vesto partner to scale electrical cable reuse

Nexans is expanding CableLoop, its electrical cable collection and recycling service, through a partnership with French reuse specialist Vesto. Construction professionals in France gain access to recycling, small-volume collection of any brand and requalification of cables for reuse.

Nexans Charleston team with Fabriq tool

Innovation

16 September 2026

Industry 4.0 transformation across global manufacturing network

How Nexans transformed plant performance management globally by digitalizing operational discipline across 40 manufacturing sites. Digital transformation case study.

gsi-tensile-bending-test-loop-5-thumbnail

Project

27 August 2026

Nexans sets new world record for deepwater HVDC cable technology

Nexans qualifies the only 525 kV HVDC cable system rated for 3,000-meter installation, presented at CIGRE 2026 as part of the Great Sea Interconnector.