Electrifying the buildings
that can’t afford to fail

Hospitals, data centers, airports and mission-critical facilities demand the highest standards of safety, reliability and sustainability. Their electrical load profile is changing at unprecedented speed: distributed solar, storage, EV charging, higher rack densities and digitalized building systems are turning the last kilometer of the grid into a mission-critical asset.

Nexans engineers the cabling solutions that keep them running.

banner-buildings

30%

of global final energy consumed in buildings sector (IEA 2025)

70%

of building devices run natively on direct current

+50%

electricity demand from buildings by 2050 (IEA)

A sector at the intersection of every major megatrend

Critical buildings, hospitals, airports, data centers, transport hubs, campuses and government facilities, represent the connective tissue of the global economy. They operate 24/7, tolerating zero downtime, yet face mounting pressure to decarbonize, electrify, and integrate renewable energy at speed.

Buildings already account for ~30% of global final energy consumption and more than half of all electricity demand worldwide (IEA 2025). With global floor area set to double by 2060, and the proliferation of EV charging, battery storage, solar and IoT devices, the density of electrical infrastructure inside buildings is accelerating sharply.

The DC microgrid market alone is projected to surpass $51 billion by 2035 at a 19.5% CAGR, driven by the native compatibility of PV, EVs and batteries with direct current. Meanwhile, fire safety regulations are tightening worldwide, and ESG mandates are elevating expectations for every material in the building’s envelope, including cables.

This convergence creates a once-in-a-generation opportunity for solutions providers who can cover the full project lifecycle: design, specification, installation, commissioning, and circular end-of-life management.

$241b

global data center construction market size in 2024 (Grand View Research 2025)

19%

CAGR of global DC microgrid market 2025-2034 (GM Insights / Research Nester 2025)

$12.6b

structured cabling market in 2025, rising to $20.7b by 2035 (Global Growth Insights 2026)

What critical buildings must overcome
Every critical facility faces a cluster of interdependent pressures that push conventional cabling solutions to their limits.

Zero-downtime power continuity

Hospitals, airports, financial infrastructure and data centers cannot tolerate interruption. Cabling systems must guarantee circuit integrity even under catastrophic fire conditions, but they must also support commissioning schedules, grid-connection constraints and high-density power demand. In data centers, even a delayed cable delivery can jeopardize the commissioning schedule; critical electrical equipment lead times now reach 18 to 36 months in some markets.

Net zero & decarbonization mandates

Buildings must reduce COโ‚‚ emissions by more than 95% by 2050 under IEA Net Zero scenarios. Every component, from the cable insulation to the installation process, must now carry verifiable environmental credentials and support a circular economy model. Specifiers are moving from generic sustainability claims to product-level evidence: PEP Ecopassport declarations, life-cycle assessment data, recycled-metal content and supplier decarbonization.

Fire safety compliance

A fire breaks out in a European building every 30 seconds, with 25%+ caused by electrical faults (FEEDS). Tightening regulations, including the French 2025 requirements for tertiary and high-rise buildings, and Construction Products Regulations (CPR) in Europe, require cables that actively limit flame spread, smoke, and toxic emissions in public spaces. Nexans Protect goes beyond baseline compliance with low-smoke, halogen-free cables manufactured primarily in France and performance that reduces fire spread by a factor of 5 to 10 compared with conventional U1000 R2V cables.

Integrating renewable energy & storage

Over 70% of building devices natively operate on DC power. Solar PV, BESS and EV chargers, all DC, are now standard on critical building projects. Traditional AC-only infrastructure creates conversion losses, cost and complexity that DC microgrids directly eliminate.

Installation speed & safety

Labor shortages, compressed construction timelines and hyperscale commissioning windows make faster, safer cable laying is a competitive differentiator. On complex tertiary and data center projects, cable drum handling can create musculoskeletal risk, on-site accidents, and planning delays.

Standardization & interoperability

DC microgrid ecosystems are still maturing. Without established cross-manufacturer standards, installers face compatibility risks, warranty voids and specification uncertainty. Active participation in standardization bodies is now a prerequisite for credible DC solution providers.

A complete solution suite for critical buildings

Nexans brings more than 120 years of electrification expertise to critical building projects. Our portfolio spans every layer of the electrical system, from the primary power feed to the last-meter DC connection, backed by industry-leading R&D, global manufacturing, and a growing suite of beyond-cable services.

We work alongside owners, engineers, architects, contractors and system integrators from specification through commissioning, and support the circular end-of-life of every cable we supply.

Nexans fire safety cables

Nexans Fire Safety Range

Low fire-hazard and fire-resistant cables engineered to limit flame spread, minimize toxic smoke, and keep critical circuits operational throughout an emergency. Compliant with CPR, IEC 60331, and the most stringent international standards.

low carbon program

Low-Carbon Cable Program

Cables manufactured with a reduced carbon footprint through use of recycled metals, renewable energy in production, and eco-designed materials. Every product comes with a PEP Ecopassportยฎ, its verified environmental identity card.

Suez

CableLoop Recycling Service

Close the loop on electrical infrastructure. CableLoop collects and recycles end-of-life copper and aluminum cables from job sites and facilities, recovering 30,000+ tonnes annually and feeding recovered metals back into Nexans’ low-carbon cable production.

Nexans MOBIWAYโ„ข Range

MOBIWAYโ„ข Range

Purpose-engineered cable handling and unwinding systems that help installers save up to 30% of installation time on average, reduce physical strain and improve jobsite safety. Designed around real construction-site conditions, the MOBIWAYโ„ข range supports faster, safer cable installation across residential, commercial, tertiary and large critical-building projects.

Direct current for buildings: the next frontier

DC microgrids eliminate the conversion losses of AC-to-DC conversion, delivering 20โ€“30% less energy loss and up to 10โ€“20% lower COโ‚‚ footprint compared to conventional architectures. Nexans is developing a dedicated portfolio of Low Voltage DC (LVDC) cables, designed to comply with CurrentOS specification rules and compatible with all safety zones in a DC building, from the PV rooftop to the server room. As one of 63+ partners co-developing global DC standards, Nexans is at the forefront of a market set to reach $8.7 billion in 2025 and $51+ billion by 2035.

Our direct current solutions

โ‰ˆ 20โ€“30%

less energy loss vs AC.

 

โ‰ˆ 30%

more power for same copper.

 

โ‰ˆ 70%

of devices are natively DC.

Tomorrow’s buildings will be smart, connected and sustainable with a DC power supply. Reflecting its active commitment to this transformation, Nexans is manufacturing specific cable systems compatible with these new infrastructures.

Lina Ruiz
Lina Ruiz

Head of the LVDC and MVDC technical platforms and new architectures at the Research and Regions Tech Centre, Nexans

Shaping the future of building electrification

Nexans contributes to the standards, conversations and technical ecosystems that will define critical building infrastructure for decades.

Perspectives
  • Article

    Serie : Innovations for Buildings’ Revolution

    Sustainable buildings

    Sustainable buildings for a brighter future

    Electrification of tomorrow

    12/10/2023

  • Article

    Serie : Innovations for Buildings’ Revolution

    Direct current powered buildings

    Unleashing the power of DC buildings

    Electrification of tomorrow

    25/07/2023

  • Article

    Serie : Innovations for Buildings’ Revolution

    Digitalization in building construction

    Digital solutions for building construction: A path to progress

    Electrification of tomorrow

    18/07/2023

  • Article

    Serie : Innovations for Buildings’ Revolution

    Fire safety and buildings

    Fire safety in buildings: Holistic certification for enhanced protection

    Electrification of tomorrow

    04/07/2023

  • Article

    Serie : Innovations for Buildings’ Revolution

    3D printing & modular wiring in buildings

    Future of building construction: 3D printing & modular technologies

    Electrification of tomorrow

    27/06/2023

  • Article

    Serie : 10 Technologies to Electrify the Future

    Direct current renaissance

    Direct current renaissance: Powering the future

    Electrification of tomorrow

    14/06/2022

  • Built for net zero โ€” from design to end of life
    Nexans’ commitment to sustainability goes beyond product performance. We are building circular, low-carbon practices into every stage of the cable lifecycle.

    Low-carbon manufacturing

    Our Low-Carbon Program targets verified reduction of Scope 1, 2 and 3 emissions across the cable manufacturing process, with certified environmental declarations on every product via PEP Ecopassportยฎ.

    CableLoop: Circular Economy

    30,000 tonnes of cables processed annually. 18,000 tonnes of copper and aluminum granules recovered. Target: 25% recycled copper in all Nexans cables by 2028. End-of-life is not the end of the story.

    DC Efficiency Gains

    By enabling DC microgrids with purpose-designed LVDC cables, Nexans helps buildings achieve 20โ€“30% lower energy losses and a 10โ€“20% reduction in COโ‚‚ footprint compared to traditional AC distribution architectures.

    Questions about our critical buildings solutions

    Ready to power your critical building project?

    Our team of experts is ready to support you from specification through commissioning, with solutions that deliver safety, sustainability and performance from day one.