Jansz-Io: Nexans Aurora lays deep-water dynamic cable off Australia
Project
20 November 2026
2 min
Nexans Aurora for Jansz Io

Nexans cable-laying vessel Aurora has finished laying and trenching the high-voltage dynamic cable for the Jansz-Io Compression (J-IC) project, operated by Chevron Australia. The vessel left Australia on 23 October 2026, after installing 26 buoyancy modules and trenching 30 km of cable.

Key facts

  • Project: Jansz-Io Compression (J-IC), Gorgon Project, Western Australia
  • Client: Chevron Australia
  • Nexans scope: turnkey design, manufacturing and installation of a 145 kV HVAC dynamic cable
  • Route: about 135 km, Barrow Island to a floating Field Control Station, in one continuous length
  • Status: offshore installation and trenching completed in October 2026
  • Next step: final soak test by the client, February 2027

Powering subsea gas compression from shore

J-IC uses subsea compression to sustain gas supply to the Gorgon LNG and domestic gas plants on Barrow Island. The 145 kV cable runs from the island to a floating Field Control Station, which powers and controls the compressors on the seabed.

 

Eight operations at sea

  • Working with teams onshore, the project team and Aurora’s crew completed:
  • Overboarding and pull-in of the cable head to the Field Control Station
  • Installation of 26 buoyancy modules, using a horizontal method developed by Nexans
  • Laying of the cable in its dynamic configuration
  • Installation of about 200 meters of VIV (vortex-induced vibration) strakes in the Scarp section
  • Cable lay up the Scarp, a steep slope on the seabed route
  • Float-out and pull-in of the second cable end at Barrow Island
  • As-laid survey
  • Trenching of 30 km of cable

Remaining work

Before handover, three steps remain:

  • Cable jointing at the Field Control Station and on Barrow Island
  • Rock stabilization along the last 28 km of the route
  • Final soak test, planned by the client for February 2027

From Jansz-Io to floating offshore wind

A dynamic cable must carry high voltage while following the motion of a floating structure for decades. The configurations and installation methods used at Jansz-Io apply to other floating assets, including electrified offshore platforms and floating wind farms.

Nexans Aurora for Jansz Io
Nexans Aurora for Jansz Io

FAQ

Our latest news

Nexans Aurora for Jansz Io

Project

20 November 2026

Jansz-Io: Nexans Aurora completes subsea cable installation

CLV Nexans Aurora has left Western Australia after laying and trenching the cable that will power subsea gas compression on Chevron’s Jansz-Io field. Jointing, rock stabilization and a soak test are next.

Electrician cutting a cable

CSR

15 October 2026

Nexans and Vesto partner to scale electrical cable reuse

Nexans is expanding CableLoop, its electrical cable collection and recycling service, through a partnership with French reuse specialist Vesto. Construction professionals in France gain access to recycling, small-volume collection of any brand and requalification of cables for reuse.

Master IRED conference

Career

06 October 2026

IRED electrical networks Masterโ€™s: Nexans, RTE & Lyon 1

Nexans, RTE and Lyon 1 University launch IRED, a unique work-study Masterโ€™s in electrical network engineering, with 40% taught by industry experts.