Offshore Wind: Nexans Advances Dieppe–Le Tréport Cable Connection
Interconnection
31 July 2025
3 min
A large ship with yellow cranes and orange buoys in calm waters near the shore.

Nexans has completed a key phase in the grid connection of the Dieppe–Le Tréport offshore wind farm for client RTE (Réseau de Transport d’Électricité). This milestone brings France one step closer to delivering a new large-scale renewable energy from offshore to shore.

A High-Precision Offshore Operation

Awarded in March 2022, the contract covers the full turnkey delivery of export cables—offshore and onshore—for one of France’s largest offshore wind projects. Nexans is responsible for the design, engineering, manufacturing, installation, and protection of the 225 kV power cables, as well as long-term inspection, maintenance, and repair (IMR) services.

The wind farm, located in the English Channel, will generate up to 496 MW of renewable electricity—enough to supply approximately 850,000 people. It will play a key role in France’s broader goals for energy transition and independence.

The recent installation campaign, completed this spring, involved more than 100 personnel and 15 different vessels throughout the various phases of the offshore operation. The work was led by Nexans’ cable-laying vessel CS Skagerrak and required tight coordination between offshore and onshore teams.

Key steps in the operation included:

  • Preparation of the cable route and subsea nearshore trenches
  • Floating of the export cable into position using temporary cable floats, guided towards shore by several powerful work boats maneuvering the cable in strong tidal currents
  • Pulling the cable ashore through a pre-installed duct to the transition joint bay
  • Removing the floats while ensuring position alignment with a pre-dug subsea trench
  • Laying the cable into the pre-defined route, avoiding subsea obstacles such as large sand dunes and potential unexploded ordinances from WW2
  • Backfilling of nearshore trenches and burial of the offshore cable into the seabed by means of jet trenching and mechanical trenching machines

Delivering Value – Technically and Locally

The grid connection consists of two 23-kilometre subsea cables and a 3-kilometre long onshore section. Nexans also provides future value through its IMR services, ensuring the long-term reliability and performance of the infrastructure.

The last outstanding phase of the project, planned for August this year, is the final pull-in and connection of the export cables to the offshore substation, followed by the commissioning, completing the export cable link between the offshore wind farm and the French electric grid.

Enabling Offshore Wind at Scale

As Europe accelerates its energy transition, large-scale offshore wind projects like Dieppe–Le Tréport are becoming essential building blocks. Nexans is proud to contribute to this transformation by delivering resilient, high-voltage cable systems that help electrify the future—safely, reliably, and sustainably.

Construction site with excavators and workers near chalk cliffs
Construction site with machinery and workers laying a large pipe, surrounded by safety cones.
Construction site with workers handling machinery and materials.
Civil engineering site with workers overseeing equipment and materials in a trench.
Marine operation with vessels and a large ship in the sea, featuring orange barriers.
View of fishing boats in the water with a distant offshore platform and floating markers
Crew members working on a floating barrier in calm waters with boats nearby and cliffs in the background.
View of a large ship with orange booms and smaller boats in a calm sea
A vibrant seascape showing boats and a large ship involved in marine operations.
Two small boats navigating a clear blue waterway with mooring buoys.
Two boats engaged in marine operations, with orange buoyancy aids visible on the water.
Aerial view of fishing boats connected to an offshore platform, with calm turquoise waters.
Aerial view of several boats on calm water with floating buoys.

Latest news

Solar farm in Morocco

Project

16 April 2026

Noor Atlas: key solar project supporting Morocco’s energy transition

Nexans Morocco wins the Noor Atlas solar project, a major milestone for renewable energy in Morocco. A strategic project highlighting the critical role of electrical infrastructure—and strong local industry—in the energy transition.

Nexans Skagerrak cable laying for Fensfjord project

Project

07 April 2026

Nexans completes deep-fjord 420 kV subsea cable project in Norway

A world-first at 530 meters below sea level: discover how Nexans successfully delivered a record-breaking 420 kV subsea cable project in Norway’s challenging fjord environment.

Agathe Pauli

Sponsorship

26 March 2026

“Thanks to Nexans, I can focus on improving, and that changes everything”

Discover how Paralympic swimmer Agathe Pauli’s journey is supported by Nexans as she aims for the podium in future competitions.