WindEnergy Hamburg 2026

22 to 25 September 2026

WindEnergy Hamburg 2026 Nexans powers Europe’s wind grid expansion

Europe’s wind sector is scaling fast, and nowhere is that momentum more visible than at WindEnergy Hamburg, the industry’s flagship gathering. From 22 to 25 September 2026, Nexans returns to its home market to meet the operators, developers and grid planners driving offshore expansion in the North Sea and Baltic, and onshore growth across the continent.

Find the Nexans team at Hall B6, Booth B6.549, where we’ll be presenting the high-voltage cable accessories supporting Europe’s next generation of wind grid connections.

Built for Europe’s grid ambitions: 72.5–145 kV accessories

As European wind capacity climbs toward increasingly ambitious 2030 and 2040 targets, grid connection infrastructure has to keep pace. Nexans’ accessories campaign, “The Power Behind the Performance“, reflects more than 50 years of cable expertise applied to that challenge:

  • 72.5 kV, field-proven, a dependable choice for the existing grid infrastructure already carrying wind power across Germany and neighbouring markets.
  • 145 kV, newly launched, engineered for the larger offshore arrays and higher-capacity onshore projects now moving from planning into construction across Europe.
  • Precision-engineered connections, built to hold up under the demanding transmission requirements of modern wind installations, on land and at sea.

Supporting the energy transition, from coastline to grid

Nexans’ presence at WindEnergy Hamburg reflects a broader commitment to Europe’s energy transition:

  • High-voltage accessories connecting offshore and onshore wind farms to national grids
  • HVDC cable sample demonstrators on display at the booth.

Europe’s shift to renewable, resilient power depends on partnerships across the value chain, from turbine manufacturers to grid operators. Nexans is building the connections that make that shift possible.

Visit us in Hamburg

Heading to WindEnergy Hamburg? Stop by to:

  • See the new 145 kV range alongside our established 72.5 kV accessories
  • Discuss grid connection solutions for your offshore or onshore wind project with our European technical team.

Location: Hamburg Messe und Congress – Hall B6, Booth B6.549
Dates: 22-25 September 2026

Today’s performance. Tomorrow’s power.

Visit us in Hamburg

Get your tickets now