Superconductivity takes center stage at CRU Hanover
Event
02 July 2026
3 min
2026 Stella Nova visit for CRU 2026

Last week, Nexans opened its Stella Nova site in Hanover to delegates attending the CRU Wire & Cable Conference, and took part in the conference itself with a keynote presentation and a panel discussion. Main focus was on superconductivity and especially on: how High-Temperature Superconducting (HTS) cable systems are being deployed today to power data centers, grids and offshore wind projects.

80 delegates toured Nexans Stella Nova site

On June 23, ahead of the conference’s official opening, 80 CRU delegates visited Nexans Stella Nova. The group included industry executives, technical experts and stakeholders from across the cable and energy sectors, and got a first-hand look at the site dedicated to Nexans’ superconducting cable systems, cryogenic transfer line technologies and forming and welding machines.

Nexans also used the visit to unveil its new HV/MV (High Voltage / Medium Voltage) testing laboratory. The lab supports cable and accessory qualification, project-specific configurations, engineering work and R&D. It can test conventional cable systems, including cables, accessories, jumpers and complete configurations, as well as more advanced technologies such as superconducting systems and Superconducting Fault Current Limiter (SFCL) validation. One facility now covers both current qualification needs and future electrification technologies.

Nexans Stella Nova relies on decades of experience and innovation capabilities associated with its industrialization drive to scale our unique solutions. This Excellence Centre is our driving force for a sustainable future, reflecting our commitment to developing and scaling innovations that power a cleaner, smarter, and more electrified world, dedicated to accelerating electrification and the energy transition.

Yann Duclot at Nexans Stella Nova visit
Yann Duclot

Acceleration Units Director, Nexans

The visit marked a second milestone for Nexans, one year after Stella Nova’s opening in June 2025, when Nexans inaugurated the 9,000 m² Hanover site and unveiled a world-first demonstration of superconducting LV AC and LV DC cables for hyperscale data centers. More than 70 engineering, research and manufacturing experts work at the site today.

Nexans Stella Nova visit - group 1

Stella Nova visit, first session

Nexans Stella Nova visit - group 2

Stella Nova visit, second session

Nexans Stella Nova visit - Gabriel Hajiri

Stella Nova visit, superconducting cable presentation by Gabriel Hajiri

Nexans Stella Nova visit - Cord Neemeyer

Stella Nova visit, cryogenic cables presentation by Cord Neemeyer

Nexans Stella Nova visit - cryogenic system

Stella Nova visit, cryogenic system presentation

Nexans Stella Nova visit - Yann Duclot presentation

Stella Nova visit, Yann Duclot presentation

Nexans Stella Nova visit - HV lab

Stella Nova visit, high-voltage lab

Superconductivity on the conference agenda

Superconductivity featured throughout the CRU Wire & Cable Conference program. Yann Duclot, Nexans Acceleration Units Director, spoke in two sessions, a keynote and a panel discussion with other industry players, on how HTS systems are being used today to scale electrification and strengthen critical infrastructure.

CRU 2026 - Yann Duclot conference on data centers

Electrifying data centers

AI, cloud computing and high-performance workloads are pushing data center power requirements to multi-hundred-megawatt and gigawatt scale. Rising power density brings heat, efficiency and sustainability challenges, and operators are having to rethink electrical architectures to move more power over longer distances while limiting energy losses.

In his presentation on data centers and energy infrastructure, Yann Duclot explained why conventional cable systems are struggling to keep up. Distributing power across a large campus takes a huge amount of infrastructure. Civil works and installation drive up cost and delays. Resistive cables generate energy losses and heat. Space constraints limit how far a site can scale. HTS cables address these issues directly. They can carry up to ten times more power than conventional cables in a footprint up to ten times smaller, with zero energy loss and no electromagnetic emissions, which suits the tight, high-density layouts of modern data centers.

Nexans pointed to its industrialized HTS cable systems as evidence the technology is already commercial. The range covers low to high voltage, in both AC and DC, from 480 V to 275 kV and up to 320 kV. The offer includes a turnkey system covering the liquid nitrogen cooling plant, cables and accessories, and it is backed by projects that have already validated performance in real operating conditions.

CRU 2026 - superconductivity panel

Scaling HTS for grid connections

Nexans also joined a panel on “Applications, Scalability and Challenges for HTS Mainstream Grid Connections,” chaired by Simon Price, Director, Energy Transition at CRU. Alongside Yann Duclot, the panel included Tim Heidel of VEIR, Rob O’Connor of SuperNode Ltd, Tommaso Botto of ASG Superconductors S.p.A. and Jay Vitha of MetOx International.

The panel agreed that AI-driven infrastructure growth is creating unprecedented electricity demand, and that superconductivity can help solve grid capacity constraints. The remaining challenge, panelists said, is no longer whether HTS technology works, but how quickly it can be deployed at scale. Standardization and certification were named as key to building market confidence. On the low-voltage side, Nexans is working with UL Solutions (a global independant safety science company) and other industry stakeholders to define certification frameworks and technical standards for complete superconducting cable systems.

Offshore wind: the SupraMarine project

Data centers are not the only application under discussion. The SupraMarine project, a consortium involving Nexans, Air Liquide, ITP, RTE and CentraleSupélec, is looking at how HTS cables could connect remote offshore wind farms to shore.

Consortium members Loïc Quéval, Professor at CentraleSupélec, and Pierre Crespi, Innovation & Foresight Advisor at Air Liquide, presented the project at the conference. They described how superconducting cables could offer a more efficient way to connect remote offshore wind generation, particularly where conventional solutions run into limits on size, cost, supply availability or infrastructure. SupraMarine combines a superconducting cable core, pipe-in-pipe insulation and industrial cryogenic cooling to propose a different approach to offshore power transmission.

What this means for the industry

Between the Stella Nova visit and the conference sessions, the message from Nexans was consistent: superconductivity is no longer a research topic. It is a technology already being deployed to power data centers, support grids and connect offshore wind. As power demand keeps rising, the question is less about whether HTS technology will be adopted, and more about how fast it can scale.

Superconducting cable systems

Learn more about our solutions

Latest news

Electrician cutting a cable

CSR

15 October 2026

Nexans and Vesto partner to scale electrical cable reuse

Nexans is expanding CableLoop, its electrical cable collection and recycling service, through a partnership with French reuse specialist Vesto. Construction professionals in France gain access to recycling, small-volume collection of any brand and requalification of cables for reuse.

06 October 2026

IRED electrical networks Master’s: Nexans, RTE & Lyon 1

Nexans, RTE and Lyon 1 University launch IRED, a unique work-study Master’s in electrical network engineering, with 40% taught by industry experts.

Nexans Charleston team with Fabriq tool

Innovation

16 September 2026

Industry 4.0 transformation across global manufacturing network

How Nexans transformed plant performance management globally by digitalizing operational discipline across 40 manufacturing sites. Digital transformation case study.