Case study

Koh Samui

  • LOCATION
    Thailand
  • MARKET
    Power networks - Subsea

Project description:

  • To supply a subsea cable to establish a new 115 kV power grid between mainland Thailand at Khanom and the island of Koh Samui.

Customer challenges:

  • Due to increasing tourism, the power requirement is likely to increase by 10-15% per annum.
  • Koh Samui lies approximately 15 km from Khanom in the Gulf of Thailand. The power connection should have a capacity of 100 MW, thereby nearly doubling capacity to the island and meeting the increasing need for electricity in the region.

Nexans' solutions:

  • Nexans manufactured  54 km of 115 kV 3-core XLPE cable and associated equipment.
  • The cable consists of 3x 500 mm² copper cores and one 24 fiber element, It was produced in the factory in Halden and completed in November 2012.