Case study

Offshore and onshore export cables for Seagreen, the largest windfarm project in Scotland

  • LOCATION
    Scotland
  • PARTNERSHIP
    SSE Renewables
  • MARKET
    Wind farms-Offshore
1,075 MW

GENERATED OF WIND TURBINES

65 km

OF OFFSHORE CABLES

20 km

OF ONSHORE CABLES

About the project

Phase 1 development, comprising the Seagreen Alpha and Bravo wind farms. It will have combined capacity of 1,075MW. When complete it will form the largest windfarm project in Scotland when they come online in 2024. To promote contract opportunities for local companies, SSE Renewables organises 'Meet the Buyer' events, where they can discuss their service offerings with members of the supply chain.

Nexans' solution

Nexans is SSE's preferred supplier for the design, manufacture and installation of the onshore and offshore export cables. Nexans will supply and install three 65 km offshore export cables and three 20 km onshore export cables.

“ We are delighted to receive this agreement from SSE and we are excited to be helping to bring the biggest windfarm in Scotland to life. ”

Vincent Dessale

SEVP for the Subsea and Land System Business Group