Nexans sets world record and completes high-voltage subsea cable installation on the Tyrrhenian Link
07 January 2026
3 min
Nexans Aurora on the Tyrrhenian Link project
  • Nexans achieves a world-record installation depth of 2,150 meters on the Tyrrhenian Link Project in Italy, set in December 2025.
  • Completion of the second pull-in operation on January 1, 2026 marks the completion of high-voltage subsea cable installation.
  • Achievement highlights Nexansโ€™ leading-edge subsea engineering, manufacturing and installation capabilities.

Nexans has successfully completed the high-voltage subsea cable installation on the Tyrrhenian Link project in Italy, confirming a world-record installation depth of 2,150 meters for a 500 kV high-voltage direct current (HVDC) subsea cable.

The world record was achieved during offshore installation campaign in December 2025, as part of Nexansโ€™ works for Terna, the Italian Transmission System Operator. The Tyrrhenian Link is a strategic 500 kV HVDC interconnection designed to strengthen Italyโ€™s national transmission grid.

The offshore execution milestone was finalized with the successful completion of the second pull-in operation on January 1, 2026, establishing the physical connection between the cable landing points in Terra Mala (Sardinia) and Fiumetorto (Sicily). This operation marks the completion of all high-voltage subsea cable laying activities on the project.

The western section of the Tyrrhenian Link, which falls within Nexansโ€™ scope of work, comprises approximately 480 km of deep-water subsea cable, installed over two offshore campaigns of around 200 km and 280 km respectively. The Tyrrhenian Link as a whole consists of two 500 kV HVDC subsea connections, each approximately 970 km in length, with a total transmission capacity of 1,000 MW.

Setting a world record at 2,150 meters and completing the high-voltage subsea cable installation phase of the Tyrrhenian Link are defining achievements for Nexans. Installing a 500 kV HVDC cable at such depths requires exceptional precision and discipline across engineering, manufacturing, route preparation and vessel operations. These milestones reflect the strength of our technology, the performance of the Nexans Aurora, and the expertise of our teams throughout the project.

Pascal Radue
Pascal Radue

Executive Vice President, PWR-Transmission, Nexans

The Tyrrhenian Link has reached a depth of 2,150 meters, setting a world record for a submarine power cable. This milestone demonstrates Ternaโ€™s ability to manage highly complex technological challenges and deliver infrastructure that strengthens the stability, security and adequacy of Italyโ€™s electricity system.

Giuseppina Di Foggia

Chief Executive Officer and General Manager, Terna

By setting a new world record and completing the high-voltage subsea cable installation, Nexans once again demonstrates its capability to deliver complex, deep-water HVDC projects with technical excellence and operational rigor.

nexans-aurora-tyrrhenian-link-cable-going-into-water-detail
nexans-aurora-tyrrhenian-link-cable-going-into-water
nexans-aurora-tyrrhenian-link-turntable
nexans-aurora-tyrrhenian-link-seabed-wr

All our press releases

Access our press releases