Nexans Electra Takes Shape in Norway
02 July 2025
3 min
Large red ship being assisted by tugboats in a busy port.

Nexans has reached a pivotal moment in the construction of Nexans Electra, its next-generation cable-laying vessel (CLV), as the hull arrives at Ulstein Verft in Norway for the final outfitting phase. More than just a milestone in shipbuilding, this event marks a significant leap in Nexansโ€™ mission to drive the global energy transitionโ€”strengthening the backbone of tomorrowโ€™s electrified world.

As the energy landscape evolves, nations and industries are accelerating investments in offshore wind, interconnectors, and deep-sea electrification projects. Nexans Electra is a strategic response to this surge in demandโ€”an advanced, high-capacity vessel engineered to deliver power where itโ€™s needed most, with greater efficiency, sustainability, and precision than ever before.

Built to meet the challenges of a low-carbon future, Electra will significantly expand Nexansโ€™ turnkey capabilities in subsea cable installationโ€”reinforcing our position as a global leader in offshore power transmission solutions.

Major Construction Milestone Reached

The hull of Nexans Electra – initially constructed at the Crist shipyard in Poland – has now arrived in Ulsteinvik, entering its critical outfitting and completion stage at Ulstein Verft. Scheduled for delivery in 2026, Electra will soon become one of the worldโ€™s most capable CLVs, purpose-built for the complexities of todayโ€™s and tomorrowโ€™s energy infrastructure.

Aerial view of a busy industrial port with ships and cranes, featuring a large red vessel docked.

Next-Level Capability

Once completed, the vessel will boast:

  • A 10,000-tonne split turntable on deck
  • A 3,500-tonne under-deck turntable
  • A 450-tonne fibre optic tank

These features will enable Electra to transport and install large volumes of high-voltage DC and AC subsea cables, as well as perform complex construction and repair tasks in deep water.

Outfitting phase in full motion

Now at Ulstein Verft, the vessel will undergo outfitting, electrical installation, insulation, and piping. The yard will also install key equipment such as the main generator set, power and propulsion systems, deck machinery, winches, and topside installations.

Designed for performance and sustainability

Measuring 155.2 metres in length and 31 metres in beam, Nexans Electra is designed to operate in harsh conditions with excellent station-keeping and maneuverability. The vessel will also be equipped with shore power capabilities, an energy storage system, and will be compatible with biofuelsโ€”significantly reducing its environmental footprint.

Nexans Electra will play a central role in enabling the global energy transition, expanding Nexansโ€™ capacity to deliver turnkey submarine cable projects with speed, precision, and resilience. From deep-sea construction to high-voltage transmission, this vessel will be at the forefront of offshore innovation, empowering customers and communities around the world.

Vue aรฉrienne d'un navire en bรขtiment avec un port et des รฉquipements industriels en arriรจre-plan.
Vue d'un grand navire rouge en mer avec des montagnes ร  l'arriรจre-plan
Vue aรฉrienne d'un port avec des bateaux, des docks et des entrepรดts.
Vue aรฉrienne d'un chantier naval avec deux grands navires et des grues au bord de l'eau.
Grand navire de couleur rouge naviguant dans une mer calme, escortรฉ par de petits remorqueurs
Vue aรฉrienne d'un port avec des grues et un navire en construction au coucher du soleil.
Navire de grande taille en construction dans un chantier naval, avec grue et paysage montagneux en arriรจre-plan.
Navire en construction dans un grand atelier, reflet sur l'eau sombre.
Un grand navire de transport de couleur rouge naviguant dans une baie calme, avec un petit bateau ร  moteur ร  proximitรฉ.
Vue aรฉrienne d'un port avec un grand bateau rouge et des petites รฎles verdoyantes.

Latest news

Electrician cutting a cable

CSR

15 October 2026

Nexans and Vesto partner to scale electrical cable reuse

Nexans is expanding CableLoop, its electrical cable collection and recycling service, through a partnership with French reuse specialist Vesto. Construction professionals in France gain access to recycling, small-volume collection of any brand and requalification of cables for reuse.

06 October 2026

IRED electrical networks Masterโ€™s: Nexans, RTE & Lyon 1

Nexans, RTE and Lyon 1 University launch IRED, a unique work-study Masterโ€™s in electrical network engineering, with 40% taught by industry experts.

Nexans Charleston team with Fabriq tool

Innovation

16 September 2026

Industry 4.0 transformation across global manufacturing network

How Nexans transformed plant performance management globally by digitalizing operational discipline across 40 manufacturing sites. Digital transformation case study.