Nexans has been awarded the contract for the Celtic Interconnector developed jointly by the Irish and French Transmission System Operators (EirGrid and RTE – RΓ©seau de Transport dβElectricitΓ©). This 700 MW capacity project is the world longest XLPE interconnector to be built and the first subsea link for direct electricity exchange between France and Ireland.
The Celtic Interconnector is recognized as a project of common interest (PCI) by the European Union. It will allow the exchange of electricity between Ireland and France, supplying power to approximately 450,000 homes, and is key in developing an integrated energy system in Europe. Such a system will speed up the European energy transition by fostering the development of renewable energy resources. The project will further help the European Union achieve its energy policy and climate objectives of affordable, secure and sustainable energy for all.
The interconnection between France and Ireland will use HVDC 320 kV technology. It includes 500km subsea cable route, 40km underground route in France (Brittany), 35km underground route in Ireland (Cork County). The 400 kV HVAC 10km connection to the Irish grid is also part of the project awarded to Nexans.
The cables will be produced in Nexansβ state-of-the-art facilities. The 1,000km of subsea cables will be manufactured in Halden (Norway) and the 180km underground cables will be manufactured in Charleroi (Belgium). Accessories will be manufactured in Cortaillod (Switzerland). Proven project delivery model along with the newly built Nexans Aurora Cable Laying Vessel and key subcontractors will ensure the highest installation and protection delivery standards. The project includes the innovative bundle lay of the two HVDC power cables along with full data capacity repeated fiber optic system.
Signing the contract for the Celtic Interconnector further cements Nexans as a major player in renewable energy. We are proud to contribute to such a historic project that works directly with the European Unionβs goal of electrical solidarity between Member States. Nexans is leading the way in connecting the parts of the world with the highest renewable energy potential to the parts of the world with the greatest demand for electricity. From energy generation and transmission to distribution and usages, Nexansβ solutions cover the full electrification value chain to ensure electricity can be delivered to all corners of the world securely, reliably, and efficiently.
CEO, Nexans
Expected to be built and energized by 2026, this major project is an important milestone in Nexansβ goal of becoming a pure electrification player. The Group keeps implementing this strategy by working on projects like the Celtic Interconnector, demonstrating its expertise and strengthening its position as a leader and an electrification pure player.