Installation of cable laying equipment commences on Nexans Aurora
The Nexans Aurora project managers from Maats, Nexans and Ulstein Verft, respectively, meeting up to inspect the installations.
The installation of the state of the art, MAATS cable laying equipment on board the CLV vessel Nexans Aurora has now commenced at the Ulstein Verft shipyard.
On 14 October, MAATS’ & Marine Fabricators’ installation team arrived on site to begin the installation, which kicked off with the two lay wheels being fitted at the stern. These wheels, in combination with the specially designed fairings, assist in guiding the cable in a controlled manner as it enters and exits the vessel. Following the lay wheels, final installation work is now being completed on the MAATS Tensioners and 75t SWL Capstan. The innovative vessel is constructed using the combined expertise of Nexans’ extensive cable laying experience, Skipsteknisk’s naval architecture know-how, Ulstein Verft’s shipbuilding prowess, and MAATS’ specialist engineering.
The first lay wheel about to be installed, photos by Daniel Osnes.
The vessel boasts a concentric, split basket 10,000Te carousel, dual cable laying capabilities, utilization of separate Capstan or Tensioner firing lines, and the ability to complete operations in the most severe weather conditions anywhere in the world.