Subsea cable resilience: Why Europe must rethink Inspection, Maintenance and Repair (IMR)
Electrification of tomorrow
14 April 2026
5 min
Subsea cable resilience

IMR: the invisible backbone of Europe’s energy transition

1.3 million km. Enough to run 32 times Earth’s circumference at the equator. Beneath Earth’s seas lies a rapidly expanding network of high-voltage subsea cables—critical infrastructure enabling offshore wind integration, cross-border electricity flows, and system stability.

But their importance is growing faster than their protection.

Europe is accelerating its ambitions, targeting 60 GW of offshore wind capacity by 2030 and 300 GW by 2050, according to the European Commission. At the same time, global demand for subsea power cables is expected to double by 2030, driven by offshore wind and interconnection needs (source: HSBC Global Research, 2023).

Recent incidents in the Baltic Sea have further exposed a key vulnerability: as resilience on subsea infrastructure increases, so does the impact of disruption.

The result is a simple but critical reality: subsea cables are no longer just technical assets, but strategic infrastructure.

 

Subsea cables: strategic lever for Europe

The role of subsea cables is evolving alongside the broader energy transition.

What was once considered a technical layer is now directly linked to energy security, sovereignty, and investor confidence. As offshore wind expands and interconnections multiply, the tolerance for prolonged outages is shrinking.

This is driving a shift in expectations, from reactive repair models to structured, anticipatory IMR strategies embedded into infrastructure planning.

For Europe, the challenge goes beyond technology. It is about aligning capabilities, coordination, and long-term investment with the scale of ambition.

If subsea cable failures remain relatively rare, when they occur, their consequences are immediate. With limited redundancy in power transmission systems, outages can disrupt electricity flows, impact markets, and delay renewable integration. Repair operations are complex and costly, depending on location and conditions.

At the same time, the ecosystem required to respond such as specialized vessels, skilled personnel, and available equipment remains constrained.

What are the results? A growing imbalance: more infrastructure, higher exposure, and limited ability to recover quickly.

 

Rethinking resilience: from prevention to readiness

Operators increasingly recognize that failures cannot be entirely avoided, whether due to environmental conditions, human activity, or external threats. The real differentiator is therefore not only prevention, but preparedness.

Inspection, Maintenance and Repair (IMR) play a central role in this shift. By combining proactive monitoring with the ability to intervene rapidly, IMR enables operators to reduce downtime and maintain system continuity.

In this context, resilience becomes operational: assets have to be restored quickly when it matters most.

To meet these new demands, the industry is moving toward more integrated models, linking infrastructure delivery with lifecycle services.

Combining EPCI (Engineering, Procurement, Construction, Installation) capabilities with IMR allows for:

  • Greater continuity between installation and operation
  • Faster, more efficient interventions
  • Improved visibility over asset condition
  • Reduced lifecycle risk.

For operators and developers, this approach helps shift IMR from a contingency measure to a built-in component of system design.

IMR subsea cable resilience

From theory to reality: what effective IMR looks like

Real-world operations demonstrate that resilience depends on preparation, speed, and execution.

The repair of Estlink 2, a key interconnector between Finland and Estonia, demonstrated how rapid mobilization and coordinated offshore operations can restore critical infrastructure within a controlled timeframe.

In a different context, the subsea cable replacement in Corfu highlighted the importance of adaptability, delivering reliable power supply under constrained and complex marine conditions.

Together, these examples illustrate a core principle: resilience is not defined by avoiding incidents, but by the ability to respond effectively when they occur.

The role of Nexans: enabling resilient electrification

As subsea infrastructure becomes more strategic, the need for experienced and integrated players increases.

Nexans combines expertise across cable design, installation, and lifecycle services, including IMR. Through dedicated agreements, advanced monitoring technologies, and adaptable repair solutions, Nexans supports operators in reducing response times and maintaining system reliability.

With a global track record across diverse environments, this approach contributes to more resilient and dependable electrification systems.

From insight to action

Want to go deeper? Nexans’ latest position paper explores the structural challenges and strategic solutions shaping subsea cable resilience in Europe.

It provides detailed analysis of the IMR capability gap, evolving policy landscape, and the operational conditions required to ensure rapid and effective cable repair. You’ll also find expert perspectives, real-world case study, and concrete recommendations to strengthen infrastructure resilience.

Download the full position paper to understand how Europe can secure its subsea infrastructure—and accelerate the energy transition with confidence.

Safeguarding the invisible lifelines

Position paper

Safeguarding the invisible lifelines

Download the position paper

Building resilience for the electrified future

Europe’s energy transition depends on the reliability of the infrastructure that supports it.

As subsea networks expand, resilience will become a defining factor, not only for operational performance, but for the credibility and scalability of the entire system.

Strengthening Inspection, Maintenance and Repair capabilities is therefore not just a technical priority. It is a key enabler of secure, sustainable, and resilient electrification.