Case study

Nexans to connect France's Saint Brieuc offshore wind farm to shore

  • LIEU
    Saint Brieuc, France
  • PARTENAIRE
    RTE
  • MARCHÉ
    Fermes éoliennes-Offshore
496 MW

GENERATED OF WIND TURBINES

225 kV

MAXIMUM VOLTAGE

67 km

OF OFFSHORE CABLES

93 km

OF ONSHORE CABLES

  • Nexans will provide the 225 kV power export cables for Saint Brieuc, one of the biggest offshore wind projects in France

  • In the framework of the 115-million-euro contract, Nexans will deliver cables featuring innovative hybrid armouring

  • Nexans will also provide Inspection, Maintenance and Repair (IMR) services for the project 

 

About the project

RTE France has awarded a € 115 million contract to Nexans to supply and install the 67km offshore and 93km onshore power export cables for the 496 MW Saint Brieuc offshore wind farm. Located in the English Channel, some 16 km off the coast of Saint Brieuc Bay, the wind farm is expected to generate enough power to meet the daily electricity needs of more than 835,000 homes. 

The project is being developed by the Ailes Marines Consortium and is one of the biggest commercial-scale offshore wind projects in France. Its success is of significant importance as it will help meet France’s climate change ambitions.

The consortium has been awarded 500 MW capacity transmission by the French government. RTE, the French transmission system operator, will design, build and maintain the two 225 kV links (submarine and land) to connect the offshore wind farm to the grid.

Nexans' Solutions

For the submarine cables, Nexans will supply two lengths of 33.5 km 225 kV 3-core cable with an innovative hybrid armouring solution. The cable also features a fibre optic element for remote health monitoring of the cable link and transmission of information between the offshore wind farm and land base. Cables will be installed by Nexans’ own cable-laying vessel, the CS Skagerrak, while the specialized Capjet system will be used to trench the cables into the seabed for protection. The awarded contract also includes Inspection, Maintenance and Repair (IMR) services for the offshore part of the link.

The land cables will include 93 km of 225 kV single-core cable, similar to those provided to RTE by Nexans under the current land cables framework agreement.

“This project will be the first offshore connection developed by Nexans for RTE. As such, RTE expects this project to be successful as well as to mark the beginning of a fruitful relationship. commented Jean Michel Prost, Marine activities director at RTE.

Nexans Norway facility in Halden will manufacture the submarine cables, while the land cables will be supplied by Nexans Benelux plant based in Charleroi, Belgium. The fiber optic elements will be supplied by Nexans Norway plant in Rognan. The laying of the submarine cables is due to commence in spring 2022.

“ We are delighted to be working with RTE to provide the grid connection for one of France’s most significant offshore wind projects. The key to this success was our long track record in this sector combined with our ability to offer innovative cable solutions. ”

Laurent Guillaumin

Business Development Director – Offshore Wind Europe
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
Vous avez le droit de vous opposer au traitement de vos données personnelles et/ou à leur utilisation à des fins de marketing direct ou à des fins commerciales.

Merci !

Merci de nous avoir contactés. Nous vous contacterons sous peu.

Erreur

Une erreur s'est produite. Veuillez réessayer.

Fermer