Artificial Intelligence (AI) has been around for a while. The first models date back to the 70s but these concepts remained theoretical until we were actually able to teach computers to think for themselves. Today, Artificial Intelligence is everywhere. It allows computers and cloud connected devices to reproduce human-related behaviours such as reasoning, planning and creativity. Artificial Intelligence is primarily dependent on the quantity of data it is given. This is where big data plays an active role. With the increased collection and analysis of digital data, big data and AI are now emerging as rich areas of opportunity for electrification professionals.
Electricity 4.0 : Big data and AI for smarter power management
Big data is a major trend in the energy industry. The Electrical network become smart grid due to Data collected from a variety of sources, such as smart meters, sensors, twin digital. Once stored, this data is an invaluable resource for the industry to make better decisions about energy production and consumption.
Electricity was deployed extensively in the late 19th century, which was the First Wave of Electrification from 1880 to 1920. This period saw the widespread adoption of electrical power in industry and the development of the first electrical grid. Then the Second Wave of Electrification took place between 1920 and 1950 with the expansion of the electrical grid into homes and the development of new electrical appliances such as refrigerators, washing machines⦠During the third wave of Electrification from 1980 to present, we have seen the growth of the digital revolution and the development of new technologies such as computers, the Internet, and mobile phones.
Today the fourth wave of electrification so-called Electricity 4.0 is characterized by the integration of digital technologies such as Artificial Intelligence (AI), the Internet of Things (IoT), and advanced data analytics into the electricity infrastructure.
The aim of Electricity 4.0 is to create a smarter, more efficient, and more sustainable electricity system that can respond to the fast changing demands (+20% by 2030, +40% by 2040).
Electricity 4.0 is expected to optimize the use of existing assets, integrate renewable energy sources into the grid, increase energy efficiency, reduce greenhouse gas emissions, improve grid stability, reduce costs for customers and provide more reliable and flexible energy services to customers.
Moreover, generative AI and adjacent models are changing the game. Indeed, support technology reaches a new level, application development time is reduced, and powerful capabilities are brought to non-technical users.
Just recently, we saw the buzz around ChatGPT and what it can achieve. For instance, if we ask the question βhow do big data and AI impact electrificationβ, we have to admit ChatGPT answer might not be perfect but is still very impressive.
These technologies will definitely have an impact on the world of electrification. But AI is mainly dependent on the quantity and quality of the data that will be used to learn. Big data provides the storage and processing capabilities necessary to educate the AI by feeding it with a lot of information.
Machine Learning and AI are the winning combo to efficiently exploit big data. This involves identifying patterns via data mining and data science more generally.
Big data: The cloud has won
In the age of big data, the famous wave 2 of “move to cloud” announced by providers is underway and is accelerating. As a reminder, the first phase of a migration to the cloud is a discovery phase that allows to analyze the strengths and weaknesses of an infrastructure and to determine future needs.
The number of detractors is getting smaller every day, privacy and sovereignty issues are both solved by the strategic commitments of clouders and swept away by the ease of use… All sectors – banking, telecoms, insurance, etc. – are rapidly adopting cloud-hosted big data solutions.
The first paradigm shifts are appearing in the world of electrification, driven in particular by operators such as Total Energie or Schneider. We can also note the predominance of the estimated Azure services of Microsoft Vs Aws of Amazon in the field of public cloud related to big data.
aa