Superconductors beneath the waves: Powering the energy transition
Renewable energies
07 October 2025
6 min
subsea-superconductivity-cables-banner

Powering the future: grids under pressure

Electricity is increasingly seen as the most viable path to reduce greenhouse gases, improve efficiency, and strengthen energy security. In fact, achieving national energy and climate goals requires global electricity use to grow 20% faster over the next decade than it did in the previous one. But today’s grids are struggling to keep up.

Demand is rising rapidly due to electric vehicles, heat pumps, and digital services. At the same time, renewable sources such as wind and solar are expanding at a record pace – but often in remote locations far from consumption centers. This combination creates a single, big challenge: move far more sustainable electricity, much farther, much faster. Meeting it requires not only new renewable plants but also grids that are smarter, stronger and more sustainable.

One promising answer lies beneath the waves: subsea superconducting cables, capable of transporting gigawatts of power with minimal losses, shrinking offshore platforms and simplifying grid infrastructure. 

+20%

electricity use must grow 20% faster in the next decade to meet climate goals

80m km

grids to be added or refurbished by 2040

>80%

share of wind and solar in global
power capacity increase by 2040,
up from <40% today

Connecting renewables at sea

Offshore wind power capacity is growing rapidly in Europe, Asia, and the United States. Yet this potential comes with mounting technical and economic hurdles.

Conventional transmission technologies, based on high-voltage alternating (HVAC) or direct current (HVDC) cables, present significant obstacles. They require large offshore platforms to convert power before it reaches the grid, adding both expense and environmental impact. They are also subject to supply chain bottlenecks, which risk delaying projects just as governments raise their targets for renewable integration.

By 2050, the majority of Europe’s electricity is expected to come from renewables. Meeting that goal means upgrading or modernising around 300,000 km of transmission lines and subsea cables. Tomorrow’s energy networks must not only carry greater volumes of power, but also deliver flexibility to cope with fluctuating renewable generation.

Key components of infrastructure transformation will include offshore wind farms, hydrogen pipelines, and long-distance transmission corridors – and crucially, technologies that allow massive amounts of electricity to flow reliably over long distances.

subsea cable for offshore wind farm

Subsea superconducting cables

Superconducting grids could speed up the integration of large-scale renewables—offshore wind farms and remote solar plants alike—by offering an alternative to conventional technologies for bulk power transmission, with lower environmental costs and quicker deployment.

Most new power assets, especially wind and solar, are built in remote locations, demanding vast new grid infrastructure in previously untouched areas. The most complex and time-consuming element of long-distance transmission is the offshore HVDC conversion platform. Superconducting cables offer two ways to bypass it, carrying several gigawatts of power over distances of 50 km or more.

Option 1: DC high-power transfer at medium voltage

Superconductors can carry very high currents without electrical losses. This makes it possible to transfer large amounts of power at lower voltages, while still maintaining—or even increasing—the capacity of the system. In renewable energy, both wind and solar power naturally produce direct current (DC) at medium voltage during their conversion process. This DC is collected and concentrated into medium-voltage direct current (MVDC) export cables for transmission. The Horizon Europe project SCARLET is focused on developing this approach.

Option 2: DC high-power transfer at medium voltage

Superconductors can also extend the reach of HVAC export cables. Future wind turbines are expected to generate alternating current (AC) power at 132 kV, a voltage suitable for medium-distance transmission. Conventional HVAC cables face a key limitation at this voltage: to reduce energy losses over long distances, they require higher voltages and multiple parallel lines, and their insulation capacitance steadily drains energy along the route.

Superconducting cables, by contrast, can carry much higher currents with less capacitance, which means they can deliver more power efficiently at lower voltages. This solution is now viable thanks to the convergence of three mature technologies:
– Cryogenic pipelines that keep superconductors at the required low temperature
– High-temperature superconducting (HTS) cables, refined over 20 years by Nexans
– LNG-based cooling systems developed by Air Liquide

The benefits of superconducting cables

Beyond technical feasibility, superconducting cables deliver tangible advantages for grids under pressure:

  • Carry far higher currents than copper or aluminium, allowing bulk electricity transmission at lower voltages over long distances
  • Offer an unmatched power density: a single 17 cm cable can deliver 3.2 GW – roughly the output of three nuclear reactors
  • Emit neither heat nor electromagnetic fields, avoiding interference with nearby power, telecom or pipeline systems
  • Are compact and unobtrusive, reducing infrastructure footprint in sensitive marine environments
  • Simplify offshore schemes and shrink conversion platforms by at least 75% by replacing resistive HVDC systems.

 

How will this help electrify the future?

Superconducting technology is emerging as a critical enabler of the energy transition. By combining HTS cables with fault current limiters, grids can achieve unprecedented levels of efficiency, capacity and sustainability. These systems expand network flexibility, simplify offshore connections and ease the integration of renewables at scale.

As global demand rises and climate pressures mount, superconductors offer a compact, modular and resilient alternative to conventional infrastructure. By reducing grid losses and supporting long-distance transmission, they align directly with the goals of electrification and decarbonisation. HTS cables, refined by industry pioneers, such as Nexans, are designed to meet this demand.

Picture of Arnaud Allais

Author

Dr. Arnaud Allais is Chief Technology Officer Machinery, Cryogenic and Superconducting Systems at Nexans. Arnaud is a globally recognized authority in advanced electrical grid technologies and high temperature superconductivity (HTS). With over two decades of experience, he leads innovation and strategic development in advanced superconducting systems that are shaping the future of energy transmission.

Arnaud earned his Ph.D. in Materials Engineering from the School of Mines of Paris, in collaboration with Alcatel, where he focused on modeling Powder-in-Tube Bi2223 superconducting wires. He also holds an engineering degree in Energy and Materials from the School of Engineering in Orléans, France. Throughout his career at Nexans, Arnaud has held several key leadership roles, including: Director of the Nexans Research Center, and R&D Program Director at the SuperGrid Institute – a joint R&D venture with GE, Alstom, EDF, and leading French universities.

Superconducting systems: The game-changing solution for tomorrow’s energy grids
Electrification of tomorrow
03 October 2025
7 min
superconductivity-grid-banner

The urban grid under pressure

Imagine plugging all your brand-new household appliances into a century-old electric system. The infrastructure is globally aging faster than it is being replaced or upgraded. There is a high risk that system will fail – and the same applies to our urban electrical grids. According to the United Nations (UN), 55% of the world’s population lives in urban areas today, a share projected to rise to 68% by 2050. And these communities demand uninterrupted, high-quality electricity with minimal faults or downtime.

Meanwhile, growing adoption of electric vehicles, heat pumps, and other low-carbon technologies—combined with smaller household sizes—is fueling a surge in both residential and industrial electricity consumption. At the same time, much of the existing electrical infrastructure is aging and operating near capacity limits, with conventional cables and distribution systems originally designed for earlier, centralized energy models now increasingly strained by modern, decentralized power flows and higher load demands.

In other words, there is a growing mismatch between what energy grids can deliver and what modern cities need.

Several systemic constraints stand in the way of modernizing urban grids efficiently:

  • Space limitations: Conventional cabling systems require substantial space and specialized equipment – but underground corridors are already saturated with existing infrastructure, making new cable routing extremely difficult.
  • Escalating costs: Environmental restrictions, land acquisition, and rental fees can add hundreds of thousands of dollars to projects.
  • Grid bottlenecks: Environmental and proximity constraints severely limit the connection of new renewable energy sources, creating a barrier to the very transition these systems are meant to support.
  • Unpopular disruption: Construction works required to install new cables often go with noise pollution, traffic congestion, and environmental concerns leading to increasing public opposition.
  • The reality is clear: succeeding in the energy transition requires radically rethinking electrical infrastructures with innovative technologies that balance growing demand, system resilience, and urban liveability. Enter superconducting systems.

How superconducting technology solves urban grid challenges

HTS cables: Zero-resistance transmission

High Temperature Superconducting (HTS) technology draws its transformative power from its core property: superconductivity. With virtually zero electrical resistance, these cables can carry extraordinarily high currents in much less sections that copper or aluminum conductors. In fact, a single 17-centimeter-diameter cable can handle up to 3.2 gigawatts à high voltage– that’s roughly the output of three nuclear reactors and several 100 MW underground at medium voltage, able to secure the supply of big cities without adding new high voltage lines.

This absence of heat generation eliminates the need for wide thermal clearances and ventilation systems, allowing HTS systems to be installed in simple trenches rather than purpose-built tunnels. Their compact footprint means that the required corridors are up to ten times narrower than for conventional systems. They also generate no electromagnetic interference and emit no external magnetic field, making them safe neighbors to other infrastructures in these confined spaces.

Beyond the installation advantages, HTS systems provide enormous operational flexibility. A 400-kilovolt conventional system can be replaced with a 132 or 275 kV-kilovolt superconducting system without losing capacity at lower cost mainly due to the saving of large 400 kV transformers in the substation—and because the cable system including ancillary systems is modular, the same cable design works equally well for compact urban networks and long-distance transmission.

SFCLs: Instantaneous fault protection

Superconducting properties can also be used to mitigate overcurrent, almost instantaneously. Superconducting Fault Current Limiters (SFCLs) provide vital protection against fault currents that can damage critical assets such as transformers and switchgear. In the event of a short circuit or fault condition, SFCLs instantly and automatically limit excessive current without the need for mechanical intervention or voltage disturbance. SFCLs use superconductors’ intrinsic properties to transition from zero-resistance to resistive state within milliseconds, limiting fault current before it damages  equipment on the same branch. SFCLs can be integrated and connect to any electrical system — offering enhanced network reliability, optimized infrastructure protection, and reduced equipment aging from thermal stress.

 

Proven success in real-world applications

Multiple operational projects demonstrate the technological maturity and transformative potential of superconducting systems in diverse urban environments. Here’s a look at three:

AmpaCity Project, Germany

Nexans manufactured and deployed in 2014 (tbc) the world’s longest superconducting cable link, featuring a three-phase 10kV HTS cable with 40 MVA capacity instead of a 110 kV conventional circuit and an integrated superconducting fault current limiter. The seven years of continuous service have proven the long-term reliability of superconducting technology.

LIPA Project, United States

This project showcased superconducting capabilities in American electrical infrastructure. In 2008 and 2012 (tbc), Nexans developed and delivered complete 138 kV AC superconducting cable systems, including the cable core, cryogenic envelope, and terminations, while supervising installation and commissioning.

Best Paths Project

Nexans designed and built a pioneering 320 kV DC superconducting loop comprising a monopole cable of 30-meter carrying 10 kA current for a nominal capacity of 3.2 GW. The project included comprehensive voltage testing at 1.85× the rated voltage (up to 592 kVDC) and impulse testing. This achieved the world’s first qualification of a full-scale 320 kV HVDC superconducting loop on a test platform, featuring a 6.4 GW HVDC circuit (2 monopoles), representing the highest power transmission capability demonstrated to date.

These concrete achievements demonstrate that superconductors have evolved from experimental technology to an industrial solution set to transform urban electrical transmission and distribution.

 

Building tomorrow’s grid

With operational projects proving their reliability and cities facing mounting pressure to electrify rapidly, superconducting systems represent more than just an upgrade; they’re a fundamental shift in how urban grids can be designed and deployed.

Rather than fighting space constraints and community resistance with conventional solutions, utilities can now build smaller, quieter, and more efficient networks that actually support the energy transition they’re meant to enable. Superconducting systems give cities a practical pathway to meet surging electricity demand while achieving decarbonization goals – a future-ready backbone for resilient and sustainable urban power.

Picture of Beate West

Authors

Dr. Beate West is Head of Engineering for Superconducting Systems in Hannover. She joined Nexans in 2010 as research engineer. She is responsible for the design of superconducting cables and fault current limiters.

Beate has a diploma and a Ph.D. in physics from the University of Bielefeld.

Picture of Arnaud Allais

Dr. Arnaud Allais is Chief Technology Officer Machinery, Cryogenic and Superconducting Systems at Nexans. Arnaud is a globally recognized authority in advanced electrical grid technologies  and high temperature superconductivity (HTS). With over two decades of experience, he leads innovation and strategic development in advanced superconducting systems that are shaping the future of energy transmission.

Arnaud earned his Ph.D. in Materials Engineering from the School of Mines of Paris, in collaboration with Alcatel, where he focused on modeling Powder-in-Tube Bi2223 superconducting wires. He also holds an engineering degree in Energy and Materials from the School of Engineering in Orléans, France. Throughout his career at Nexans, Arnaud has held several key leadership roles, including: Director of the Nexans Research Center, and R&D Program Director at the SuperGrid Institute – a joint R&D venture with GE, Alstom, EDF, and leading French universities.

The grid revolution: how superconductors will power tomorrow and ensure safe and efficient energy transition
Electrification of tomorrow
15 September 2025
11 min
Superconductivity and EV, in cities

Right now, at least 3,000 gigawatts of renewable energy projects are sitting in connection queues worldwide, including 1,500 gigawatts in advanced stages. That’s already five times the solar and wind capacity added in 2022 – and current data only covers half of it.

So, if sustainable energy generation isn’t the problem, then what is? The true obstacle lies in moving that energy from where it’s produced to where it’s needed – and these bottlenecks are fast becoming one of the greatest risks to achieving net-zero targets, energy security, and climate resilience.

What the energy transition requires is infrastructure that matches the scale and urgency of the challenge. Enter superconductors, a game-changing (super) solution capable of aligning grid capacity with ambition.

The infrastructure challenge

As demand from electric vehicles, hydrogen production, and heating and cooling systems accelerates, grids face unprecedented pressure. However, much of today’s cable network—particularly in Western Europe, North America, and Japan—is already decades old, never designed for the loads we are seeing today.

Take, for example, a distribution system operator in New York with a cable network that’s over 50 years old and operating near capacity. Adding new loads from EVs and heat pumps not only accelerates the aging of existing cables but also limits the ability to connect new renewable generation due to thermal and voltage constraints. Replacing or upgrading these cables using conventional high-voltage solutions requires extensive excavation in urban areas, where underground space is already crowded with telecommunications, water, gas, and transport infrastructure.

Even when installation is technically possible, environmental restrictions, lane rental charges, and traffic management fees can increase project costs by hundreds of thousands of dollars. Land acquisition for wider cable routes compounds the challenge, particularly when existing rights-of-way cannot accommodate the spacing needed for conventional cables, which require significant separation to manage heating effects and electromagnetic interference.

Meanwhile, safety and reliability requirements keep rising. Networks must deliver electricity without cuts, breakdowns, cascading failures, or blackouts. They need to handle fault currents that can damage critical assets like transformers and switchgear. And as public expectations grow, networks must minimize electromagnetic interference, reduce CO₂ emissions, recycle obsolete assets responsibly, and reassure communities about safety.

This scenario is playing out in major cities worldwide, while rural areas face their own infrastructure constraints. Meeting electrification needs at scale will require massive infrastructure upgrades: grids will need roughly 80 million kilometers of new or refurbished cable by 2040 – and conventional systems alone cannot keep up with demand.

data center

Data centers: a core challenge

In addition, data centers have emerged as the core of the digital infrastructure, operating with extensive computational power, storage capacities and energy requirements. However, as their footprint and power consumption increase, significant challenges arise in terms of efficiency, heat management, land utilization, and environmental impact. The demand for digital services is soaring. As the digital economy continues its exponential growth, data centers are becoming the backbone of global digital infrastructure. Hyperscale and gigawatt-scale data centers are emerging to meet soaring compute demands, especially driven by AI, cloud services and advanced analytics. These next-generation facilities are pushing the limits of traditional electrical infrastructure, both inside and outside the data center footprint.

Power requirements are rapidly escalating, with new hyperscale data centers being designed for power capacities approaching or exceeding 5 gigawatts — an order of magnitude above previous-generation facilities. This scale introduces critical challenges in power delivery, thermal management, land use, carbon emissions and capital investment. The current reliance on conventional copper-based cabling systems is increasingly unsustainable.

The bottleneck in numbers

3,000 GW

of renewable energy projects are stuck in grid connection queues worldwide – 5x the solar & wind capacity added in 2022

1,500 GW

of that total are in advanced stages

80m km

of new or refurbished cable needed by 2040 to meet electrification targets

About

10%

of electricity is lost during transmission over long distances – equivalent to roughly 180 TWh per year in Europe

> 5 GW

power capacities of new hyperscale data centers — an order of magnitude above previous-generation facilities. This scale introduces critical challenges in power delivery, thermal management, land use, carbon emissions and capital investment

The superconducting solution

High-Temperature Superconducting (HTS) cables and fault current limiters represent a fundamentally different approach to power transmission. The technology exploits the complete loss of electrical resistance that occurs in certain materials at extremely low temperatures, known as one of the key properties of superconductivity.

HTS materials require cooling to approximately -200°C, typically with liquid nitrogen. “High temperature” here means relative to the first generation of superconductors, which requires temperatures below -243°C to operate. The liquid nitrogen circulates in cryogenic envelopes, a thermally-insulated jacket that surrounds the cable. Liquid nitrogen is relatively inexpensive, environmentally harmless, and easier to manage than many industrial coolants. More importantly, the energy saved by eliminating transmission losses exceeds the energy required to maintain the cryogenic environment.

The electricity flowing through your home right now has traveled hundreds of miles of conventional resistive cables, losing roughly 10% of its power along the way. That waste, about 180 TWh annually in Europe alone, is enough to power three major cities. HTS cables requires 10 times less energy to supply electricity.

Why choose superconducting cables?

For modern grids, HTS systems offer huge advantages over conventional alternatives, especially in dense urban environments:

  • Space efficiency and economics: HTS cables generate no heat or electromagnetic fields at any load along the cable route, so phases need no separation. Cables can be buried at any depth and close to other multi-energy network without expensive tunneling or specialized conduits, shrinking rights-of-way to up to one-tenth the width of conventional systems. In cities where land costs tens of thousands per meter, this benefit alone is game-changing.
  • Enormous transmission capacity: One HTS cable can handle over 3 gigawatts. Fewer circuits and minimal substation upgrades are needed, while retrofits can multiply tunnel capacity without major construction with minimal electrical loss if not zero in Direct Current.
  • Smaller environmental footprint: Less excavation and reduced permitting complexity can result in shorter project timelines and less public opposition.
  • Resilience: Fully shielded, superconducting cables are weatherproof, highly secure, and nearly free of stray electromagnetic fields – meaning power availability is protected even if part of the grid is disrupted.

It’s a win-win(-win-win).

Superconductivity and train stations, in cities, data centers

Grid transformation beyond capacity

Unlike conventional grids that struggle with distributed energy resources like rooftop solar, fuel cells, and remote wind parks, HTS systems enable networks to absorb energy from any source and facilitate market-driven power flows.

Superconducting Fault Current Limiters (SFCLs) is invisible in the network during normal conditions, and automatically transition to a highly resistive state when faults occur, limiting dangerous currents and reducing the level of short circuit current to be supported by all the equipment in the substation before circuit breakers activate. This technology is using intrinsic behavior of superconductors and is not requiring active control or monitoring.

This technology supports the move to smarter, more flexible grid systems where demand can adjust with multiple supply sources. Urban power densities can increase dramatically with minimal public disruption, thanks to SFCL that can absorb the increase of short circuit current induced by the addition of new sources and new load in the network.

For electric vehicle charging infrastructure, the capacity and efficiency advantages become particularly important as charging speeds increase and deployment scales up. Industrial electrification processes that require large amounts of reliable power can be supported without the massive infrastructure investments that conventional systems would require.

For data centers, this unlocks transformative advantages across power transmission, distribution, and infrastructure design. Delivering efficient and reliable power in limited spaces is a major industry concern, and superconducting cable systems offer a promising solution. With zero electrical resistance, ultra-high current capacity and a compact footprint, HTS cables can radically simplify power infrastructure, reduce thermal loads and support the broader goals of sustainability and electrification. Superconducting cables (High-Temperature Superconducting (HTS) systems)represent a transformative solution for power transmission within and around large-scale data centres. These advanced conductors can transmit electricity with virtually zero resistance, eliminating the energy losses and heat generation that are inherent to traditional copper-based systems.

Smarter, denser grids

  • Any source, anywhere: HTS cables handle rooftop solar, fuel cells, remote wind parks.
  • Automatic protection: SFCLs limit fault currents instantly, no active controls needed.
  • Smart, resilient grids: SFCLs allow the increase of supply and demand, improving reliability and supporting integration of distributed or remote generation.
  • Electrification ready: Scales EV charging and industrial loads without massive new builds.

Ready for a superconducting grid revolution?

Infrastructure demands, technological maturity, and a strong business case are aligning to support widespread HTS adoption. Companies like Nexans, with facilities across Germany, France, and Norway, have developed cutting-edge expertise across the entire superconducting technology stack and are contributing to international standards that will accelerate global rollout.

The question isn’t whether superconducting technology will transform electrical grids, but how quickly utilities, governments, and investors will recognize the opportunity. Grid operators who move early will gain significant competitive advantages in efficiency, reliability, and capacity. Those who wait may find themselves constrained by the very infrastructure limitations that superconducting technology is designed to solve.

Photo of Yann Duclot

Author

Yann Duclot is Acceleration Units Director at Nexans. In this role, he oversees the Nexans Acceleration Units made of 2 companies centered around the Energy Transition: Nexans Solar Technologies (NST) and Nexans Machinery, Cryogenics and Superconductivity (MCS).  Yann leads a team of 65 people based in France and Germany centered around the engineering, manufacturing of new and disruptive technologies (superconductivity, cryogenics, solar trackers) in order to accelerate our growth in high potential markets for the energy transition.

Yann began his career at Nexans in 2000 and, with a brief interruption at Cavotec as Chief Marketing Officer, has now been part of the company for 14 years. With over 25 years of experience in business unit management, organizational transformation, and innovation leadership, Yann has been instrumental in scaling up business activities and driving the company’s growth and profitability. He holds a Master of Science from Grenoble Ecole de Management (GEM).

Superconducting cables, miracles of electrical connectivity
Electrification of tomorrow
06 September 2023
5 min
Superconducting cables

Superconductivity is currently the subject of intense interest and debate, fuelled in particular by research into superconductors at ambient temperature and pressure, the discovery of which would trigger a technological revolution. The many questions raised by this work are reminiscent of the scientific challenges researchers had to overcome when they discovered high-temperature superconductors in 1986. A look back at this crucial technology for the cable industry, exploring recent advances, persistent challenges, but also how Nexans is providing the world’s very first superconducting cable system integrated into a rail network.

As we move towards an all-electric future, the need to increase power supply in cities becomes ever more urgent. Equally important is the need for resilience: as electricity becomes the main source of energy, supply will need to be 100% reliable. Downtime is not an option.

Why superconductors?

Superconducting cable are electrical connectivity miracles. They have unique qualities that make them perfectly suited to modern, high-capacity electrification projects in cities.

First, superconducting cables can carry extraordinarily high currents – far greater than conventional copper or aluminium cables. This makes it possible to transmit and distribute electricity at relatively low voltages. In practical terms, this means there is less need for substations in city centres – a major cost saving.

Second, superconductors can transmit a huge amount of power relative to their size. For example, a single superconducting cable with a diameter of just 17 cm can transmit 3.2 GW – enough to power a large city. Corridors for superconducting cables can be as narrow as one metre, meaning they can be deployed with minimal disruption.

Third, superconducting cables do not produce heat and can be fully shielded on an electromagnetic standpoint, so there is no interference with power, telecom and pipe networks which typically criss-cross cities. Many of the constraints that govern cable routing do not apply when superconductors are used.

On top of this, superconductors are incredibly efficient. Superconducting cables have extremely low resistance when an AC current is carried and no resistance when the current is DC, so losses are minimal.

superconductor-cable-nexans

A first for rail

Nexans is working with SNCF, France’s national rail company, on a pioneering project to boost power supplies to Montparnasse station in Paris using superconducting cables.

Montparnasse is one of the busiest railway stations in France and handles more than 50 million passengers a year. This figure is expected to exceed 90 million by 2030. Handling new demand will require extra trains – and extra power.

As with any city-centre power upgrade, the big challenge at Montparnasse was finding a way to bring in a new power supply without the need to dig up the surrounding roads – which can be a long, expensive and disruptive process.

Fortunately, the existing cable route between Montparnasse railway station and the substation that serves it had spare conduits available. Unfortunately, there were only four of them. Using conventional copper cables to deliver the required power would require a dozen of cables. What could be done?

Superconducting cables are the answer. Nexans’ solution uses just two cables, each less than 100mm in diameter so they can be easily threaded through the existing conduits. Despite their small dimensions, each cable is capable of handling 5.3 MW, or 3500 A at 1500 VDC – a huge amount of electrical energy.

What makes this project so significant is that it is the first-ever use of superconducting cables in France, and the first time superconductors are integrated in a railway grid anywhere in the world. The new power supply at Montparnasse will be commissioned in 2023.

What does the future hold?

The Montparnasse project underlines the massive potential superconducting cable systems have for boosting power supplies in cities – particularly where site constraints place limits on the use of conventional copper and aluminium cabling.

Rail transport aside, superconducting cable systems are likely to play a bigger and bigger role in satisfying the rising demand for electricity. This is being driven by new commercial uses – such as data centres – and by new sources of domestic consumption, which include electric vehicle charging, heat pumps and air conditioning.

In addition to meeting increased demand for bulk power, superconducting systems will play a critical role in boosting the resilience of urban electricity networks.

The Resilient Electric Grid (REG) project in Chicago, USA, underlines the direction of travel. Nexans designed, manufactured and installed a superconducting cable for the REG system, which helps to prevent power outages by interconnecting and sharing excess energy capacity from nearby substations, and by preventing high fault currents.

Nexans is the global leader in superconducting cable systems. Our unique capabilities in R&D, innovation, testing, manufacturing and deployment mean that we are perfectly placed to assist our customers, partners and stakeholders as they prepare to electrify the future.