The Invisible Backbone: 5 Unsung Innovations Keeping Wind and Solar energy Alive
Renewable energies
22 August 2025
6 min
invisible-backbone-banner

Imagine standing at dawn under a remote wind farm, the turbines slicing through salty air, miles from the nearest city. What guarantees these giants deliver resilient power to the grid, day after day, through all-weather events? The answer isn’t obvious, or visible. It’s the unspoken link: the connecting accessories quietly holding everything together.

As the transition to clean energy accelerates, wind and solar are no longer marginal contributors; they are quickly becoming the backbone of the renewable energy transition.

According to the IEA’s updated Net Zero Roadmap (2023), to reach net-zero energy sector CO2 emissions, over 70% of new energy capacity must come from wind and solar farms by 2050. But scaling up to meet this target is only half the battle. Ensuring wind and solar installations operate reliably across oceans, deserts, or mountains is just as critical.

Wind and solar farms are often built in some of the world’s harshest and most remote locations. Once installed, their components must function for decades with limited human access and under constant exposure to salt, sand, heat, and vibrations.

While most attention is focused on turbines and electrical panels, equally critical elements of system performance lie in the accessories that connect everything.

 

invisible-backbone-illustration

Accessories: the critical link to renewable energy reliability

Cable accessories (joints, terminations, and connectors) are crucial to the reliability of solar and wind energy. In fact, up to a third of breakdowns in these enormous installations start not in the blades or panels, but in their connections (WindEurope O&M Benchmarking, 2022). It’s as if a single loose shoelace could halt a marathon. For the industry? That means billions in lost power, unexpected outages, and missed climate targets that affect us all. These vital connection components may be invisible, but their performance has a direct impact on grid uptime, maintenance costs, and return on investment.

Like any high-performance system, such as long-haul aviation, offshore oil rigs, or space exploration, solar and wind systems demand components that are robust, modular, and remotely diagnosable. In a utility-scale wind or solar energy farm, a single weak link can compromise system integrity and interrupt power delivery. Which is why the industry is shifting from passive, one-size-fits-all accessories to tailored, intelligent component systems that anticipate downtime risks, extend infrastructure lifespan, and reduce overall operating costs.

The 5 grid accessory innovations leading this shift are: modular 145kV connectors for offshore wind farms, pre-assembled cable systems for grid electrical systems, sensor-based components, modular cable kits, and high-performance polymers and sealing materials.

Five accessory innovations redefining reliability in wind and solar energy farms.

1. Offshore-ready connectors engineered for high-voltage resilience

Offshore wind farms face unique conditions: constant motion, salt-laden air, and high-voltage transmission requirements. Conventional connectors can corrode, loosen, or degrade over time.

The innovation: Compact, modular 145 kV connectors designed for offshore wind applications are enabling more efficient transmission from increasingly powerful turbines. Their compact design facilitates installation in constrained environments while minimizing bending forces on connected equipment such as switchgear or transformers. Engineered for long-term performance, they feature high resistance to corrosion, vibration, and pressure, making them well-suited for the harsh and demanding conditions of subsea and offshore environments.

The result: Fewer failure points, longer service intervals, and enhanced safety in locations where unplanned repairs are difficult and expensive.

2. Pre-connected cable systems that minimize human error

In remote or high-risk locations, every hour spent on electrical installation increases exposure and cost. Grid technicians often face high levels of fatigue, while installation errors such as overtightening or misalignment can compromise long-term performance.

The innovation: Factory-assembled, tested and pre-connected cable systems minimize on-site handling, which helps reduce human error and accelerate installation in challenging environments.

The result: Safer, faster installations and greater reliability from day one, especially important in demanding environments.

3. Sensorized accessories that detect failure before it happens

Failure in a joint or termination often begins invisibly due to exposure to thermal fatigue, mechanical stress, vibrations, and moisture ingress. In remote wind and solar farms, these silent failures can go undetected until a power outage occurs.

The innovation: Accessories equipped with built-in sensors that continuously monitor internal conditions such as temperature and insulation health. The sensor-generated data is directly integrated with Supervisory Control and Data Acquisition (SCADA) systems and predictive operation and maintenance (O&M) schedules, enabling smart monitoring and intelligent diagnostics. Ørsted, the global leader in offshore wind and one of the world’s largest renewable energy companies, integrates cable diagnostics and performance monitoring into its offshore substations to support early fault detection and reduce unplanned downtime.

The result: Issues are detected early, enabling preventive maintenance instead of reactive repairs. This significantly reduces downtime and helps operators move toward fully digital, condition-based asset management.

4. Modular connector kits adapted to site-specific layouts

Each solar and wind farm configuration is unique.  Varying terrain, layout constraints, and project scale all affect how cable accessories are planned and installed.

The innovation: Modular connector kits tailored to site-specific layouts are now helping reduce errors and delays on large renewable projects. Each wind or solar farm comes with its own constraints (terrain variations, equipment spacing, layout geometry)—which can complicate on-site installation. To streamline this process, system modeling tools are used upstream to configure customized kits of pre-assembled connectors, adapted to the physical layout and routing paths of each site.

The result: This modular approach, inspired by practices used in offshore wind and utility-scale solar projects, ensures faster, safer, and more reliable installations, especially in remote or hard-to-access environments where technician time is limited and rework is costly.

5. Materials that resist decades of environmental stress

UV exposure, salt spray, sand, moisture ingress, hot ambient temperature and thermal cycling are harsh realities for wind and solar installations.

The innovation: High-performance polymers (such as EPDM Material) and sealing materials that resist abrasion, extreme temperature variations, and long-term weathering. These components are engineered to maintain integrity under the toughest environmental conditions, whether buried, exposed, or submerged.

The result: Accessories that withstand years of exposure without degradation, helping ensure system stability over time. Offshore wind developers now utilize vibration-tolerant junction systems to extend the lifespan of accessories in one of the harshest operating environments. As renewable infrastructure expands into increasingly extreme terrain and climate zones, long-lasting materials are proving crucial to performance and return on investment.

Innovative accessory technologies for a more resilient wind and solar energy future

As wind and solar energy take center stage in the global energy mix, connecting accessories must evolve to meet the demand for robust components that are adapted to extreme environments. Innovative accessory technologies are transforming once-passive components into intelligent, tailored, and long-lasting solutions that improve the system-wide reliability and cost-effectiveness of large-scale wind and solar farms.

Smart accessories, equipped with embedded diagnostics, connected to SCADA systems, and optimized through system modeling, are helping operators meet performance expectations while managing costs and risks.

In decentralized energy systems, even the smallest components bear the greatest responsibility. Nexans is at the forefront of advancing accessory technologies that enable uninterrupted power and reinforce system reliability in demanding environments. By focusing on robust design, embedded intelligence, and configuration based on system modeling, Nexans ensures that these silent connections deliver consistent reliability, contributing to the resilience of solar and wind installations.

Photo of Samuel Griot

Authors

Samuel Griot joined Nexans in 2021 as head of the electrical engineering department within Nexans Innovation, to lead a team of experts developing new innovative solutions for low, medium and high voltage applications in order to answer the future needs for the electrical grids. He was appointed early 2025 Innovation Solutions Director for the PWR Grid Market Division. He has a strong background in electrical grid architecture and switchgears. He holds a Master degree in electrical engineering from INSA of Lyon, France.

johan-burnier

Johan Burnier is a Business Development Manager in Renewable Energy at Nexans, based in Paris, France. With over 12 years of experience in the energy sector, Johan has transitioned from six rewarding years in International Project Management, where he worked on EPC contracts in Dubai and Scotland, to his current B2B commercial role. He specializes in 72kV accessories for Offshore Windfarm applications, focusing on market study, sales channel definition, and international customer relationship management.

Before his current role, Johan served as a Project Manager for Onshore Export cable systems, notably on the BEATRICE Offshore Wind Farm project, an international undertaking with a €250 million turnover. He also gained significant international experience as a VIE (International Volunteer Program) Project Engineer in Dubai, working on 400 kV underground electrical circuits. Johan holds an engineering diploma from ECAM LaSalle.

 

Smart Accessories: unlocking electrical grid reliability and performance
Electrification of tomorrow
25 July 2025
7 min
banner-smart-accessories

With electrification accelerating at an unprecedented rate, electrical grids built more than thirty years ago are now under tremendous strain. Many are outdated and struggle to handle increasing demand during extended periods while maintaining the expected levels of efficiency and reliability.

In this increasingly strained environment, every component of the grid matters. Yet, some of the most critical (and vulnerable) components often remain unnoticed.

 

While attention is often focused on cables and transformers, the most overlooked and failure-prone elements of electrical grids are the accessories that silently connect everything.

More than 70% of distribution grid failures occur at junctions; but most utilities still rely on inspections with limited visibility.

These hidden critical links are often buried beneath city streets and deep under the ocean floors, silently carrying power. When they fail, the consequences include costly repairs, extended downtime, and widespread service disruptions. Preventing this costly domino effect is a top priority for grid operators today.

So, why do these critical connection points fail in the first place, and more importantly, how can they be avoided?

Accessories: the hidden cause behind grid failure

It is often mistakenly assumed that electrical grid failures are due to faulty cables and transformers. But in reality, it is the accessories (cable connectors, joints, and terminations) that account for a disproportionate share of failures.

These components degrade over time due to thermal fatigue, mechanical stress, vibrations, moisture ingress, and, in many cases, improper installation practices such as misalignment or over torque. Pinpointing the location of a failure is notoriously difficult. Limited visibility and lack of diagnostic data make troubleshooting time-consuming and costly.

As an example, an MV cable connector failure can cost, on average, between €10,000 and €50,000 to repair.

3 reasons why accessory systems fail

These failure mechanisms underscore why accessories, despite their compact size, harbor a disproportionate share of the operational risk within medium-voltage grids. Yet their role extends well beyond reliability concerns alone, serving as critical enablers of performance, safety, and future-ready grid modernization.

smart-accessories-illustration

The rising strategic role of accessories in modern grids

Accessories are instrumental in powering mega data centers, lighting cities, and supporting transport systems. This strain is especially evident in older accessories, many of which were never designed to support today’s continuous and elevated load demands.

According to the European Network of Transmission System Operators for Electricity (ENTSO-E), over 60% of Europe’s grid components are more than 30 years old. These aging components are expected to deliver uninterrupted power in an environment where downtime is no longer acceptable.

 

The impact of aging components on electrical grids

Across Germany, Italy, and the Netherlands, up to 80% of medium-voltage cable faults stem from defective joints and splices, as reported by national utilities (Unareti Grid Fault Analysis, 2022).

Much like the telecommunications industry before it, the energy sector must now evolve toward real-time visibility, predictive fault detection, and continuous diagnostic intelligence to meet the demands of a modernized grid.

Smart Accessories: From Hidden Weak Links to Strategic Grid Resilience Enablers

To address these vulnerabilities and modernize grid maintenance strategies, accessories are now being elevated into intelligent assets.

Despite their modest size, accessories like joints and connectors are often the weakest links in grid infrastructure. Their vulnerability is compounded by harsh environmental exposure; yet, until recently, they have been treated as passive components.

That’s now changing. As utilities grapple with aging infrastructure and the rising cost of outages, accessories are being redefined as intelligent and predictive assets. Equipped with embedded sensors and connected into digital monitoring platforms, today’s smart accessories enable early fault detection and real-time performance insights, allowing operators to shift from reactive maintenance to proactive grid management.

Utilities adopting these technologies have already reported notable reductions in outage durations, emergency interventions, and overall operational expenditures.

The Technology Powering Smart Accessories

Transforming accessories from passive components into intelligent assets requires a new generation of technologies. These innovations empower operators with real-time visibility capabilities, allowing them to anticipate failures before they occur, rather than respond after the fact.

To meet these evolving expectations, manufacturers are now delivering advanced accessory systems featuring:

  • Smart joints, terminations, and connectors equipped with embedded sensors for voltage, temperature, and partial discharge (PD) monitoring
  • Predictive dashboards that combine historical data with live grid inputs to flag emerging risks
  • Seamless integration with digital twins, mobile diagnostics tools, and SCADA platforms for comprehensive grid visibility.

Together, these technologies are shifting maintenance strategies from reactive interventions to proactive, data-driven grid optimization, enabling faster diagnostics, more accurate root-cause analysis, and fewer unexpected outages.

But what makes these smart accessories possible? At the heart of this transformation are three enabling technologies, powering the shift from passive parts to intelligent, self-monitoring systems:

3 Innovative technologies powering smart accessories

Real-world impact: how utilities leverage smart accessories

Utilities that embed smart accessories within predictive diagnostics and installation traceability frameworks are achieving tangible performance gains:

  • A Nordic operator reduced fault localization times from 48 hours to under six hours, sharply reducing costly emergency interventions and, consequently, OPEX.
  • National Grid in the UK deploys partial discharge and thermal sensors in medium- and high-voltage cable systems to reduce unplanned outages and maintain lower SAIDI (National Grid Innovation Report, 2022).
  • Alliander (Netherlands) is deploying more than 3,000 Smart Cable Guard systems (recently partnering with Nexans) across its medium-voltage grid to tackle aging infrastructure and outage risk. Field data shows that each unit prevents over 6,000 customer minutes lost annually, with fault localization accurate within 1% of cable length. Following strong results from initial pilots, the rollout supports Alliander’s broader effort to lower SAIFI and SAIDI across a 40,000 km MV network.

 A Strategic Shift in Grid Management

The evolution of accessories from passive components to intelligent assets is reshaping how utilities manage and future-proof their grids. Smart accessories now play a strategic role in boosting reliability, extending component lifespan, and reducing operation costs.

As utilities confront the twin pressures of aging infrastructure and accelerating electrification, these solutions are becoming essential to predictive maintenance and resilient network operation. This marks a broader transformation, from static systems to intelligent, self-monitoring grids.

Nexans is helping lead this industry shift, providing advanced smart accessory systems and end-to-end lifecycle support that enable grid operators to anticipate, monitor, and optimize their networks with unprecedented precision and confidence.

Discover the full suite of Nexans’s Accessories

Photo of Samuel Griot

Authors

Samuel Griot joined Nexans in 2021 as head of the electrical engineering department within Nexans Innovation, to lead a team of experts developing new innovative solutions for low, medium and high voltage applications in order to answer the future needs for the electrical grids. He was appointed early 2025 Innovation Solutions Director for the PWR Grid Market Division. He has a strong background in electrical grid architecture and switchgears. He holds a Master degree in electrical engineering from INSA of Lyon, France.

Photo of Moussa Kafal

Moussa Kafal leads the Grid Reliability portfolio at Nexans, spearheading the development and global deployment of advanced solutions that enhance the performance, integrity, and resilience of power networks. Holding a PhD in Engineering and executive credentials from HEC Paris, he bridges deep technical expertise with strategic acumen to accelerate energy system transformation. Moussa oversees key initiatives across Europe, North America, LATAM, and APAC, positioning Nexans as a leading smart grid solutions provider in a rapidly evolving digital infrastructure landscape.

The Power of Certifying Training in Electrification Acceleration
Electrification of tomorrow
17 July 2025
6 min
banner-power-training

From aerospace to manufacturing, today’s leaders are no longer just providers of products. They are long-term partners involved in every phase of the customer journey, from design and deployment to diagnostics, support, and, increasingly, training.

Across industries, the way companies serve their customers is being redefined. Training has become a critical part of how companies reduce risk, ensure operational results, and build trust with those who rely on their technologies.

Customer experience starts with skills

In many sectors, performance depends as much on human precision as on technological advancement:

  • In aviation, simulation-based training helps crews stay prepared for complex scenarios
  • In advanced manufacturing, augmented reality tools guide workers through critical procedures
  • In financial services, AI-based coaching improves the quality of client interactions

These approaches reflect a shared belief that strong customer experience comes not only from great products, but from the ability of people to apply them correctly, consistently, and along the whole value chain, from the start to the end. Up-skilling is even more relevant in the energy sector.

The electrification challenge: complexity and consequence

As the global push for decarbonization accelerates, electrification has become the backbone of energy systems. Power networks today must integrate renewable energies and always more decentralized generation, leading to bi-directional flows and intermittent production. In the meantime, electrification and new customer needs are growing (electrical vehicules, heat pumps, AI development and related construction of datacenters, electro intensive industries…).

Grids must therefore be modernized and become Smarter. They also have to become more resilient against extreme weather events. Their vulnerability against human errors during installation has become more critical than ever.

According to ENTSO-E, more than 60 percent of Europe’s grid components are over 40 years old. In this context, the margin for error is shrinking. A single installation mistake can affect reliability, safety, and customer satisfaction, leading to delays, warranty claims, and long-term service costs.

The numbers speak for themselves:

  • 400 million euros are lost each year in Europe due to improper installation of cable accessories
  • Up to 50% of medium-voltage (MV) cable accessory failures are caused by installation errors
  • In the Netherlands, 12.5% of total SAIDI (System Average Interruption Duration Index) minutes are attributed to these issues
    (Source: EA Technology, Jicable 2023 E1-4; Review of Medium-Voltage Asset Failure Investigations, 2018)

These are not design flaws. They are execution problems. And they are preventable.

innovation-thumbnail

Why (certified) training is essential in electrification worldwide?

One of the root causes is a growing global shortage of qualified professionals in the grid sector. Across the energy industry, there is a bottleneck in the availability of skilled technicians able to install and maintain increasingly complex grid systems. This talent gap affects not only speed of deployment but also safety and long-term performance of states and industries. In many countries, there are not enough certified teams to meet infrastructure goals, particularly in fast-developing electrification markets. The result is clear: without widespread access to certified training, even the most advanced technologies remain vulnerable.

In many countries, certification must also carry formal recognition. In France, for example, certifications are expected to bear official accreditation such as CofracTM, ensuring that certification process is fair for all national stakeholders. QualiopiTM is also a well-recognized quality stamp to ensure training process meets national standards and is recognized by the wider market. These stamps not only validate training quality, they first and foremost bring a license to operate for grid installors while supporting professional mobility and technical accountability on the grid.

Training also closes the gap between system design and field reality. In today’s energy infrastructure, it serves three purposes: it transfers critical technical knowledge and workmanship, strengthens accuracy and speed on the ground, and supports a culture of accountability and excellence.

Measurable impact in the field

In recent assessments, teams that completed structured and certifying training programs showed:

  • A 58% reduction in Medium Voltage cable accessories failure rates
  • A 25% improvement in installation speed
  • A customer satisfaction rate of 97%
    (Source: Nexans Internal Impact Study, 2024)

These improvements are not theoretical. They directly affect grid resilience, budget predictability, customer satisfaction and trust.

Training for modernizing and expanding grids

As grids become more complex, training must adapt. This includes at Nexans:

  • Hands-on installation practice
  • Certification based on practical performance, not just theory
  • Partial discharge and AC withstand testing of i samples assembled during training
  • Language flexibility and local adaptations
  • Programs covering low, medium, and high-voltage applications, including renewables

Training today is not a static classroom experience. It is technical, tailored, and aligned with operational goals. In most cases, it also provides certification that is now increasingly necessary to operate and secure installations in compliance with industry standards.

The example of Nexans Certifying Training Services

In response to growing demand for skilled installation and maintenance teams and to a lack of certified technicians in most countries, Nexans has structured a comprehensive global training program. Delivered worldwide through eight centers located mainly in Africa, Middle East, Asia-Pacific and Europe including France and DOM-TOM, and supported by a dedicated team of 25 trainers and experts all over the world (including the US and Latin Americas), the program is designed to reflect the diversity and complexity of real-world electrification projects.

In 2024 only, over 2,800 professionals took part in training sessions offered in seven languages and tailored to more than 15 voltage levels and accessory types. The curriculum spans low-, medium-, and high-voltage systems, as well as renewable applications, with flexible, on-demand modules to support different phases of a project.

Each session combines technical theory with hands-on practice. For the most demanding applications, installed samples are tested under real conditions using partial discharge and AC withstand protocols, and certification is awarded based on demonstrated results, not just attendance (in France, the certification process is COFRAC accredited).

Beyond Training: Supervision of Installation

In complex projects, reliability can be such a stake that on top of installer training, supervision of operation can be the best way to ensure best in class execution of the installation. In such cases support can be proposed on site by a technical expert or trainer, or if the project is remote, mixed-reality tools.

That is where tools like Microsoft HoloLens 2 come in. This headsets and glasses device allow a remote expert to guide a technician in real time, through visual overlays and live communication.

At Nexans, such mixed reality solutions are directly integrated into training sessions and remote support services, offering installers immediate, hands-free assistance in the field. This approach enhances installation quality and optimizes project execution, especially in isolated locations such as offshore wind farms or rural substations.

The success of electrification worldwide depends not only on smart systems, but on the right-skilled people who install and operate them. Training gives those people the skills and confidence they need to deliver reliability, safety and consistency to the grid networks.

Companies that invest in training are doing more than reducing technical risk. They are building trust, reinforcing performance, and redefining what great customer experience looks like. In the race toward a sustainable energy future, human expertise is what brings every connection to life.

As an innovation-driven leader in the electrification sector, Nexans continues to pioneer advanced training and supervision solutions that help build the grids of tomorrow.

Discover our Certified Trainings with “Skills Power“

laurent-keromnes

Author

Laurent Keromnes, graduated from ENSCPB Bordeaux in 1997 (Physics and Chemistry), started his career as a chemical engineer in Arkema, the French chemical company. He spent there almost 11 years developing PVC foams and then organic peroxides dedicated to polymer crosslinking.

Since 2011, he moved to Nexans (cable manufacturer) to work on cable development. After 5 years in the Research Center he moved to another position in the company, as a Business development engineer for buried cables in power networks. He is involved in standardization as a TC20 member at AFNOR, and member of several Technical Committees for cables at french SYCABEL.

From early 2024 he is now in charge of Nexans training centers involved in Medium Voltage (MV) accessories installation for Power Grid Business Division.