The grid revolution: how superconductors will power tomorrow and ensure safe and efficient energy transition
Electrification of tomorrow
15 September 2025
11 min
Superconductivity and EV, in cities

Right now, at least 3,000 gigawatts of renewable energy projects are sitting in connection queues worldwide, including 1,500 gigawatts in advanced stages. That’s already five times the solar and wind capacity added in 2022 – and current data only covers half of it.

So, if sustainable energy generation isn’t the problem, then what is? The true obstacle lies in moving that energy from where it’s produced to where it’s needed – and these bottlenecks are fast becoming one of the greatest risks to achieving net-zero targets, energy security, and climate resilience.

What the energy transition requires is infrastructure that matches the scale and urgency of the challenge. Enter superconductors, a game-changing (super) solution capable of aligning grid capacity with ambition.

The infrastructure challenge

As demand from electric vehicles, hydrogen production, and heating and cooling systems accelerates, grids face unprecedented pressure. However, much of today’s cable network—particularly in Western Europe, North America, and Japan—is already decades old, never designed for the loads we are seeing today.

Take, for example, a distribution system operator in New York with a cable network that’s over 50 years old and operating near capacity. Adding new loads from EVs and heat pumps not only accelerates the aging of existing cables but also limits the ability to connect new renewable generation due to thermal and voltage constraints. Replacing or upgrading these cables using conventional high-voltage solutions requires extensive excavation in urban areas, where underground space is already crowded with telecommunications, water, gas, and transport infrastructure.

Even when installation is technically possible, environmental restrictions, lane rental charges, and traffic management fees can increase project costs by hundreds of thousands of dollars. Land acquisition for wider cable routes compounds the challenge, particularly when existing rights-of-way cannot accommodate the spacing needed for conventional cables, which require significant separation to manage heating effects and electromagnetic interference.

Meanwhile, safety and reliability requirements keep rising. Networks must deliver electricity without cuts, breakdowns, cascading failures, or blackouts. They need to handle fault currents that can damage critical assets like transformers and switchgear. And as public expectations grow, networks must minimize electromagnetic interference, reduce CO₂ emissions, recycle obsolete assets responsibly, and reassure communities about safety.

This scenario is playing out in major cities worldwide, while rural areas face their own infrastructure constraints. Meeting electrification needs at scale will require massive infrastructure upgrades: grids will need roughly 80 million kilometers of new or refurbished cable by 2040 – and conventional systems alone cannot keep up with demand.

data center

Data centers: a core challenge

In addition, data centers have emerged as the core of the digital infrastructure, operating with extensive computational power, storage capacities and energy requirements. However, as their footprint and power consumption increase, significant challenges arise in terms of efficiency, heat management, land utilization, and environmental impact. The demand for digital services is soaring. As the digital economy continues its exponential growth, data centers are becoming the backbone of global digital infrastructure. Hyperscale and gigawatt-scale data centers are emerging to meet soaring compute demands, especially driven by AI, cloud services and advanced analytics. These next-generation facilities are pushing the limits of traditional electrical infrastructure, both inside and outside the data center footprint.

Power requirements are rapidly escalating, with new hyperscale data centers being designed for power capacities approaching or exceeding 5 gigawatts — an order of magnitude above previous-generation facilities. This scale introduces critical challenges in power delivery, thermal management, land use, carbon emissions and capital investment. The current reliance on conventional copper-based cabling systems is increasingly unsustainable.

The bottleneck in numbers

3,000 GW

of renewable energy projects are stuck in grid connection queues worldwide – 5x the solar & wind capacity added in 2022

1,500 GW

of that total are in advanced stages

80m km

of new or refurbished cable needed by 2040 to meet electrification targets

About

10%

of electricity is lost during transmission over long distances – equivalent to roughly 180 TWh per year in Europe

> 5 GW

power capacities of new hyperscale data centers — an order of magnitude above previous-generation facilities. This scale introduces critical challenges in power delivery, thermal management, land use, carbon emissions and capital investment

The superconducting solution

High-Temperature Superconducting (HTS) cables and fault current limiters represent a fundamentally different approach to power transmission. The technology exploits the complete loss of electrical resistance that occurs in certain materials at extremely low temperatures, known as one of the key properties of superconductivity.

HTS materials require cooling to approximately -200°C, typically with liquid nitrogen. “High temperature” here means relative to the first generation of superconductors, which requires temperatures below -243°C to operate. The liquid nitrogen circulates in cryogenic envelopes, a thermally-insulated jacket that surrounds the cable. Liquid nitrogen is relatively inexpensive, environmentally harmless, and easier to manage than many industrial coolants. More importantly, the energy saved by eliminating transmission losses exceeds the energy required to maintain the cryogenic environment.

The electricity flowing through your home right now has traveled hundreds of miles of conventional resistive cables, losing roughly 10% of its power along the way. That waste, about 180 TWh annually in Europe alone, is enough to power three major cities. HTS cables requires 10 times less energy to supply electricity.

Why choose superconducting cables?

For modern grids, HTS systems offer huge advantages over conventional alternatives, especially in dense urban environments:

  • Space efficiency and economics: HTS cables generate no heat or electromagnetic fields at any load along the cable route, so phases need no separation. Cables can be buried at any depth and close to other multi-energy network without expensive tunneling or specialized conduits, shrinking rights-of-way to up to one-tenth the width of conventional systems. In cities where land costs tens of thousands per meter, this benefit alone is game-changing.
  • Enormous transmission capacity: One HTS cable can handle over 3 gigawatts. Fewer circuits and minimal substation upgrades are needed, while retrofits can multiply tunnel capacity without major construction with minimal electrical loss if not zero in Direct Current.
  • Smaller environmental footprint: Less excavation and reduced permitting complexity can result in shorter project timelines and less public opposition.
  • Resilience: Fully shielded, superconducting cables are weatherproof, highly secure, and nearly free of stray electromagnetic fields – meaning power availability is protected even if part of the grid is disrupted.

It’s a win-win(-win-win).

Superconductivity and train stations, in cities, data centers

Grid transformation beyond capacity

Unlike conventional grids that struggle with distributed energy resources like rooftop solar, fuel cells, and remote wind parks, HTS systems enable networks to absorb energy from any source and facilitate market-driven power flows.

Superconducting Fault Current Limiters (SFCLs) is invisible in the network during normal conditions, and automatically transition to a highly resistive state when faults occur, limiting dangerous currents and reducing the level of short circuit current to be supported by all the equipment in the substation before circuit breakers activate. This technology is using intrinsic behavior of superconductors and is not requiring active control or monitoring.

This technology supports the move to smarter, more flexible grid systems where demand can adjust with multiple supply sources. Urban power densities can increase dramatically with minimal public disruption, thanks to SFCL that can absorb the increase of short circuit current induced by the addition of new sources and new load in the network.

For electric vehicle charging infrastructure, the capacity and efficiency advantages become particularly important as charging speeds increase and deployment scales up. Industrial electrification processes that require large amounts of reliable power can be supported without the massive infrastructure investments that conventional systems would require.

For data centers, this unlocks transformative advantages across power transmission, distribution, and infrastructure design. Delivering efficient and reliable power in limited spaces is a major industry concern, and superconducting cable systems offer a promising solution. With zero electrical resistance, ultra-high current capacity and a compact footprint, HTS cables can radically simplify power infrastructure, reduce thermal loads and support the broader goals of sustainability and electrification. Superconducting cables (High-Temperature Superconducting (HTS) systems)represent a transformative solution for power transmission within and around large-scale data centres. These advanced conductors can transmit electricity with virtually zero resistance, eliminating the energy losses and heat generation that are inherent to traditional copper-based systems.

Smarter, denser grids

  • Any source, anywhere: HTS cables handle rooftop solar, fuel cells, remote wind parks.
  • Automatic protection: SFCLs limit fault currents instantly, no active controls needed.
  • Smart, resilient grids: SFCLs allow the increase of supply and demand, improving reliability and supporting integration of distributed or remote generation.
  • Electrification ready: Scales EV charging and industrial loads without massive new builds.

Ready for a superconducting grid revolution?

Infrastructure demands, technological maturity, and a strong business case are aligning to support widespread HTS adoption. Companies like Nexans, with facilities across Germany, France, and Norway, have developed cutting-edge expertise across the entire superconducting technology stack and are contributing to international standards that will accelerate global rollout.

The question isn’t whether superconducting technology will transform electrical grids, but how quickly utilities, governments, and investors will recognize the opportunity. Grid operators who move early will gain significant competitive advantages in efficiency, reliability, and capacity. Those who wait may find themselves constrained by the very infrastructure limitations that superconducting technology is designed to solve.

Photo of Yann Duclot

Author

Yann Duclot is Acceleration Units Director at Nexans. In this role, he oversees the Nexans Acceleration Units made of 2 companies centered around the Energy Transition: Nexans Solar Technologies (NST) and Nexans Machinery, Cryogenics and Superconductivity (MCS).  Yann leads a team of 65 people based in France and Germany centered around the engineering, manufacturing of new and disruptive technologies (superconductivity, cryogenics, solar trackers) in order to accelerate our growth in high potential markets for the energy transition.

Yann began his career at Nexans in 2000 and, with a brief interruption at Cavotec as Chief Marketing Officer, has now been part of the company for 14 years. With over 25 years of experience in business unit management, organizational transformation, and innovation leadership, Yann has been instrumental in scaling up business activities and driving the company’s growth and profitability. He holds a Master of Science from Grenoble Ecole de Management (GEM).

Explore more on superconducting innovation

Continue exploring how superconducting technology is reshaping the energy landscape with our related articles — from groundbreaking systems redefining power grids and subsea connections enabling the energy transition, to advances driving the next generation of rail networks and sustainable, high-performance data centers.

Spotlight on Superconductivity
  • Article

    Serie : Spotlight on Superconductivity

    data-centers-and-superconductivity_thumbnail

    Data centers of the future: powered by superconducting cables for scalable and sustainable growth

    Electrification of tomorrow

    19/11/2025

  • Article

    Serie : Spotlight on Superconductivity

    superconductivity-rails-and-data-thumbnail-2

    Superconductivity: Powering tomorrow’s rail and data infrastructure

    Electrification of tomorrow

    29/10/2025

  • Article

    Serie : Spotlight on Superconductivity

    subsea-superconductivity-cables-thumbnail

    Superconductors beneath the waves: Powering the energy transition

    Renewable energies

    07/10/2025

  • Article

    Serie : Spotlight on Superconductivity

    superconductivity-grid-thumbnail-2

    Superconducting systems: The game-changing solution for tomorrow’s energy grids

    Electrification of tomorrow

    02/10/2025