Superconducting systems: the game-changing solution for tomorrow’s energy grids
Electrification of tomorrow
03 October 2025
7 min
superconductivity-grid-banner

The urban grid under pressure

Imagine plugging all your brand-new household appliances into a century-old electric system. The infrastructure is globally aging faster than it is being replaced or upgraded. There is a high risk that system will fail – and the same applies to our urban electrical grids. According to the United Nations (UN), 55% of the world’s population lives in urban areas today, a share projected to rise to 68% by 2050. And these communities demand uninterrupted, high-quality electricity with minimal faults or downtime.

Meanwhile, growing adoption of electric vehicles, heat pumps, and other low-carbon technologies—combined with smaller household sizes—is fueling a surge in both residential and industrial electricity consumption. At the same time, much of the existing electrical infrastructure is aging and operating near capacity limits, with conventional cables and distribution systems originally designed for earlier, centralized energy models now increasingly strained by modern, decentralized power flows and higher load demands.

In other words, there is a growing mismatch between what energy grids can deliver and what modern cities need.

Several systemic constraints stand in the way of modernizing urban grids efficiently:

  • Space limitations: Conventional cabling systems require substantial space and specialized equipment – but underground corridors are already saturated with existing infrastructure, making new cable routing extremely difficult.
  • Escalating costs: Environmental restrictions, land acquisition, and rental fees can add hundreds of thousands of dollars to projects.
  • Grid bottlenecks: Environmental and proximity constraints severely limit the connection of new renewable energy sources, creating a barrier to the very transition these systems are meant to support.
  • Unpopular disruption: Construction works required to install new cables often go with noise pollution, traffic congestion, and environmental concerns leading to increasing public opposition.
  • The reality is clear: succeeding in the energy transition requires radically rethinking electrical infrastructures with innovative technologies that balance growing demand, system resilience, and urban liveability. Enter superconducting systems.

How superconducting technology solves urban grid challenges

HTS cables: Zero-resistance transmission

High Temperature Superconducting (HTS) technology draws its transformative power from its core property: superconductivity. With virtually zero electrical resistance, these cables can carry extraordinarily high currents in much less sections that copper or aluminum conductors. In fact, a single 17-centimeter-diameter cable can handle up to 3.2 gigawatts à high voltage– that’s roughly the output of three nuclear reactors and several 100 MW underground at medium voltage, able to secure the supply of big cities without adding new high voltage lines.

This absence of heat generation eliminates the need for wide thermal clearances and ventilation systems, allowing HTS systems to be installed in simple trenches rather than purpose-built tunnels. Their compact footprint means that the required corridors are up to ten times narrower than for conventional systems. They also generate no electromagnetic interference and emit no external magnetic field, making them safe neighbors to other infrastructures in these confined spaces.

Beyond the installation advantages, HTS systems provide enormous operational flexibility. A 400-kilovolt conventional system can be replaced with a 132 or 275 kV-kilovolt superconducting system without losing capacity at lower cost mainly due to the saving of large 400 kV transformers in the substation—and because the cable system including ancillary systems is modular, the same cable design works equally well for compact urban networks and long-distance transmission.

SFCLs: Instantaneous fault protection

Superconducting properties can also be used to mitigate overcurrent, almost instantaneously. Superconducting Fault Current Limiters (SFCLs) provide vital protection against fault currents that can damage critical assets such as transformers and switchgear. In the event of a short circuit or fault condition, SFCLs instantly and automatically limit excessive current without the need for mechanical intervention or voltage disturbance. SFCLs use superconductors’ intrinsic properties to transition from zero-resistance to resistive state within milliseconds, limiting fault current before it damages  equipment on the same branch. SFCLs can be integrated and connect to any electrical system — offering enhanced network reliability, optimized infrastructure protection, and reduced equipment aging from thermal stress.

 

Proven success in real-world applications

Multiple operational projects demonstrate the technological maturity and transformative potential of superconducting systems in diverse urban environments. Here’s a look at three:

AmpaCity Project, Germany

Nexans manufactured and deployed in 2014 (tbc) the world’s longest superconducting cable link, featuring a three-phase 10kV HTS cable with 40 MVA capacity instead of a 110 kV conventional circuit and an integrated superconducting fault current limiter. The seven years of continuous service have proven the long-term reliability of superconducting technology.

LIPA Project, United States

This project showcased superconducting capabilities in American electrical infrastructure. In 2008 and 2012 (tbc), Nexans developed and delivered complete 138 kV AC superconducting cable systems, including the cable core, cryogenic envelope, and terminations, while supervising installation and commissioning.

Best Paths Project

Nexans designed and built a pioneering 320 kV DC superconducting loop comprising a monopole cable of 30-meter carrying 10 kA current for a nominal capacity of 3.2 GW. The project included comprehensive voltage testing at 1.85× the rated voltage (up to 592 kVDC) and impulse testing. This achieved the world’s first qualification of a full-scale 320 kV HVDC superconducting loop on a test platform, featuring a 6.4 GW HVDC circuit (2 monopoles), representing the highest power transmission capability demonstrated to date.

These concrete achievements demonstrate that superconductors have evolved from experimental technology to an industrial solution set to transform urban electrical transmission and distribution.

 

Building tomorrow’s grid

With operational projects proving their reliability and cities facing mounting pressure to electrify rapidly, superconducting systems represent more than just an upgrade; they’re a fundamental shift in how urban grids can be designed and deployed.

Rather than fighting space constraints and community resistance with conventional solutions, utilities can now build smaller, quieter, and more efficient networks that actually support the energy transition they’re meant to enable. Superconducting systems give cities a practical pathway to meet surging electricity demand while achieving decarbonization goals – a future-ready backbone for resilient and sustainable urban power.

Picture of Beate West

Authors

Dr. Beate West is Head of Engineering for Superconducting Systems in Hannover. She joined Nexans in 2010 as research engineer. She is responsible for the design of superconducting cables and fault current limiters.

Beate has a diploma and a Ph.D. in physics from the University of Bielefeld.

arnaud-allais

Dr. Arnaud Allais is Chief Technology Officer Machinery, Cryogenic and Superconducting Systems at Nexans. Arnaud is a globally recognized authority in advanced electrical grid technologies  and high temperature superconductivity (HTS). With over two decades of experience, he leads innovation and strategic development in advanced superconducting systems that are shaping the future of energy transmission.

Arnaud earned his Ph.D. in Materials Engineering from the School of Mines of Paris, in collaboration with Alcatel, where he focused on modeling Powder-in-Tube Bi2223 superconducting wires. He also holds an engineering degree in Energy and Materials from the School of Engineering in Orléans, France. Throughout his career at Nexans, Arnaud has held several key leadership roles, including: Director of the Nexans Research Center, and R&D Program Director at the SuperGrid Institute – a joint R&D venture with GE, Alstom, EDF, and leading French universities.