The Invisible Backbone: 5 Unsung Innovations Keeping Wind and Solar energy Alive
Renewable energies
22 August 2025
6 min
invisible-backbone-banner

Imagine standing at dawn under a remote wind farm, the turbines slicing through salty air, miles from the nearest city. What guarantees these giants deliver resilient power to the grid, day after day, through all-weather events? The answer isn’t obvious, or visible. It’s the unspoken link: the connecting accessories quietly holding everything together.

As the transition to clean energy accelerates, wind and solar are no longer marginal contributors; they are quickly becoming the backbone of the renewable energy transition.

According to the IEA’s updated Net Zero Roadmap (2023), to reach net-zero energy sector CO2 emissions, over 70% of new energy capacity must come from wind and solar farms by 2050. But scaling up to meet this target is only half the battle. Ensuring wind and solar installations operate reliably across oceans, deserts, or mountains is just as critical.

Wind and solar farms are often built in some of the world’s harshest and most remote locations. Once installed, their components must function for decades with limited human access and under constant exposure to salt, sand, heat, and vibrations.

While most attention is focused on turbines and electrical panels, equally critical elements of system performance lie in the accessories that connect everything.

 

invisible-backbone-illustration

Accessories: the critical link to renewable energy reliability

Cable accessories (joints, terminations, and connectors) are crucial to the reliability of solar and wind energy. In fact, up to a third of breakdowns in these enormous installations start not in the blades or panels, but in their connections (WindEurope O&M Benchmarking, 2022). It’s as if a single loose shoelace could halt a marathon. For the industry? That means billions in lost power, unexpected outages, and missed climate targets that affect us all. These vital connection components may be invisible, but their performance has a direct impact on grid uptime, maintenance costs, and return on investment.

Like any high-performance system, such as long-haul aviation, offshore oil rigs, or space exploration, solar and wind systems demand components that are robust, modular, and remotely diagnosable. In a utility-scale wind or solar energy farm, a single weak link can compromise system integrity and interrupt power delivery. Which is why the industry is shifting from passive, one-size-fits-all accessories to tailored, intelligent component systems that anticipate downtime risks, extend infrastructure lifespan, and reduce overall operating costs.

The 5 grid accessory innovations leading this shift are: modular 145kV connectors for offshore wind farms, pre-assembled cable systems for grid electrical systems, sensor-based components, modular cable kits, and high-performance polymers and sealing materials.

Five accessory innovations redefining reliability in wind and solar energy farms.

1. Offshore-ready connectors engineered for high-voltage resilience

Offshore wind farms face unique conditions: constant motion, salt-laden air, and high-voltage transmission requirements. Conventional connectors can corrode, loosen, or degrade over time.

The innovation: Compact, modular 145 kV connectors designed for offshore wind applications are enabling more efficient transmission from increasingly powerful turbines. Their compact design facilitates installation in constrained environments while minimizing bending forces on connected equipment such as switchgear or transformers. Engineered for long-term performance, they feature high resistance to corrosion, vibration, and pressure, making them well-suited for the harsh and demanding conditions of subsea and offshore environments.

The result: Fewer failure points, longer service intervals, and enhanced safety in locations where unplanned repairs are difficult and expensive.

2. Pre-connected cable systems that minimize human error

In remote or high-risk locations, every hour spent on electrical installation increases exposure and cost. Grid technicians often face high levels of fatigue, while installation errors such as overtightening or misalignment can compromise long-term performance.

The innovation: Factory-assembled, tested and pre-connected cable systems minimize on-site handling, which helps reduce human error and accelerate installation in challenging environments.

The result: Safer, faster installations and greater reliability from day one, especially important in demanding environments.

3. Sensorized accessories that detect failure before it happens

Failure in a joint or termination often begins invisibly due to exposure to thermal fatigue, mechanical stress, vibrations, and moisture ingress. In remote wind and solar farms, these silent failures can go undetected until a power outage occurs.

The innovation: Accessories equipped with built-in sensors that continuously monitor internal conditions such as temperature and insulation health. The sensor-generated data is directly integrated with Supervisory Control and Data Acquisition (SCADA) systems and predictive operation and maintenance (O&M) schedules, enabling smart monitoring and intelligent diagnostics. Ørsted, the global leader in offshore wind and one of the world’s largest renewable energy companies, integrates cable diagnostics and performance monitoring into its offshore substations to support early fault detection and reduce unplanned downtime.

The result: Issues are detected early, enabling preventive maintenance instead of reactive repairs. This significantly reduces downtime and helps operators move toward fully digital, condition-based asset management.

4. Modular connector kits adapted to site-specific layouts

Each solar and wind farm configuration is unique.  Varying terrain, layout constraints, and project scale all affect how cable accessories are planned and installed.

The innovation: Modular connector kits tailored to site-specific layouts are now helping reduce errors and delays on large renewable projects. Each wind or solar farm comes with its own constraints (terrain variations, equipment spacing, layout geometry)—which can complicate on-site installation. To streamline this process, system modeling tools are used upstream to configure customized kits of pre-assembled connectors, adapted to the physical layout and routing paths of each site.

The result: This modular approach, inspired by practices used in offshore wind and utility-scale solar projects, ensures faster, safer, and more reliable installations, especially in remote or hard-to-access environments where technician time is limited and rework is costly.

5. Materials that resist decades of environmental stress

UV exposure, salt spray, sand, moisture ingress, hot ambient temperature and thermal cycling are harsh realities for wind and solar installations.

The innovation: High-performance polymers (such as EPDM Material) and sealing materials that resist abrasion, extreme temperature variations, and long-term weathering. These components are engineered to maintain integrity under the toughest environmental conditions, whether buried, exposed, or submerged.

The result: Accessories that withstand years of exposure without degradation, helping ensure system stability over time. Offshore wind developers now utilize vibration-tolerant junction systems to extend the lifespan of accessories in one of the harshest operating environments. As renewable infrastructure expands into increasingly extreme terrain and climate zones, long-lasting materials are proving crucial to performance and return on investment.

Innovative accessory technologies for a more resilient wind and solar energy future

As wind and solar energy take center stage in the global energy mix, connecting accessories must evolve to meet the demand for robust components that are adapted to extreme environments. Innovative accessory technologies are transforming once-passive components into intelligent, tailored, and long-lasting solutions that improve the system-wide reliability and cost-effectiveness of large-scale wind and solar farms.

Smart accessories, equipped with embedded diagnostics, connected to SCADA systems, and optimized through system modeling, are helping operators meet performance expectations while managing costs and risks.

In decentralized energy systems, even the smallest components bear the greatest responsibility. Nexans is at the forefront of advancing accessory technologies that enable uninterrupted power and reinforce system reliability in demanding environments. By focusing on robust design, embedded intelligence, and configuration based on system modeling, Nexans ensures that these silent connections deliver consistent reliability, contributing to the resilience of solar and wind installations.

Photo of Samuel Griot

Authors

Samuel Griot joined Nexans in 2021 as head of the electrical engineering department within Nexans Innovation, to lead a team of experts developing new innovative solutions for low, medium and high voltage applications in order to answer the future needs for the electrical grids. He was appointed early 2025 Innovation Solutions Director for the PWR Grid Market Division. He has a strong background in electrical grid architecture and switchgears. He holds a Master degree in electrical engineering from INSA of Lyon, France.

johan-burnier

Johan Burnier is a Business Development Manager in Renewable Energy at Nexans, based in Paris, France. With over 12 years of experience in the energy sector, Johan has transitioned from six rewarding years in International Project Management, where he worked on EPC contracts in Dubai and Scotland, to his current B2B commercial role. He specializes in 72kV accessories for Offshore Windfarm applications, focusing on market study, sales channel definition, and international customer relationship management.

Before his current role, Johan served as a Project Manager for Onshore Export cable systems, notably on the BEATRICE Offshore Wind Farm project, an international undertaking with a €250 million turnover. He also gained significant international experience as a VIE (International Volunteer Program) Project Engineer in Dubai, working on 400 kV underground electrical circuits. Johan holds an engineering diploma from ECAM LaSalle.