Blog Posts

  • Energy

    Frank Schmidt Apr 22, 2020

    Meeting the Megacity Challenge – with Superconductors

    The Covid-19 crisis is having a major impact on electricity demand. Yet the long-term trend is towards higher consumption – particularly in cities. Could superconducting cables help DSOs to meet rising demand?

  • Energy

    Jean-Maxime Saugrain Mar 25, 2020

    Standby for Superconductors

    Superconductors were once the stuff of science fiction. Now they’re transforming the way electricity is delivered.

  • Energy

    Jérôme Fournier Mar 3, 2020

    The Future is Electric

    The ambition is huge. By 2050, Europe intends to be the world’s first climate-neutral continent. To achieve this, renewable generation will need to replace the electricity currently produced using fossil fuels. This must be achieved while catering for a rapid increase in global electricity demand, which is expected to rise by more than 60% over the next 20 years.

  • Energy

    Julien TRUFLANDIER Oct 10, 2019

    Oil, Gas & Chemicals projects: 5 key criteria for choosing the right cabling solution

    In the context of growing concern regarding the future of fossil fuels and ongoing commodity price fluctuations, cost control and optimization remain crucial for the Oil, Gas and Chemical industry

  • Energy

    Bjørn Sanden Sep 30, 2019

    The King of long distance

    For decades, high-voltage direct current (HVDC) mass impregnated (MI) cables have been the preferred solution for long-distance subsea power transmission