Nexans power umbilicals will play critical role in Ormen Lange Phase 3 project

Nov 28, 2019
Nexans power umbilicals will play critical role in Ormen Lange Phase 3 project

Nexans power umbilicals will play critical role in Ormen Lange Phase 3 project

  • Nexans will supply 240-km power umbilicals to power and control an innovative subsea multiphase compression system to extend the production life of Norway’s second-largest gas field. 
  • The power umbilicals will be manufactured in Nexans factory in Halden, Norway, and installed in 2023 by Aurora, the new Nexans cable-laying vessel.

Paris La Défense, November 28, 2019 — Nexans announced today an award by OneSubsea®—the subsea technologies, production and processing systems division of Schlumberger—for the design, manufacture and supply of two 120-km power umbilicals for a subsea multiphase compression system. The system will help extend the production life of the Ormen Lange field, Norway’s second-largest gas field that currently supplies 20 percent of the UK’s gas needs.

Located in the Norwegian Sea, the Ormen Lange gas field produces about 70 million cubic meters of gas a day that is piped to the onshore Nyhamna processing plant. It is then purified and transported to the UK through one of the world’s longest subsea pipelines, which covers about 1,200 km.

The OneSubsea multiphase compression system is an innovative technology developed to boost the gas pressure. OneSubsea and its Subsea Integration Alliance partner Subsea 7 are supplying and installing two 16-megawatt (MW) subsea compression stations tied into existing manifolds and pipelines at a water depth of 850 meters. The system will be powered and controlled from the Nyhamna onshore gas processing plant, located 120 km away from the subsea location.

Nexans is delivering the power umbilicals that will integrate all the 52-kV electrical power, hydraulic and fiber optic elements required to power and control the compressor station.

“ We are delighted that OneSubsea has awarded us the turnkey power umbilical contract for this ground-breaking subsea multiphase compression system. It is a further confirmation that Nexans is at the forefront of umbilical technology. It is also especially pleasing to have further involvement with the Ormen Lange gas field as we were responsible for the umbilicals for the first stage in 2007, which are still supporting the operations . ”

Vincent Dessale

Nexans Senior Executive Vice President for the Subsea and Land System Business Group

The Ormen Lange power umbilicals will be designed and manufactured by Nexans Norway specialist facility in Halden. Delivery and installation by the new Aurora cable laying vessel is scheduled for 2023.

 

OneSubsea is a mark of Schlumberger.

Your Contact

Angéline Afanoukoe

Press Relations

Aurelia Baudey-Vignaud