LAN - Data Centre

Nexans simplifies data centre network monitoring and scale-up with the launch of LANsense AIM and new high-density copper & fibre solutions

Mar 12, 2019

  • Nexans launches its new LANsense® Automated Infrastructure Management (AIM) solution for port to outlet network monitoring and optimisation
  • During Data Center World 2019, the Group will present its cutting-edge LANmark® ENSPACE ultra high density fibre solution and Slimflex copper Category 6A solution aimed at minimising footprint and maximising scalability.
  • Nexans will also showcase its flagship TITANEX® power cable suitable for all mobile and fixed installations.

Paris La Défense, March 12, 2019 – As new trends such as 5G and edge computing put more strain on data centres, the race for efficiency, reliability and scalability continues. To help data centres effectively address their physical layer-related challenges, Nexans launches new cutting-edge solutions at the 11th edition of Data Centre World 2019, UK’s largest gathering of data centre expertise. The new solutions presented by the Group include LANsense AIM software for network monitoring, LANmark ENSPACE high-density fibre solution and Slimflex Cat. 6A high-density copper solution.

LANsense AIM: get clear instructions from port to outlet

LANsense monitors, manages and optimises network capacity remotely and more efficiently. Data Centre managers can trace circuits end-to-end, flag disconnects, find available rack space and make sure redundant and load balancing circuits are connected.

 

LANmark ENSPACE fibre: make room for scalability

In a modern data centre there is limited space for passive cabling. LANmark ENSPACE solution increases the number of connections in 1U by 50%. ENSPACE panels come with three individual sliding trays per ‘U’ allowing 144 LC connections in 1U and up to 576 connections in a 4U.

Slimflex Cat 6A Copper: achieve double density in data centres

Nexans' Slimflex Category 6A solution saves up to 50% space in data centre installations[1]. This new copper range consists of a 48-port panel, Slimflex cords and Cat 6A connectors. Once installed the result is a neat and cleaned up high density installation.

In addition to its data transmission technology, Nexans will showcase its flagship TITANEX® power cables. For more than 50 years the TITANEX® cable range has been recognized as the industry-leading solution for all mobile and fixed installations in industrial environments, including data centers.

The power cable is highly robust but flexible enough to cope with the restrictions of a data centre. It withstands high operating temperatures up to 90°C and has excellent mechanical resistance to impacts. TITANEX® is easy to work with, even in large cross sections. The cable can comprise up to 36 cores, with 1 to 630 mm² cross section.

Footnote

[1] Compared to standard Category 6A panels

Your Contact

Angéline Afanoukoe

Press Relations

Ksenia Kanareva

Press relations

Michel Gédéon