Case study

Maritime Link

  • LIEU
    Canada
  • PARTENAIRE
    Emera Inc.
  • MARCHE
    Réseaux d'énergie - Sous-marin

About the project

The Maritime Link is a 500 MW high voltage direct current (HVDC) that transport clean, renewable and reliable electricity from Newfoundland and Labrador to Nova Scotia and other energy markets in Canada and the North-eastern United States. For the first time in its history, the island of Newfoundland is connected to the North American transmission system. The Maritime Link also provide Nova Scotia with new access to clean renewable energy to offset coal fired generation and meets more stringent Canadian emissions requirements. The project included two 170 km subsea cables across the Cabot Strait, with almost 50 km of overland transmission in Nova Scotia and close to another 300 km of overland transmission on the island of Newfoundland.

Nexans' solution

Nexans designed, manufactured and installed two 200 kV HVDC power cables that spanned a subsea distance of approximately 170 km. Nexans supplied approximately 340 km of mass impregnated (MI) HVDC subsea and land cables together with fibre optic elements, transition joints for the sea and land cables, joints and terminations. 
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
Vous disposez d’un droit d’opposition à ce que les données à caractère personnel vous concernant fassent l’objet d’un traitement et/ou à ce qu’elles soient utilisées à des fins de prospections, notamment commerciales

Merci!

Merci pour votre message. Nous prendrons contact avec vous dans les plus brefs délais.

Erreur

Une erreur s'est produite. Veuillez réessayer.

Fermer