Nexans achieves two world records for deepest and longest 420 kV XLPE submarine cable system for Norway’s BKK grid connection

90 km XLPE cable system has just been installed to reinforce the grid in western Norway to meet growing demand for electricity

Paris, June 6, 2016 – BKK Nett AS, the Norwegian power company based in Bergen, will soon be the operator of a recording breaking subsea power link as Nexans just completed a project to install the world’s longest and deepest 420 kV XLPE (cross-linked polyethylene) insulated submarine cable system. In a turnkey project worth around 75 million euros to reinforce the grid in western Norway, Nexans has delivered 90 km of 420 kV AC XLPE cable. This contract fulfils Nexans’ vision of helping to meet the growing global demand for electricity.

Nexans achieves two world records for deepest and longest 420 kV XLPE submarine cable system for Norway’s BKK grid connectionThe new power link, comprising three single core cables in parallel, runs between Mongstad and Kollsnes, crossing two fjords: Hjeltefjorden and Lurefjorden. At its deepest point, the cables were installed at 390 m, making this both the world’s deepest 420 kV XLPE system, and longest at this depth, with a length of 22 km.

The cable system for the two fjords are manufactured, delivered and installed by Nexans. The cables were laid by Nexans’ cable laying vessel, C/S Nexans Skagerrak. In the near-shore areas, the cables were mainly protected with HDPE pipes, outer shells or trenched by water jetting.

Tom Skattum, Project Manager at Nexans Norway, said, “Achieving these new world records was a great challenge for Nexans and this contract for BKK represents the height of Nexans’ expertise in submarine power cables.”

The submarine cables have been manufactured at Nexans’ facility in Halden, Norway, and laying was completed in May 2016. This will be followed by termination work on shore, ready for the handover testing in autumn 2016.

Grid reinforcement project

BKK, one of Norway’s largest utility companies, is building the new connection to reinforce the power grid in the west of the country. The new power line is essential to ensure security of supply for the forecast growth in consumption by residents, businesses and industrial consumers in the Bergen region, which is an important growth area. It will also provide additional capacity for the grid connection of new generation resources.

The total length of the new 420 kV Mongstad to Kollsnes connection will be around 30 km. On land, overhead lines will carry the power. However, the majority of the route crosses two fjords, requiring the installation of the submarine cables.
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
Michel.gedeon@nexans.com

About Nexans

As a global leader in advanced cabling and connectivity solutions, Nexans brings energy to life through an extensive range of best-in-class products and innovative services. For over 120 years, innovation has been the company’s hallmark, enabling Nexans to drive a safer, smarter and more efficient future together with its customers. Today, the Nexans Group is committed to facilitating energy transition and supporting the exponential growth of data by empowering its customers in four main business areas: Building & Territories (including utilities, smart grids, e­mobility), High Voltage & Projects (covering offshore wind farms, submarine interconnections, land high voltage), Telecom & Data (covering data transmission, telecom networks, hyperscale data centers, LAN), and Industry & Solutions (including renewables, transportation, Oil & Gas, automation, and others). Corporate Social Responsibility is a guiding principle of Nexans’ business activities and internal practices. In 2013 Nexans became the first cable provider to create a Foundation supporting sustainable initiatives bringing access to energy to disadvantaged communities worldwide. The Group’s commitment to developing ethical, sustainable and high-quality cables drives its active involvement within several leading industry associations, including Europacable, The National Electrical Manufacturers Association (NEMA), International Cablemakers Federation (ICF) or CIGRE to mention a few. Nexans employs more than 26,000 people with industrial footprint in 34 countries and commercial activities worldwide. In 2017, the Group generated 6.4 billion euros in sales. Nexans is listed on Euronext Paris, compartment A. For more information, please consult: www.nexans.com