Nexans to deliver robotic fiber optic connection solution for Stokab in Sweden

Paris, February 16, 2016: Stokab, the Swedish telecom operator has awarded Nexans its first order for an Automated Optical Distribution Frame (AODF) following a successful year-long field trial in Stockholm, Sweden. The AODF will be used to facilitate remote controlled patching to support and improve Stokab’s hot spot communication business, which enables TV and radio broadcasters to transmit high bandwidth communication over optical fiber from almost 30 locations in Stockholm to their studios.

Nexans to deliver robotic fiber optic connection solution for Stokab in SwedenThe innovative AODF has been developed to drive the global roll out of state of the art fiber optic telecommunication networks. It enables remote and fully automatic optical patching and testing. Its sophisticated, but very simple to use software, arranges patching by a robot based hardware within minutes compared to sending technicians to sites in the busy Stockholm traffic.

The AODF provides a secure and reliable cross connection at the first physical layer in the fiber-optic network, with the patch-cord connector always installed in the right socket. Remote operation via a web interface eliminates routine site visits by technicians for network reconfiguration, cutting service times and costs. Testing can also be carried out remotely during low-traffic periods, such as at night, and in case of network failure it allows for a shorter mean-time-to-repair (MTTR).

Lars Josefsson, Sales & Marketing Director - D&I, Telecom and Utilities at Nexans said, “Nexans is since 20 years a proud supplier of optical fibre ribbon slotted core cables and related hardware to Stokab, which owns and operates the largest open and independent dark fiber network in the world. Nexans has continuously brought new solutions to the market and the AODF is yet a new important object in a large dark fiber network. The AODF is brought to the market in a partnership between Nexans and TeliSwitch Solution.” 

“We constantly try to improve our offerings to our customers. With the AODF-robot, from Nexans, we are now able to offer dark fibre connections in a minute to a variety of selected locations” Staffan Ingvarsson, Stokab’ Chief Executive Officer.

Further information about AOFD is available from this short video presentation

Related Document

Your Contact

Angéline Afanoukoe Press relations
Phone +33 1 78 15 04 67
Michel Gédéon Investor Relations
Phone +33 1 78 15 05 41

About Nexans

Nexans brings energy to life through an extensive range of cables and cabling solutions that deliver increased performance for our customers worldwide. Nexans’ teams are committed to a partnership approach that supports customers in four main business areas: Power transmission and distribution (submarine and land), Energy resources (Oil & Gas, Mining and Renewables), Transportation (Road, Rail, Air, Sea) and Building (Commercial, Residential and Data Centers). Nexans’ strategy is founded on continuous innovation in products, solutions and services, employee development, customer training and the introduction of safe, low-environmental-impact industrial processes.
In 2013, Nexans became the first cable player to create a Foundation to introduce sustained initiatives for access to energy for disadvantaged communities worldwide.
Nexans is an active member of Europacable, the European Association of Wire & Cable Manufacturers, and a signatory of the Europacable Industry Charter. The Charter expresses its members' commitment to the principles and objectives of developing ethical, sustainable and high-quality cables.
We have an industrial presence in 40 countries and commercial activities worldwide, employing close to 26,000 people and generating sales in 2014 of 6.4 billion euros. Nexans is listed on NYSE Euronext Paris, compartment A.
For more information, please consult: