Europe’s largest solar farm to be connected with Nexans’ photovoltaic cables

Nexans has been awarded a contract by Eiffage Energie on behalf of Clemessy to supply specialized photovoltaic cables and power cables for the Cestas solar farm in France

Nexans Cestas Copyright GIMBALL-ProdParis, June 30, 2015Europe’s largest solar farm will be connected with Nexans’ Energyflex® photovoltaic cables after Eiffage Energie awarded Nexans the contract to supply 90 percent of the cables for the Cestas solar farm in France. As part of the contract, Nexans will manufacture and supply approximately 5,000 kilometres of medium and low voltage, photovoltaic cables (PV) and data cables (optical fiber).

The solar farm, located near Bordeaux in southwest France, will generate more than 350 GWh per year with a peak capacity of 300 MW. Eiffage Energie operates on behalf of Clemessy which pilots a consortium of several investors including Neoen, formed to build, operate and maintain the farm.

Approximately one million solar panels will cover 250 hectares of land divided into 25 solar plants. The farm will be connected to the grid in October 2015.

Nexans’ Energyflex® cables will provide durable, high performance in-field connections between the PV panels and the inverters that will transform the solar energy into usable AC electricity. Energyflex® cables were developed by Nexans to meet the increasing demand for reliable, efficient cables in the specialised photovoltaic market.

Fernando Dos Santos, Photovoltaic Projects Manager at Eiffage Energie said, “Eiffage Energie chose Nexans because of its full range offer from low and medium voltage cables to photovoltaic cables for this project. Another important factor was that Nexans offers advanced supply chain solutions and direct delivery to site.

The cables are being manufactured at the Bourg-en-Bresse, Jeumont and Andrézieux plants in France. Installation is due to be completed by summer 2015.

 

 

Your Contact

Angéline Afanoukoe Press relations
Phone +33 1 78 15 04 67
Angeline.afanoukoe@nexans.com
Michel Gédéon Investor Relations
Phone +33 1 78 15 05 41
Michel.Gedeon@nexans.com

About Nexans

Nexans brings energy to life through an extensive range of cables and cabling solutions that deliver increased performance for our customers worldwide. Nexans’ teams are committed to a partnership approach that supports customers in four main business areas: Power transmission and distribution (submarine and land), Energy resources (Oil & Gas, Mining and Renewables), Transportation (Road, Rail, Air, Sea) and Building (Commercial, Residential and Data Centers). Nexans’ strategy is founded on continuous innovation in products, solutions and services, employee development, customer training and the introduction of safe, low-environmental-impact industrial processes.
In 2013, Nexans became the first cable player to create a Foundation to introduce sustained initiatives for access to energy for disadvantaged communities worldwide.
Nexans is an active member of Europacable, the European Association of Wire & Cable Manufacturers, and a signatory of the Europacable Industry Charter. The Charter expresses its members' commitment to the principles and objectives of developing ethical, sustainable and high-quality cables.
We have an industrial presence in 40 countries and commercial activities worldwide, employing close to 26,000 people and generating sales in 2014 of 6.4 billion euros. Nexans is listed on NYSE Euronext Paris, compartment A.
For more information, please consult: www.nexans.com

www.nexans.com