Nexans launches its next generation SUTA-FLEX Subsea Umbilical Termination Assembly

Nexans combines SUTA-FLEX with its wide range of umbilicals to deliver a complete solution from a single supplier

Paris May 4, 2015 - Nexans is at OTC 2015 to launch its next generation SUTA-FLEX Subsea Umbilical Termination Assembly. SUTA-FLEX is designed to work in combination with Nexans’ range of umbilicals to provide a complete, single source solution that enables oil and gas customers to benefit from more efficient and cost-effective project execution.

Nexans launches its next generation SUTA-FLEX Subsea Umbilical Termination AssemblyA Subsea Umbilical Termination Assembly is an electro-hydraulic system that enables multiple wells to be controlled by a single one umbilical by connecting a number of subsea control modules to the same communications, electrical and hydraulic supply lines.

The Nexans SUTA-FLEX concept offers a flexible modular design, based on standardized features that fit easily within the perimeters of the reel. It is also compact and allows a wide range of tensioners to be used for installation and is developed to withstand high pressure and ultra deep waters (up to 15,000 psi and 10,000 feet). SUTA-FLEX is supplied with field proven Nexans Electrical Field Installable Termination Assembly (FITA) and Fiber Optic Termination Unit (FOTU).

New possibilities

The use of a single supplier for the design, manufacture and assembly of subsea projects offers improved project execution. The SUTA-FLEX system is based on standardized components, which are assembled in accordance with the project’s specific needs.

The modular design gives customers full flexibility with regards to its constituent components. SUTA-FLEX is able to accommodate hydraulic, electrical or fiber optic components - or any combination of the three – within its compact outer dimensions. The design contributes to significantly improved reel packing as well as smoother handling and lifting operations.

The design is based on field proven components. Its optimized weight and size allows the termination system to work with a wide range of offshore installation vessel tensioners. A greater range of installation vessels may therefore be utilized.


OTC 2015
Offshore Technology Conference
Houston, Texas
4-7 mai 2015
Stand 5553

Related Document

About Nexans

Nexans brings energy to life through an extensive range of cables and cabling solutions that deliver increased performance for our customers worldwide. Nexans’ teams are committed to a partnership approach that supports customers in four main business areas: Power transmission and distribution (submarine and land), Energy resources (Oil & Gas, Mining and Renewables), Transportation (Road, Rail, Air, Sea) and Building (Commercial, Residential and Data Centers). Nexans’ strategy is founded on continuous innovation in products, solutions and services, employee development, customer training and the introduction of safe, low-environmental-impact industrial processes.
In 2013, Nexans became the first cable player to create a Foundation to introduce sustained initiatives for access to energy for disadvantaged communities worldwide.
Nexans is an active member of Europacable, the European Association of Wire & Cable Manufacturers, and a signatory of the Europacable Industry Charter. The Charter expresses its members' commitment to the principles and objectives of developing ethical, sustainable and high-quality cables.
We have an industrial presence in 40 countries and commercial activities worldwide, employing close to 26,000 people and generating sales in 2014 of 6.4 billion euros. Nexans is listed on NYSE Euronext Paris, compartment A.
For more information, please consult: