Statoil’s Gullfaks subsea compression station powered by Nexans umbilicals

Nexans’ power umbilicals will power two subsea compressors at the Gullfaks field off the coast of Norway

Paris, April 13, 2015 – The Statoil operated Gullfaks gas field in the Norwegian Sea will rely on Nexans’ innovative power umbilicals combining power, fiber-optic and hydraulic lines in a single cross section. The cables were successfully handed over to Statoil this month.

Gullfaks - sailing away-01 w225The subsea gas compression station will be installed on the seafloor at the Gullfaks Sør satellite field, 15 km from the Gullfaks C platform. It will increase total gas extraction by 22 million barrels.

The cables will power two five-megawatt gas compressors at a depth of 135 metres. The 650 tonne station will be housed in a 420 tonne protective structure, managing a flow rate of 10 million cubic metres per day.

Subsea compression is used when reservoir pressure falls below a critical level, reducing gas production. By compressing the gas on the seafloor, pressure in the pipelines is increased. Gas flows faster and allowing more to be extracted from the field. Subsea compression increases production, as well as the lifetime of the field.

Gullfaks - sailing away-02 w225The Gullfaks field is located 160 km west of Sognefjorden, Norway. The subsea gas compression station will be only the second of its kind in the world. Nexans delivered umbilicals to the first subsea compression station at the Åsgard gas field, also operated by Statoil, last year.

Subsea wet gas compression is suitable for small and midsized fields because of the compact size of the compressor. The solution can be installed in new or existing fields opening up possibilities for developing fields in the Arctic and other deep water regions.

Dirk Steinbrink, Senior Executive Vice President of High Voltage & Underwater Cable Business at Nexans, said, “We are proud of our position at the cutting edge of this development. The long-term partnership between Statoil and Nexans over many years has been important in facilitating this technological development“.

The Gullfaks compression station will be in operation later this year.
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
Michel.gedeon@nexans.com

About Nexans

Nexans brings energy to life through an extensive range of cables and cabling solutions that deliver increased performance for our customers worldwide. Nexans’ teams are committed to a partnership approach that supports customers in four main business areas: Power transmission and distribution (submarine and land), Energy resources (Oil & Gas, Mining and Renewables), Transportation (Road, Rail, Air, Sea) and Building (Commercial, Residential and Data Centers). Nexans’ strategy is founded on continuous innovation in products, solutions and services, employee development, customer training and the introduction of safe, low-environmental-impact industrial processes.
In 2013, Nexans became the first cable player to create a Foundation to introduce sustained initiatives for access to energy for disadvantaged communities worldwide.
Nexans is an active member of Europacable, the European Association of Wire & Cable Manufacturers, and a signatory of the Europacable Industry Charter. The Charter expresses its members' commitment to the principles and objectives of developing ethical, sustainable and high-quality cables.
We have an industrial presence in 40 countries and commercial activities worldwide, employing close to 26,000 people and generating sales in 2014 of 6.4 billion euros. Nexans is listed on NYSE Euronext Paris, compartment A.
For more information, please consult: www.nexans.com

www.nexans.com