Nexans has been awarded a subsea cable contract in excess of Euro 120 million by Scottish Hydro Electric Transmission

Nexans subsea cables will be installed by the C/S Nexans Skagerrak in deep waters to create a vital new high voltage power link for Scotland.

Paris, August 26, 2013 - Nexans, a worldwide expert in the cable industry, has been awarded a contract worth in excess of Euro 120 million by Scottish Hydro Electric (SHE) Transmission plc to supply and install a subsea power link to upgrade the electricity transmission network between the Kintyre peninsula and mainland coast in Southwest Scotland. The upgrade, which is part of SHE Transmission’s wider plans to invest up to Euro 6 billion in its electricity network between 2013 and 2021, will release up to 150 MW of additional grid capacity for renewable projects signalling a significant boost for the Kintyre economy.   

Nexans has been awarded a subsea cable contract in excess of Euro 120 million by Scottish Hydro Electric TransmissionNexans will create a twin subsea cable link, rated at 230 kV and 240 MVA, from a new substation on the peninsula to the mainland coast. The project includes the supply and installation of two 41 km 3-core submarine cables together with six 5 km single core underground cables for the land element. A fibre optic cable for control of the cable link will be integrated within the subsea cables and supplied separately for the land cables. Nexans will also supply a range of accessories.

Due to the route, the installation of the subsea cables in water depths of over 100 metres is one of the key elements of the project. The installation will be carried out by Nexans’ own cable ship, the C/S Nexans Skagerrak and the cable will be protected on the seabed by burial using the specialised Capjet system as well as rock dumping.

 “Nexans is delighted to be working with Scottish Hydro Electric Transmission on this high profile project that will provide vital reinforcement for Scotland’s power infrastructure” says Kjetil Hovland, Vice President, Submarine High Voltage Business Line in Nexans. “A key factor in winning this major contract was our proven capability to deliver complete subsea power cable solutions in-house from design and manufacture through to the installation scheduled for 2015”.

Related Document

Your Contact

Angéline Afanoukoe Press relations
Phone +33 1 78 15 04 67
Michel Gédéon Investor Relations
Phone +33 1 78 15 05 41

About Nexans

With energy at the basis of its development, Nexans, worldwide expert in the cable industry, offers an extensive range of cables and cabling solutions. The Group is a global player in the energy transmission and distribution, industry and building markets. Nexans addresses a wide series of market segments: from energy and telecom networks to energy resources (wind turbines, photovoltaic, oil and gas, and mining) to transportation (shipbuilding, aerospace, automotive and automation, and railways). Nexans is a responsible industrial company that regards sustainable development as integral to its global and operational strategy. Continuous innovation in products, solutions and services, employee development and commitment, customer orientation and the introduction of safe industrial processes with limited environmental impact are among the key initiatives that place Nexans at the core of a sustainable future. With an industrial presence in 40 countries and commercial activities worldwide, Nexans employs 25,000 people and had sales in 2012 of nearly 7.2 billion euros. Nexans is listed on NYSE Euronext Paris, compartment A.