Case study

Tyrrhenian Link

  • LOCATION
    Italy
  • PARTNERSHIP
    Terna
  • MARKET
    Power networks - Subsea

The Tyrrhenian Link is a significant milestone in the much-needed development of the electricity grid in Europe. It creates a new electricity corridor between Sicily, Sardinia, and Campania that will allow the first loop to be established between the two islands and the Italian mainland.

As part of the contract, Nexans will manufacture and install 500km of a 500kV mass-impregnated (MI) cable and Fiber Optic (FO) cable at more than 2,000m water depth, the deepest depth ever for a subsea power cable in the Mediterranean.

The project will help increase electricity exchange capacity and support the development of renewable energy flows. In addition, it will strengthen network stability and security as well as increase competitiveness for producers in the local electricity markets.

This frame contract showcases the success of Nexans’ unique subsea deep-water know-how and full-turnkey approach, notably combining manufacturing and installation with excellence in risk management. Also, it demonstrates the Group’s key role as a major player in the electrification of Europe and signals its critical role in improving grid infrastructure across the Mediterranean, with more projects in the region expected to be announced further.

For the Nexans installation of the interconnector cable, Nexans’ will use the recently launched cable-laying vessel “Nexans Aurora”, which can install deep water cables in water depth of over 2,000m and supports a 10,000ton cable payload.

Layer 1
Related market
Subsea Interconnectors Discover