CSR performance

Nexans' group social and environmental indicators

Responsible performance confirmed by extra-financial rating agencies

In the rapidly changing international environment, Nexans is committed to building long-term relationships and to sharing value with each of its stakeholders.
Nexans’ consistently improving scores show both the strength of our CSR policy for stakeholders and intelligent management of the Group’s strategy.

Nexans CSR performance - 2018

Nexans CSR scorecard

2018 ratings

A

Carbon Disclosure Project (CDP)

in 2018, Nexans has reached new milestones across a panel of ratings, including being referenced, for the first time, as one of the global leaders fighting against climate change by Carbon Disclosure Project (CDP). 

B-

ISS Oekom

ISS Oekom attributed a B- rating to Nexans up from C+ in 2017. The best rating in the sector being B, the Group has obtained Prime status. At the end of 2018, Nexans was ranked 11th out of 80 in the Electronic Components sector.

71%

Sustainalytics

Sustainalytics gave a score of 71% (compared to 63% in 2017), which allows the Group to be ranked 11th out of 43 in its sector.

BBB

MSCI

MSCI attributed a BBB rating to the Group up from BB rating in 2017 and 2016, which places the Group on the 9th position in its sector.

72%

EcoVadis

EcoVadis attributed the 72% "Advanced" rating compared to 68% in 2016 and 2015. The Group has thus obtained the EcoVadis "CSR Commitment" Gold level label, becoming one of the top 5% of companies evaluated by the rating agency.

Nexans' group social and environmental indicators

Environmental indicators

Social indicators