Layer 1

Power generation & transmission

Interested in our solutions ?

Overview

At the beginning of the electrification process, power generation and transmission actors are facing a series of new challenges. As power demand is predicted to increase by 19% between now and 2030, they are fully focused on responding to this fast growing power demand, while meeting increasingly strict environmental and regulatory requirements. As electrification also requires a growing number of advanced, reliable interconnections that can transport more power over longer distances, offshore and onshore, Nexans brings energy from the generation area to the consumption area and is commited to make the most challenging generation and transmission projects a success.

+19%

increase in world energy demand between 2021 and 2030

200 GW

additional capacity to come from offshore windfarms in the next decade

250%

expected market growth of inter array and export cables for offshore wind farms between 2019 and 2030