Login Get Registered Catalog Browser Contact Us
Global expert in cables and cabling system

About Nexans

Products and Solutions

Customer Service

Work at Nexans

News and Press

Go

Nexans to supply special cables for Baggage Handling System for extension or transforming airport programs worldwide

Send link to this page Your Nexans contact on this page
The group will provide power and control cables for terminals of Dubai, Dublin and Doha international airports

Dublin's airport bagage handling systemParis, December 16, 2009 – Nexans, the worldwide leader in the cable industry, has been awarded several contracts to supply around 400 km of special cables for the extension or transformation of terminals at Dubai (UAE), Dublin (Ireland) and Doha (Qatar) international airports. The cables will provide power and control and equip the baggage handling systems (BHS).

Nexans will supply halogen free fire-retardant power and control cables, as well as bus cables. Most of these cables will be manufactured at Nexans’ facilities in Monchengladbach and Nuremberg in Germany, and Frameries in Belgium.

Baggage handling systems are extremely complex and the cables for these systems must adhere to strict technical and security requirements”, says Paolo Pieri, Nexans Executive Business Developer, Airport project. “They must operate at high temperatures, prevent premature cable aging and look after passenger safety in the event a fire occurs by assuring low smoke density and corrosive gases”.

Dubai Airport Terminal 3 Concourse 3

Nexans will provide to Siemens Middle East around 200 km of specialized cables for the Extension of Terminal 3 Concourse 3 at Dubai Airport. The cables will provide power and control and equip the baggage handling systems being installed at Dubai´s Airport’s new Terminal 3. The cables should be installed in 2010.

Dubai International Terminal 3 opened on October 14, 2008 for the exclusive use of Emirates. Its capacity of 43 million passengers per year expanded the airport’s overall capacity to 60 million passengers. The Terminal 3 complex includes an associated airside facility (also known as concourse 2) and an A380 dedicated airside facility (concourse 3) that is currently under construction.

Between 2005 and 2007, Nexans has already delivered 2.000 km of cables for the Baggage Handling System for the Terminal 3 and the Mega Cargo at Dubai International.


Transforming Dublin Airport program

Nexans will supply to Siemens Ireland around 100 km of power and control cables for the Transforming Dublin Airport Programs, and particularly to equip the baggage handling systems at new Terminal Two. Installation should start by the end of 2009.

Terminal Two is the centre-piece of the Transforming Dublin Airport program. Work started on T2 in October 2007 and it is scheduled to open to the public in April 2010. When the program is complete the new facilities will allow Dublin Airport to comfortably handle up to 35 million passengers per year and will create a modern airport that will be an efficient gateway to the Ireland of the 21st century.

 

Doha Airport Extension program

Finally, Nexans also participates to the Doha Airport Extension program as the Group has been awarded a contract by Interoller Singapore (newly branded Pteris) to supply 100km of cable for the Baggage Handling Systems.

 

Nexans cable solutions for modern airports

In addition to baggage handling systems, Nexans provides a complete range of cable solutions that meets the expectations of safety, security and efficiency for the modern airports. For airport infrastructure, Nexans supplies power (high, medium and low voltage) and fiber optic cables for energy and communication networks installations in multiple terminals, hangars, airfields and control towers, etc. Nexans has already equipped many airports throughout the world such as Incheon Airport in Seoul, South Korea, Enfidha, Tunisia and Jeddah, Saudi Arabia.

 


Related Information
Discover nexans' offer for airports

Related Document
  Nexans to supply special cables for Baggage Handling System for extension or transforming airport programs worldwide  (79.7kb)

Your Contact
Céline Révillon
Corporate Communications - Press relations
Phone + 33 1 73 23 84 12
celine.revillon@nexans.com
Michel Gédéon
Investor Relations
Phone +33 (0)1 73 23 85 31
Michel.Gedeon@nexans.com

About
About Nexans
With energy as the basis of its development, Nexans, the worldwide leader in the cable industry, offers an extensive range of cables and cabling systems. The Group is a global player in the infrastructure, industry, building and Local Area Network markets. Nexans addresses a series of market segments from energy, transport and telecom networks to shipbuilding, oil and gas, nuclear power, automotive, electronics, aeronautics, handling and automation. With an industrial presence in 39 countries and commercial activities worldwide, Nexans employs 22,400 people and had sales in 2008 of 6.8 billion euros. Nexans is listed on NYSE Euronext Paris, compartment A. More information on www.nexans.com



Related Document
  Nexans to supply special cables for Baggage Handling System for extension or transforming airport programs worldwide  (79.7kb)


Related Information
Discover nexans' offer for airports


Nexans © copyright 2001 - 2010   Legal Notice | Contact Us | Site Map