English Login Zarejestruj się Catalog Browser Contact Us
Światowy ekspert w dziedzinie kabli i systemów kablowych

O firmie Nexans

Produkty i rozwiązania

Mój Nexans

Praca w Nexans

Aktualności i wiadomości prasowe

Go

Skagerrak cable-laying vessel

Bookmark Contact Us
for laying cables securely on the seabed

  • Nexans’ Skagerrak is one of the world’s most advanced cable-laying vessels, with a 7,000 tonne capacity turntable, a state-of-the-art global positioning system, and multiple cranes.

 

The Skagerrak laid a 400 kV submarine cable across the Strait of Gibraltar and a 576-km-long HVDC cable between Norway and the Netherlands. With Prysmian, it is laying a 275 km energy/fiber cable at 1,500 meters between Mallorca and mainland Spain. It is also completing 292 km of HVDC for the Norwegian Valhall oil field.

 

Skagerrak large picture

 

Nexans provides efficient solutions for cable laying like Capjet trenching system and Captrack positioning system.

 

Nexans Capjet trenching system has been developed to provide an efficient solution for protection of submarine cables, umbilicals and pipelines based on the water jetting principle. Nexans Capjet has buried 8,000 km since it was first introduced in 1986.

The trenching units have a purpose built Launch And Recovery System (LARS) for safe and efficient operation from the vessel. Nexans has three identical CAPJET Systems complete with handling system, and all can be equipped with the developed tools.

 

Nexans Captrack is designed to ride on rollers on top of the cable during cable laying. The Captrack gives accurate touchdown position. By means of depth sensor, altimeter and inclinometer, the most accurate bottom tension control is obtained. All data is transmitted to the control container topside.

 

Nexans Capjet, trencing system

Nexans Capjet,
trenching system

Launch And Recovery System

Purpose built Launch
And Recovery System

Nexans Captrack, positioning system

Nexans Captrack, positioning system

 

The systems were used for Ormen Lange, NorNed, Snøhvit, Tyrihans, Åsgaard, Troll, Valhall, Statfjord C and recently the Hainan project.

 





 TOP
Nexans © copyright 2001 - 2012   Legal Notice | Contact Us | Site Map