|
|
|
|
We help our customers meet their commitments by adding value to the installation process.
|
|
More...
|
|
|
|
|
This unit is more than an automative sensor; it protects and stabilizes itself against malfunction.
|
|
More...
|
|
|
|
|
Sometimes, a technical innovation gives rise to unforeseen benefits.
|
|
More...
|
|
|
|
|
iSwitch G 1043E joins WINDLINK®, a range of high-performance solutions for wind turbines.
|
|
More...
|
|
|
|
|
This local production will enable Nexans to meet the demands of customers operating in China’s booming rail industry
|
|
More...
|
|
|
|
|
When it came to cabling their new state of the art Honda Centre, Lings Honda wanted the very best – so Nexans LANmark-7 was a natural choice.
|
|
More...
|
|
|
|
|
Without any doubt 10 Gigabit is ‘THE’ current hot topic in data cabling. But with so many manufacturers claiming solutions with ‘guaranteed compliance’, arguments in the press over who was first, and a raft of claims to demonstrate the size of the installed base of 10 Gigabit-ready ports, one wonders why all this press activity is really necessary if it’s all so simple and straightforward. The reality is of course that it’s not quite as cut and dried as some may have us believe – after all there’s no smoke without mirrors!
|
|
More...
|
|
|
|
|
Nexans has developed a new steep terrain dredger/ sub-sea intervention vehicle for the demanding seafloor terrain of the Ormen Lange gas field on the Norwegian continental shelf.
|
|
More...
|
|
|
|
|
Nexans, the worldwide leader in the cable industry, has been awarded a contract of approximately 7.5 million USD, by Alaska Electric Light and Power (AEL&P), for the supply and installation of a 3 core 69 kV XLPE solid dielectric submarine cable
|
|
More...
|
|
|
|
|
March 22, 2005 - Nexans, the worldwide leader in the cable industry, announces the new generation of LANmark snap-in connectors: LANmark EVO. This new LANmark EVO series design has evolved from Nexans' well established LANmark-5 & LANmark-6 snap-in connectors, and provides enhanced termination benefits for installers, including a saving of at least 20 percent in installation time, and is complemented by a new Universal Comfort Tool.
|
|
More...
|
|
|
|
|
March 18, 2005 - Nexans, the worldwide leader in the cable industry, has been awarded a project worth around 22 million Euros for trenching services, by Hydro as operator for the Ormen Lange licence group, for two MEG (Mono Ethylene Glycol) pipelines and two umbilical cables serving the undersea gas field on the continental shelf around 120 km off the coast of Norway.
|
|
More...
|
|
|
|
|
UCL : University College London Engineering Building
|
|
More...
|
|
|
|
|
Nexans announces that its Machinery unit based in Hanover in Germany has signed an exclusive cooperation agreement with the Austrian company Cincinnati Extrusion GmbH. This agreement concerns the sale of equipment used to manufacture plastic-metal composite pipes.
|
|
More...
|
|
|
|
|
Nexans, the worldwide leader in the cable industry, has won a contract worth around Euros 15 million to manufacture and install the world's first 420kV XLPE (cross-linked polyethylene) submarine power cable for the ongoing development of the Ormen Lange gas field on the Norwegian continental shelf. The customer is Statnett, Norway's state-owned transmission system operator.
|
|
More...
|
|
|
|
|
Nexans has launched new range of optical fibre connectivity to provide complete solutions for every situation including Storage Area Networks and Data Centres.
|
|
More...
|
|
|
|
|
'1-2-Fly', the Hannover based travel agency has installed over 3000 GG45 connections in it's new HQ.
|
|
More...
|
|
|
|
|
Nexans has Launched the Quickmount III cabinet - an upgraded version of the popular fast assembly cabinet with additional new features. The cabinet is available in 800x800x42U format.
|
|
More...
|
|
|
|
|
Nexans has enhanced it is LANmark-5 range with the addition of fixed PCB patch panels in order to be more competitive where the benefits of the sliding versions are not required.
|
|
More...
|
|
|
|
|
Nexans has Launched the Quickmount III cabinet - an upgraded version of the popular fast assembly cabinet with additional new features. The cabinet is available in 800x800x42U format.
|
|
More...
|
|