English
Assistance & Tools
Login
Search Go
Search +
Global expert in cables and cabling system

About Nexans

Products and Solutions

Customer Service

Finance

Work at Nexans

News and Press


Frequently Asked Questions

Search Go
Or click on a specific topic to display related FAQ :

Product information (2)
Site usage (3)
Brochures (2)

How do I reach the home page of your site
Click on the Nexans Logo
Back to top
I have problems to view pdf files
Symptoms

When trying to open a PDF from a web-site using the PC version of Adobe Acrobat Reader 5, the browser either:

1. Freezes and stops responding to user input;
2. Crashes, giving an error message in a dialog box and then closes the browser.

Solution

1. Instead of opening the PDF form as you would do for a normal link, Right Click on the link to the PDF file and choose "Save Target As...".
2. Select an easy-to-remember location on your hard drive to store the file
3. Go to the location where you saved the form, and double-click the file to open
4. This will launch the Adobe Acrobat Reader

Back to top
What is POF?

POF (Plastic Optical Fiber) has been developed by DuPont in the late 1960s as a medium for illumination. After 30 or so years, a new interest has emerged in short link cabling technologies based on multimode POF for multimedia and data communications.Polymethylmethacrylate (PMMA) is generally the polymer material for step index plastic optical fibers (SI-POF). Perfluorinated polymer (e.g. CYTOP) is mainly used in graded index plastic optical fibers (GI-POF). The attenuation of fluorinated polymers is lower than PMMA allowing higher performances.

POF offers a viable alternative to copper and glass solutions. At data transmission rates of 100 Mbit/s to 10 Gbit/s, POF can operate faster than usual copper wire and is not sensible to electromagnetic (EM) perturbation. The flexibility and the large diameter of POF, typically 200 mm to 1mm, presents a great advantage for plastic compared to glass. The fragile and brittle nature of glass optical fibers, combined with core diameters from 8 to 62,5 mm, makes it more difficult and costly to install and align than POF.

Back to top
What kind of browser should I use?
Currently, the site is best suited for PC users equipped with Internet Explorer, if possible with a version above 5.5. The site works also with Netscape version 4.5 or above, some default might appear in the layout. For Mac users, some functionalities of the site will not be available. We apologize for the inconvenience while we are trying to solve the technological incompatibility in the different technology.
Back to top
Where are POFs used?

Today plastic optical fibers are already widely used in cars, multimedia links, CD players, industrial electronics, minidisc systems and PCs. The main actual market is the automotive market where POF (SI) replaces copper wires to communicate information between radio, navigation system, CD player and mobile phone system (already installed in all Mercedes, Peugeot´) In BMW, POF does not only connect the multimedia systems but also some safety features.

In the next five years, Local Area Network (LAN) is expected to become a fantastic market where GI POF might substitute a significant part of copper twisted pair and silica multi mode cabling systems.

Home networking is also expected to become a major market for POF, which will be driven in the digital age by the increasing audio/video and electronics games systems.

Back to top
Contact Us
Contact Us

Top 5 FAQ
Nexans © copyright 2001 - 2008   Legal Notice | Contact Us | Site Map