Nexans launches PVC-free MOTIONLINE® HALEX automation cables

New, halogen-free material offers enhanced fire protection at low additional costs compared with PVC

Paris, November 22, 2016 – Nexans has launched the new MOTIONLINE® HALEX cable series, a range of halogen-free flexible automation cables for industrial applications.

Nexans launches PVC-free MOTIONLINE® HALEX automation cablesIn the past, operators who needed halogen-free (PVC-free) cables could only choose PUR cables, which offer outstanding mechanical performance but are significantly more expensive than PVC-sheathed cables. Nexans is now offering an alternative that not only is flexible, robust, drag-chain-capable and flame-retardant, but also entails low additional costs compared with PVC cables.

Nexans’ HALEX cables do not contain halogens and, like PUR cables, are flame-retardant. In contrast to PVC, they do not release any highly toxic or irritant gases in the event of a fire. The sheath permits small bending radii (at least 2 million cycles at 10xD) and is resistant to abrasion, oil and cooling lubricants.

Philipp Teepe, Product Manager Automation at Nexans said, “We’re very proud of what we are able to offer with the HALEX range. The cables are ideal for meeting the demand for PVC-free cables without having to compromise on functionality. It is also helping us to meet our target of reducing environmentally harmful PVC.

Nexans offers HALEX cables in the form of drag-chain-capable sensor, servo, bus, Industrial Ethernet, energy and control cables. Like other MOTIONLINE® cables, the design of products from the HALEX series can be adapted according to customer requirements.
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
Michel.gedeon@nexans.com

About Nexans

As a global leader in advanced cabling and connectivity solutions, Nexans brings energy to life through an extensive range of best-in-class products and innovative services. For over 120 years, innovation has been the company’s hallmark, enabling Nexans to drive a safer, smarter and more efficient future together with its customers. Today, the Nexans Group is committed to facilitating energy transition and supporting the exponential growth of data by empowering its customers in four main business areas: Building & Territories (including utilities, smart grids, e­mobility), High Voltage & Projects (covering offshore wind farms, submarine interconnections, land high voltage), Telecom & Data (covering data transmission, telecom networks, hyperscale data centers, LAN), and Industry & Solutions (including renewables, transportation, Oil & Gas, automation, and others). Corporate Social Responsibility is a guiding principle of Nexans’ business activities and internal practices. In 2013 Nexans became the first cable provider to create a Foundation supporting sustainable initiatives bringing access to energy to disadvantaged communities worldwide. The Group’s commitment to developing ethical, sustainable and high-quality cables drives its active involvement within several leading industry associations, including Europacable, The National Electrical Manufacturers Association (NEMA), International Cablemakers Federation (ICF) or CIGRE to mention a few. Nexans employs more than 26,000 people with industrial footprint in 34 countries and commercial activities worldwide. In 2017, the Group generated 6.4 billion euros in sales. Nexans is listed on Euronext Paris, compartment A. For more information, please consult: www.nexans.com