Nexans helps boost train fire safety with new FLAMEX® SI-FR Rolling Stock cables

FLAMEX® SI-FR New Range Ensures Cable Integrity keeping critical emergency functions in the Most Demanding Fire Situations

Paris, March 21, 2017 – Rail transportation plays an integral role in the global transportation industry with a steady growth in rail passenger transport observed between 2011 and 2015 and around 416 billion ton-kilometers traveling by train freight in Europe alone in 2015. Seeking to boost passenger railway fire safety, Nexans, the leading global supplier of industrial cabling solutions, has launched its innovative FLAMEX® SI-FR line of fire-resistant cable products for critical power and control systems used in trains. The new cables maintain circuit integrity during a fire, enabling conductors and operators to travel out of compromising situations to safety if a fire were to break out. All FLAMEX® cables also help limit the spread of potential fires and the release of harmful smoke.

Nexans helps boost train fire safety with new FLAMEX® SI-FR Rolling Stock cablesFLAMEX® SI-FR cables can withstand the harsh operating conditions on rolling stock such as variations in temperature, snow, rain, sunlight and heavy vibrations. They are particularly suitable where high temperatures are required to save weight as the cables can operate at up to 170°C with a maximum operating voltage of 3 or 6 kV. Yannick Goutille, Rolling Stock Product Manager at Nexans said, “FLAMEX® SI-FR meets the expectations of customers that are designing rolling stock equipments and that are handling the products.

In the rail industry, tunnels can quickly turn from transportation convenience to potentially lethal enclosures if a fire breaks out. When flames start roaring through rail cars, it is essential to maintain power and control system operation to ensure the train can continue on to a safe place. Nexans’ FLAMEX® FR cables enable the continuous flow of power needed for emergency systems to function reliably when needed most, providing improved safety for operators and fire response personnel. Yannick Goutille said, “Safety is a key concern for Nexans and our customers, transit authorities and manufacturers. Addressing this concern is our top priority. This new FLAMEX® range meets the most stringent regulations in the industry while maintaining performance, and therefore safety.”

In addition to being fire retardant, the new FLAMEX® range of power, control and communication cables are also designed to emit low levels of smoke during fire. The cables are compliant with EN 45545-2 requirements for the highest hazard level class, and meet fire resistance requirements laid out by EN 50200 or IEC 60331 standards. The range is also asbestos free and RoHS (Restriction of Hazardous Substances) compliant.

To learn more about Nexans’ new FLAMEX® product line and all of its cabling offerings, please visit www.nexans.com.
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
Michel.gedeon@nexans.com

About Nexans

As a global leader in advanced cabling and connectivity solutions, Nexans brings energy to life through an extensive range of best-in-class products and innovative services. For over 120 years, innovation has been the company’s hallmark, enabling Nexans to drive a safer, smarter and more efficient future together with its customers. Today, the Nexans Group is committed to facilitating energy transition and supporting the exponential growth of data by empowering its customers in four main business areas: Building & Territories (including utilities, smart grids, e­mobility), High Voltage & Projects (covering offshore wind farms, submarine interconnections, land high voltage), Telecom & Data (covering data transmission, telecom networks, hyperscale data centers, LAN), and Industry & Solutions (including renewables, transportation, Oil & Gas, automation, and others). Corporate Social Responsibility is a guiding principle of Nexans’ business activities and internal practices. In 2013 Nexans became the first cable provider to create a Foundation supporting sustainable initiatives bringing access to energy to disadvantaged communities worldwide. The Group’s commitment to developing ethical, sustainable and high-quality cables drives its active involvement within several leading industry associations, including Europacable, The National Electrical Manufacturers Association (NEMA), International Cablemakers Federation (ICF) or CIGRE to mention a few. Nexans employs more than 26,000 people with industrial footprint in 34 countries and commercial activities worldwide. In 2017, the Group generated 6.4 billion euros in sales. Nexans is listed on Euronext Paris, compartment A. For more information, please consult: www.nexans.com