Nexans drives the transition to higher Voltage wind farm networks

Nexans is pioneering a step-change in the renewables industry as wind farm operators switch to higher voltage inter-array networks that boost their output capacity while utilising cost-effective, robust and easy to install cable systems. the new 72.5 kv accessories complement the previous development of Nexans’ high-voltage inter-array cables.

Nexans PABG 72.5 kVParis, June 30, 2016 – Nexans is launching a new range of cable and power accessories to meet the growing demand for higher capacity windfarms. The new generation of power accessories with F-type outer cone comprising separable T-connectors, coupling connectors and surge arresters has been developed to operate at 72.5 kV.

To transmit the increased power between each individual turbine and collection platforms efficiently, Nexans has created inter-array cable systems able to operate at 72.5 kV instead of the traditional 36 kV. Transformer and switchgear OEMs have upgraded their designs to take into account the higher voltage.

As renewable energy becomes more prevalent, economic power supply becomes more and more important. There is now  a new common standard for offshore wind connection systems up to 72.5 kV.

The standardized interface between power accessories and equipment bushings is a first in the field of this voltage class. Unlike traditional connection solutions, separable, compact T-shape connectors offer many advantages. The outer cone standard allows several combinations of cable arrangements such as single connection, double connector arrangement with coupling connector, double connector arrangement with surge arrester.

All of Nexans power accessories up to 72.5 kV are type tested according to IEC 60840. Equipment bushings by EUROMOLD® are additionally type tested according to IEC 60137. Both, separable connectors and bushings are tested according to IEC 60068 successfully (solar radiation IEC 60068-2-5 and salt mist IEC 60068-2-52).

All kits of Nexans connectors, terminations and joints include conductor contacts use patented GPH® mechanical connection technology, which is type tested according IEC 61238-1. GPH® mechanical connectors and cable lugs have been in use for 25 years. They are compatible with aluminum and copper conductors of the most designs. An innovative system of patented shear-off-head bolts ensures easy installation and the stability of electrical connections.

Your Contact

Angéline Afanoukoe Press relations
Phone +33 1 78 15 04 67
Angeline.afanoukoe@nexans.com
Michel Gédéon Investor Relations
Phone +33 1 78 15 05 41
Michel.Gedeon@nexans.com

About Nexans

As a global leader in advanced cabling and connectivity solutions, Nexans brings energy to life through an extensive range of best-in-class products and innovative services. For over 120 years, innovation has been the company’s hallmark, enabling Nexans to drive a safer, smarter and more efficient future together with its customers. Today, the Nexans Group is committed to facilitating energy transition and supporting the exponential growth of data by empowering its customers in four main business areas: Building & Territories (including utilities, smart grids, e­mobility), High Voltage & Projects (covering offshore wind farms, submarine interconnections, land high voltage), Telecom & Data (covering data transmission, telecom networks, hyperscale data centers, LAN), and Industry & Solutions (including renewables, transportation, Oil & Gas, automation, and others). Corporate Social Responsibility is a guiding principle of Nexans’ business activities and internal practices. In 2013 Nexans became the first cable provider to create a Foundation supporting sustainable initiatives bringing access to energy to disadvantaged communities worldwide. The Group’s commitment to developing ethical, sustainable and high-quality cables drives its active involvement within several leading industry associations, including Europacable, The National Electrical Manufacturers Association (NEMA), International Cablemakers Federation (ICF) or CIGRE to mention a few. Nexans employs more than 26,000 people with industrial footprint in 34 countries and commercial activities worldwide. In 2017, the Group generated 6.4 billion euros in sales. Nexans is listed on Euronext Paris, compartment A. For more information, please consult: www.nexans.com