Nexans’ near-invisible overhead line conductors blend into Norwegian nature reserve for Statnett project

Nexans’ coloured conductors produced by a unique surface treatment process will help Statnett meet growing energy demands in Norway through its new overhead line

Paris, June 22, 2016 - Statnett, Norway’s state owned power system operator, has energised 68 km of Nexans’ coloured conductors on its new overhead transmission line connecting central Norway to western Norway. The line will secure the supply of power in the region. Nexans’ coloured conductors have been used on 8.5 km of the line that run through a protected nature reserve, allowing the cables to blend in with the environment.

Nexans’ near-invisible overhead line conductors blend into Norwegian nature reserve for Statnett projectNexans has used a unique surface treatment to manufacture the green coloured aluminium wires. This helped the conductors blend in with the environment, making it more acceptable to local residents. The patented treatment process is able to produce different types of conductors in almost all colours, and in contrast to traditional coatings methods it has no adverse effect on the aluminium wire substrate, the conductors remain easy to connect and the colour will not deteriorate over time due to UV exposure.

Nexans’ near-invisible overhead line conductors blend into Norwegian nature reserve for Statnett projectThe coloured conductors have undergone electrical and mechanical tests, and a complete system was assembled with implosive fittings to ensure the conductors will behave as expected.

The 420 kV line was constructed to reduce the 8 TWh energy deficit in central Norway by increasing the grid capacity between a region with energy surplus to central Norway.. The deficit is equivalent to the annual power consumption of 400,000 single family homes. Statnett’s 297 km line will also facilitate  around 100 small hydropower schemes to the grid between Ørskog and Fardal. 

Steinar Beurling, Electromechanical engineer at Statnett said, “We were looking for a solution that would allow us to reduce the energy deficit in central Norway, while maintaining the natural beauty in our country. Nexans provided a solution through its coloured conductors.

Cyprien Federspiel, VP Sales & Marketing for Land High Voltage at Nexans added, “Nexans is committed to increasing access to energy. As the only manufacturer with this offering, we are pleased to help Statnett reinforce Norway’s grid.”
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
Michel.gedeon@nexans.com

About Nexans

As a global leader in advanced cabling and connectivity solutions, Nexans brings energy to life through an extensive range of best-in-class products and innovative services. For over 120 years, innovation has been the company’s hallmark, enabling Nexans to drive a safer, smarter and more efficient future together with its customers. Today, the Nexans Group is committed to facilitating energy transition and supporting the exponential growth of data by empowering its customers in four main business areas: Building & Territories (including utilities, smart grids, e­mobility), High Voltage & Projects (covering offshore wind farms, submarine interconnections, land high voltage), Telecom & Data (covering data transmission, telecom networks, hyperscale data centers, LAN), and Industry & Solutions (including renewables, transportation, Oil & Gas, automation, and others). Corporate Social Responsibility is a guiding principle of Nexans’ business activities and internal practices. In 2013 Nexans became the first cable provider to create a Foundation supporting sustainable initiatives bringing access to energy to disadvantaged communities worldwide. The Group’s commitment to developing ethical, sustainable and high-quality cables drives its active involvement within several leading industry associations, including Europacable, The National Electrical Manufacturers Association (NEMA), International Cablemakers Federation (ICF) or CIGRE to mention a few. Nexans employs more than 26,000 people with industrial footprint in 34 countries and commercial activities worldwide. In 2017, the Group generated 6.4 billion euros in sales. Nexans is listed on Euronext Paris, compartment A. For more information, please consult: www.nexans.com