Nexans cables to bring Internet to Amazon Rainforest

Nexans Norway is supplying 275 km fibre optic cables to the Connected Amazonia Program in Brazil

Paris, April 21, 2016 – Brazil’s Connected Amazonia Program will include Nexans submarine fibre optic cables. The total project aims to bring Internet to 4 million people in the Amazon Rainforest. The project comprises 7,700 km of cables to connect 52 municipal areas through five separate cable routes on and beneath riverbeds because of the unique environment in the Amazon.

Nexans cables to bring Internet to Amazon RainforestFor Brazil’s Connected Amazonia Program, one of the largest submarine fibre projects in the world, the 275 km of Nexans cables will be installed in riverbeds between Coari and Tefé. The entire network will be made up of five data highways: Upper Negro river, Upper Solimões, Madeira, Purus and Juruá.

For this project, Nexans recommended using high performance cables that have a minimal environmental impact. This allows the project to serve the needs of local communities while preserving the fragile Amazon Rainforest ecosystem. Nexans supplied cables that will not release harmful substances into the delicate river ecosystem and therefore have no negative impact on the environment. The fibre optic cables from Nexans’ URC-1 family of cables meet all international standards for submarine cables.

To handle the strong currents in the river that occur throughout the year, a flat-bottomed barge will be used as the cable-laying vessel. For additional security, five support vessels will accompany the cable-laying barge. In the future, local teams with specialist tools can maintain the cables.

Nexans cables to bring Internet to Amazon RainforestThe Connected Amazonia Program aims to bring a high quality Internet connection to the State of Amazonas, not only to connect residents to the Internet, but also to enable telemedicine, distance learning and greater interconnection between health, security and traffic services. The Program aims to do this while minimising the environment impact of the installation.

Brazil is ranked fourth in the world for the number of users accessing the Internet[i] and this will only grow with this project, which connects native and riverside communities in the Amazon to the Internet. In order to provide a premium service, the cables were manufactured at Nexans Norway, a specialist plant focussing on high performance Ethernet solutions, and shipped to Brazil for installation.

Ragnar Vogt, Director at Nexans Norway said, “This project will do more than connect native people to the Internet. It will bring investment, improved healthcare and better access to education to traditionally isolated regions. We are proud to be helping to bring technology to the Amazon Rainforest. Nexans is looking forward to the challenge of working in such a unique environment. To ensure the Program got all the expertise we could offer, the Norwegian and Brazilian teams worked together to combine technological and local area knowledge.

 


[i] Source : eMarketer, company specialized in researches about digital market
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
Michel.gedeon@nexans.com

About Nexans

As a global leader in advanced cabling and connectivity solutions, Nexans brings energy to life through an extensive range of best-in-class products and innovative services. For over 120 years, innovation has been the company’s hallmark, enabling Nexans to drive a safer, smarter and more efficient future together with its customers. Today, the Nexans Group is committed to facilitating energy transition and supporting the exponential growth of data by empowering its customers in four main business areas: Building & Territories (including utilities, smart grids, e­mobility), High Voltage & Projects (covering offshore wind farms, submarine interconnections, land high voltage), Telecom & Data (covering data transmission, telecom networks, hyperscale data centers, LAN), and Industry & Solutions (including renewables, transportation, Oil & Gas, automation, and others). Corporate Social Responsibility is a guiding principle of Nexans’ business activities and internal practices. In 2013 Nexans became the first cable provider to create a Foundation supporting sustainable initiatives bringing access to energy to disadvantaged communities worldwide. The Group’s commitment to developing ethical, sustainable and high-quality cables drives its active involvement within several leading industry associations, including Europacable, The National Electrical Manufacturers Association (NEMA), International Cablemakers Federation (ICF) or CIGRE to mention a few. Nexans employs more than 26,000 people with industrial footprint in 34 countries and commercial activities worldwide. In 2017, the Group generated 6.4 billion euros in sales. Nexans is listed on Euronext Paris, compartment A. For more information, please consult: www.nexans.com