English
Assistance & Tools
Login
Search Go
Search +
Global expert in cables and cabling system

About Nexans

Products and Solutions

Customer Service

Finance

Work at Nexans

News and Press


Nexans equips Belgacom Towers in Brussels with LANmark Category 6 solution

Send link to this page Your Nexans contact on this page

Paris, January 23, 2003 - Nexans has been awarded the contract for cabling the two �Belgacom U+T Towers� in Brussels with a LANmark Category 6 solution.

Belgacom, which is both a major customer and an approved reseller of the LANmark solution, will install over 40000 LANmark-6 snap-in connectors in the 28 floors of each tower.

Nexans has previously supplied Category 5 cabling into the towers which from now on will be used mainly for telephony applications. The new Category 6 system is intended to upgrade the buildings to prepare them for the needs of the next decade.

One of the requirements of the new system was to provide maximum flexibility to allow simple and cost effective moves, adds, and changes during the infrastructure lifetime.  Nexans was able to meet the requirement using a three connector channel including an RJ45 consolidation point. The fully screened solution will also utilize Nexans unique LANmark-6 F2TP dual foil cable. This will not only provide enhanced EMC performance but was also considered a major installation benefit, the easy to install termination delivering substantial labor saving on a project of this scale.

The installation began in September 2002 and will continue in a phased process through to the end of 2004.

Emiel Vandeput, Nexans Product Manager, who was closely involved at the design stage said, �Nexans was awarded the project against fierce competition. Clearly our reputation for high performance and the quality of our product range helped the decision, but it was our commitment to provide ongoing support throughout the project that finally demonstrated we would provide the best value for money�.


Related Document
  Nexans equips Belgacom Towers in Brussels with LANmark Category 6 solution  (14.3kb)

Your Contact
Michel Gédéon
Financial Communication
Phone +33 (0)1 56 69 85 31
michel.gedeon@nexans.com
Céline Révillon
Press relations
Phone +33 (0)1 56 69 84 12
Celine.Revillon@nexans.com

About
About Nexans
Nexans is the worldwide leader in the cable industry. The Group brings an extensive range of advanced copper and optical fiber cable solutions to the infrastructure, industry and building markets. Nexans cables and cabling systems can be found in every area of people's lives, from telecommunications and energy networks, to aeronautics, aerospace, automobile, railways, building, petrochemical, medical applications, etc. The program is completed by superconducting materials and components, cryoflex transfer systems and special machinery for the cable industry. With an industrial presence in 28 countries and commercial activities in 65 countries, Nexans employs 17,150 people and had sales in 2002 of euros 4.3 billion. Nexans is listed on the Paris stock exchange. More information on http://www.nexans.com

Nexans © copyright 2001 - 2008   Legal Notice | Contact Us | Site Map