français Login Contact Us
Global expert in cables and cabling system

About Nexans

Products and Solutions

Customer Service

Finance

Work at Nexans

News and Press

Go

The Mont-Blanc Tunnel: Nexans supplies the safety cables

Send link to this page Your Nexans contact on this page
Nexans helps improve the safety of the Mont-Blanc Tunnel

Mont BlancParis, March 11, 2002 - Nexans, the worldwide leader in the cable industry, has supplied the safety cables installed in the Mont-Blanc Tunnel. These cables, which will carry the medium- and low-voltage power supplies in the tunnel, as well as voice, data and video surveillance transmissions, are fire-resistant and do not propagate smoke or noxious gases.

Nexans has supplied 90 km of aluminum cables for the medium-voltage supply and 300 km of copper cable for the low-voltage supply. The contract for the supply of the power cables for the entire tunnel was awarded by Gemmo Impianti de Vincenza and Cegelec Lyons. Gemmo is prime contractor for cable installation in the Italian section of the tunnel, while Cegelec is prime contractor for the French section.

For the Telecoms part, the Group has delivered 100 km of multimode optical fiber cables with 72, 36 and 6 fibers dedicated to telephony and 50 km of multimode 50/125 cables with 2, 12 and 24 fibers for data and video surveillance transmission. The cables have been installed by Gemmo-Cegelec.

The cables, like the special Nexans accessories, meet the most stringent international safety standards.

"We are particularly happy to be contributing towards the reconstruction of the Mont-Blanc Tunnel, stated Bruno Thomas, Nexans� Strategic Operations Director. Safety is one of Nexans' leading priorities, and our researchers work constantly on improving cable performance. Fires are in effect often aggravated by the propagation of flames and toxic fumes along the cables. Moreover, if the cables are not fire-resistant, the power is cut and the alarm systems no longer function.�


Note to Editors

Nexans has been developing research programs to HFFR (Halogen-Free Fire-Resistant) cables since 1988. This has resulted in high-performance cables based on new materials that do not propagate the flames and do not give off thick or toxic fumes.
These new materials are tested in the Nexans research laboratories where they undergo intensive testing to verify their resistance to fire and heat under extreme conditions. Some of Nexans security-system cables are, for example, capable of functioning for 3 hours at a temperature of 1000°C.


Related Document
  The Mont-Blanc Tunnel: Nexans supplies the safety cables  (49.8kb)

Your Contact
Angéline Afanoukoe
Press relations
Phone +33 (0)1 73 23 84 12
Angeline.afanoukoe@nexans.com
Michel Gédéon
Financial Communication
Phone +33 (0)1 73 23 85 31
michel.gedeon@nexans.com

About
About Nexans
Nexans is the worldwide leader in the cable industry. The Group brings an extensive range of advanced copper and optical fiber cable solutions to the infrastructure, industry and building markets. Nexans cables and systems can be found in every area of people's lives, from telecommunications and energy networks, to aeronautics, aerospace, automobile, railways, building, petrochemical, medical applications, etc. With an industrial presence in 28 countries and commercial activities in 65 countries, Nexans employs 17,500 people and had sales in 2001 of euros 4.8 billion. Nexans is listed on the Paris stock exchange. More information on www.nexans.com

Nexans © copyright 2001 - 2012   Legal Notice | Contact Us | Site Map