français Login Contact Us
Global expert in cables and cabling system

About Nexans

Products and Solutions

Customer Service

Finance

Work at Nexans

News and Press

Go

Nexans launches LANmark EVO Snap-in Connectors

Send link to this page Your Nexans contact on this page

LANmark EVOParis, March 22, 2005 - Nexans, the worldwide leader in the cable industry, announces the new generation of LANmark snap-in connectors: LANmark EVO. This new LANmark EVO series design has evolved from Nexans' well established LANmark-5 & LANmark-6 snap-in connectors, and provides enhanced termination benefits for installers, including a saving of at least 20 percent in installation time, and is complemented by a new Universal Comfort Tool.

New exclusive features.
Exclusive new features of the LANmark EVO connectors are: shorter length - for ease of use in shallow boxes; quicker installation - thanks to the new EMC (ElectroMagnetic Compatibility) cover; easier to use - new wire organiser simplifies and speeds up wire placement; reusability - the EVO series can be re-terminated using the new Universal Comfort Tool; increased versatility - the range includes versions designed specifically for use with stranded conductors providing enhanced reliability for consolidation points.

The new LANmark EVO series connector is fully compatible with snap-in format outlets and patchpanels and can be used in conjunction with existing connectors if required.

In recent years, termination time has had an increasingly dramatic effect on the total installed cost. So Nexans has developed the EVO series with installers in mind to save at least 20 percent of the installation time compared with competitors products.

The EVO series will be phased in to replace the existing connectors during March and April as current stocks are replenished.

A new Universal Comfort Tool
 Nexans has also launched a new Universal Comfort Tool that can be used with the new EVO series connectors as well as the current range and the LANmark-7 GG45. In addition to providing fast reliable termination, it also enables the wire organiser to be removed in the event of a wire map error and re-terminated.

For more information visit www.nexans.com/e-service


Related Document
  Nexans launches LANmark EVO Snap-in Connectors  (60.5kb)

Your Contact
Angéline Afanoukoe
Press relations
Phone +33 (0)1 73 23 84 12
Angeline.afanoukoe@nexans.com
Michel Gédéon
Financial Communication
Phone +33 (0)1 73 23 85 31
michel.gedeon@nexans.com

About
About Nexans
Nexans is the worldwide leader in the cable industry. The Group brings an extensive range of advanced copper and optical fiber cable solutions to the infrastructure, industry and building markets. Nexans cables and cabling systems can be found in every area of people's lives, from telecommunications and energy networks, to aeronautics, aerospace, automobile, railways, building, petrochemical, medical applications, etc. With an industrial presence in 29 countries and commercial activities in 65 countries, Nexans employs 20,000 people and had sales in 2004 of euros 4.9 billion. Nexans is listed on the Paris stock exchange. More information on www.nexans.com
http://www.nexans.com/

Nexans © copyright 2001 - 2012   Legal Notice | Contact Us | Site Map