Nexans cable solutions create innovative connections for the wind industry

Visit our booth 282 in the hall B6, from September 27-30, 2016

Visitors attending the WindEnergy Exhibition can see how Nexans offers a comprehensive range of innovative connection technologies for wind energy applications. A main highlight of the stand is 66 kV inter-array cables for the new generation of high voltage wind farms, together with high voltage submarine and land AC and HVDC cables as well as power accessories including the WINDLINK ® CONNECTION SYSTEM.

Nexans high voltage cables are ideally suited for the creation of high performance, low loss connections for future offshore and onshore wind applications. 66 kV submarine cables have been developed specifically for inter-array connections that interlink high voltage wind turbines and connecting them to transformer stations – they are currently being deployed in UK’s Blyth offshore wind demonstration project.

HVDC export cables

HVDC power links are now able to utilize Nexans state-of-the-art XLPE cables that are fully qualified to 320 kV, while type testing at 525 kV has just been successfully completed. At the same time Nexans has further extended the capability of its mass impregnated cables by qualifying its 600 kV design that provides a power transmission capacity of 1900 MW in a bipole configuration.

Nexans power accessories

Nexans is a leading supplier of low-voltage, medium-voltage and high-voltage accessories, as well as connection technology for power cables. At the exhibition Nexans is presenting its EUROMOLD® power accessories up to 72.5 kV along with the new GPH® mechanical connector for flexible aluminium conductors.
Also on show is the WINDLINK® CONNECTION SYSTEM that provides easy-to-assemble, safe and customer specific possibilities for the durable connection of low-voltage systems. Nexans also offers an extensive range of additional equipment and installation training programmes.

Request your WindEnergy 2016 Guest Pass 

Where to find us?

Booth 282 hall B6 (hall plans)

Hamburg Messe und Congress GmbH
Messeplatz 1
20357 Hamburg
Opening hours

Tuesday  September 27 9:00 a.m. - 6:00 p.m
Wednesday September 28 9:00 a.m. - 6:00 p.m
Thursday September 29 9:00 a.m. - 6:00 p.m
Friday September 30 9:00 a.m. - 6:00 p.m

Discover on Nexans booth

WINDLINK®: Complete, customized cable solutions and services for wind turbines worldwide


Complete cable solutions to develop your windfarm infrastructure


Event web site  

About Nexans

As a global leader in advanced cabling and connectivity solutions, Nexans brings energy to life through an extensive range of best-in-class products and innovative services. For over 120 years, innovation has been the company’s hallmark, enabling Nexans to drive a safer, smarter and more efficient future together with its customers. Today, the Nexans Group is committed to facilitating energy transition and supporting the exponential growth of data by empowering its customers in four main business areas: Building & Territories (including utilities, smart grids, e­mobility), High Voltage & Projects (covering offshore wind farms, submarine interconnections, land high voltage), Telecom & Data (covering data transmission, telecom networks, hyperscale data centers, LAN), and Industry & Solutions (including renewables, transportation, Oil & Gas, automation, and others). Corporate Social Responsibility is a guiding principle of Nexans’ business activities and internal practices. In 2013 Nexans became the first cable provider to create a Foundation supporting sustainable initiatives bringing access to energy to disadvantaged communities worldwide. The Group’s commitment to developing ethical, sustainable and high-quality cables drives its active involvement within several leading industry associations, including Europacable, The National Electrical Manufacturers Association (NEMA), International Cablemakers Federation (ICF) or CIGRE to mention a few. Nexans employs more than 26,000 people with industrial footprint in 34 countries and commercial activities worldwide. In 2017, the Group generated 6.4 billion euros in sales. Nexans is listed on Euronext Paris, compartment A. For more information, please consult: