English
Assistance & Tools
Login
Search Go
Search +
Global expert in cables and cabling system

About Nexans

Products and Solutions

Customer Service

Finance

Work at Nexans

News and Press


World’s first transmission voltage superconductor cable energised successfully in LIPA’s power grid

Send link to this page Your Nexans contact on this page
Nexans claims two world records: the longest cable with the highest voltage.

Paris, April 30, 2008 – The world’s longest and highest-voltage superconductor power transmission cable, developed and manufactured by Nexans, the worldwide leader in the cable industry, has just been energised successfully in a test installation for the Long Island Power Authority (LIPA), one of the largest municipal electric utilities in the US. The 600-metre, 138 kV, 574 MVA power link, comprising three high temperature superconductor (HTS) cable phases running in parallel, is the world’s first superconductor cable system installed in a live grid operating at transmission voltage.

The purpose of the LIPA project, which is supported by the US Department of Energy (DOE), is to provide a real-life demonstration of the application of an HTS cable within an electric utility’s operational transmission system. The cable system, including six outdoor terminations for connection to LIPA’s grid, was designed, manufactured and installed by Nexans. The cable utilizes HTS wire produced by American Superconductor Corporation (AMSC), which also is the prime contractor for the project. Air Liquide has provided the liquid nitrogen refrigeration system.

The superconductor cable has been installed in LIPA’s Holbrook transmission right-of-way. It is capable of transmitting up to 574 MVA of electricity – enough to power 300,000 homes. After an initial operational period and following performance and economic reviews, LIPA plans to retain the superconductor cable as a permanent part of its grid.

  LIPA cable installation PR

  

HTS cable benefits

HTS cables can carry three to five times more power than conventional copper cables of similar sizes. Thermally-independent, compact HTS cables can be installed into existing rights-of-way, helping to reduce the cost and environmental impact of future grid upgrades. With lower impedance than conventional technology, superconductor cables can be placed strategically in the power grid to draw flow away from overtaxed cables or overhead lines, reducing network congestion while providing an environmentally friendly solution. The DOE sees HTS cables as a core component of a modern electricity superhighway, one that is free of bottlenecks and can readily transmit power to customers from remote generating sites, such as wind farms.

LIPA cable PR            LIPA cable 3 PR

 


Related Information
Discover Nexans' offer for Power networks

Your Contact
Céline Révillon
Corporate Communications - Press relations
Phone + 33 1 56 69 84 12
celine.revillon@nexans.com
Michel Gédéon
Investor Relations
Phone +33 (0)1 56 69 85 31
Michel.Gedeon@nexans.com

About
About Nexans
With energy as the basis of its development, Nexans, the worldwide leader in the cable industry, offers an extensive range of cables and cabling systems. The Group is a global player in the infrastructure, industry, building and Local Area Network markets. Nexans addresses a series of market segments from energy, transport and telecom networks to shipbuilding, oil and gas, nuclear power, automotive, electronics, aeronautics, handling and automation. With an industrial presence in more than 30 countries and commercial activities worldwide, Nexans employs 22,800 people and had sales in 2007 of 7.4 billion euros. Nexans is listed on NYSE Euronext Paris, compartment A. More information on www.nexans.com



Related Information
Discover Nexans' offer for Power networks


Nexans © copyright 2001 - 2008   Legal Notice | Contact Us | Site Map