français Login Contact Us
Global expert in cables and cabling system

About Nexans

Products and Solutions

Customer Service

Finance

Work at Nexans

News and Press

Go

Nigeria – Niger: a sustainable link with aerial conductors AERO-Z®

Send link to this page Your Nexans contact on this page

AeroZ in West Africa

 

Installing an AERO-Z® cable for the link between Birnin-Kebbi and Niamey will allow Nexans to respond to an increased demand for electricity in the Niger River area because it will increase the power transmission capacity of this link by up to 75%.

It will replace the traditional saturated conductors that previously required energy to be produced locally in parallel by gas turbines and diesel generators that are very costly in terms of fuel.

Securing the power supply will allow vital facilities (water pumps, health centers, public lighting systems) to receive a continuous supply of electricity and almost stop the use of fossil fuels to operate auxiliary generators.

Nexans supplied and installed in an extremely short time a total length of 820 km of AERO-Z® conductors to the Nigerian Electricity Society (NIGELEC) for this project in 2008.
 


Related Information
Press release: Nexans and INEO install 264 km of high voltage overhead lines in record time to reinforce vital power link in West Africa

Nexans © copyright 2001 - 2012   Legal Notice | Contact Us | Site Map