français Login Contact Us
Global expert in cables and cabling system

About Nexans

Products and Solutions

Customer Service

Finance

Work at Nexans

News and Press

Go

Nexans launches new FLAMEX® brand name for high-performance cable solutions for the rolling stock industry

Send link to this page Your Nexans contact on this page

Paris, May 25, 2009 – Nexans, the worldwide leader in the cable industry, has launched FLAMEX® as the new brand name for its range of cables for the rolling stock industry. The FLAMEX range covers all the product families from power to control cables, data-bus, jumpers, optical fiber and roof HV pantograph cables.

 

A complete range of advanced cables

FLAMEX® cables are rated for voltages of 300 V up to 45 kV AC. Their cross sections range are from 0.25mm2 up to 500mm2. Operating temperature ranges depend on the required life time: either 120° C/20,000h for rubber insulated cable or 180° C/20,000h for silicon insulated materials. FLAMEX® cables are suitable when standard or highly flexible cables (such as jumper cables) are needed and can be screened or unscreened.

FLAMEX® control cables consist of thin-wall low voltage cables, which are used to provide energy and low frequency control for communications, public address, automatic doors, and lighting; databus cables, which support the main data standard protocols like UIC, MVB, WTB, CAN and Ethernet ; coaxial cables, which are used for multimedia and GSM radio transmissions for rail traffic management and train control; and optical fibre, which is used for the safe transmission in view of EMC or high speed rate.

 

Flamex fire resistance test photoSafety: compliance with all international standards

FLAMEX® cables have been designed with safety in mind. They conform to all international standards, such as European (EN), French (NFF), German (VDE), British (BS) and International standards (IEC). The cables are also environmental friendly as strictly Halogen free.

FLAMEX® cables resist the propagation of fire and produce low smoke emissions that are, by the way, not corrosive and low in toxicity. FLAMEX® also has excellent tensile strength and provides excellent mechanical resistance to abrasion, cutting forces and chemical agents. These characteristics are especially necessary for the rolling stock industry, because in the event of a fire they will help secure the power supply for doors, ventilation, and the loudspeaker, as well as any data transmission.

Overall the range is flexible, easy to strip and install, allows users to make weight and space savings and thanks to its outstanding quality level has a long service life.


Related Information
Discover Nexans' offer for Rolling stock

Related Document
  Nexans launches new FLAMEX® brand name for high-performance cable solutions for the rolling stock industry  (31.5kb)
  Discover FLAMEX® Range  (1082.0kb)

Your Contact
Angéline Afanoukoe
Corporate Communications - Press relations
Phone + 33 1 73 23 84 12
Angeline.afanoukoe@nexans.com
Michel Gédéon
Investor Relations
Phone +33 (0)1 73 23 85 31
Michel.Gedeon@nexans.com

About
About Nexans
With energy as the basis of its development, Nexans, the worldwide leader in the cable industry, offers an extensive range of cables and cabling systems. The Group is a global player in the infrastructure, industry, building and Local Area Network markets. Nexans addresses a series of market segments from energy, transport and telecom networks to shipbuilding, oil and gas, nuclear power, automotive, electronics, aeronautics, handling and automation. With an industrial presence in 39 countries and commercial activities worldwide, Nexans employs 23,500 people and had sales in 2008 of 6.8 billion euros. Nexans is listed on NYSE Euronext Paris, compartment A. More information on www.nexans.com



Related Document
  Nexans launches new FLAMEX® brand name for high-performance cable solutions for the rolling stock industry  (31.5kb)
  Discover FLAMEX® Range  (1082.0kb)


Related Information
Discover Nexans' offer for Rolling stock


Nexans © copyright 2001 - 2012   Legal Notice | Contact Us | Site Map