français Login Contact Us
Global expert in cables and cabling system

About Nexans

Products and Solutions

Customer Service

Finance

Work at Nexans

News and Press

Go

Nexans launches ICEFLEX®

Send link to this page Your Nexans contact on this page
This is the first halogen free marine & offshore full range cable to resist ultra-cold Arctic temperatures down to – 50°

Paris, April 9, 2009 – Nexans, the worldwide leader in the cable industry, has launched ICEFLEX®, the world’s first marine and offshore full range cable qualified for extremely low temperatures such as those experienced in the Arctic.  This range of cable, which is intended for use in a wide variety of shipboard and offshore/onshore applications, remains highly flexible at temperatures as low as –50°C, while ensuring advanced fire performance.

Normally cables with conventional insulation become stiff and brittle in intense cold, which can be problematic especially in places such as the Arctic. To address this problem, Nexans has developed ICEFLEX®, featuring special materials that enables the cable to stay flexible at low temperatures. This makes it ideal to support the growing number of oil & gas projects taking place in the Arctic.

ICEFLEX® adheres to all current environmental and safety standards, and the cable is able to meet the challenge of severe cold or ice storms. It operates reliably in icy, snowy conditions under a variety of technical applications, and can survive in exposed conditions onboard, topside or in frozen ground or permafrost. The cable also easily adapts to abrupt temperature variations such as those taking place during Spring and Autumn. 

 

Iceflex cable illustrationICEFLEX® comes in two versions

ICEFLEX® is available in two versions – Halogen-Free Flame & Fire Retardant (HFFR) and halogenated versions. The cables do not propagate smoke, fire, or generate toxic gases and maintain power supplies for vital safety equipment, such as emergency lighting, fire pumps, or communications circuits.

Furthermore, both are widely specified in shipbuilding and the oil & gas industry, and are fully certified by Lloyds Register. ICEFLEX® is also mechanically tough, which makes it resistant to atmospheric agents (ozone, UV, heat, etc.), and deterioration from oil, chemicals, heat and extreme weather. 

ICEFLEX® also has a high impact-resistance, which means it won’t crack or break when subjected to sustained or violent physical shocks, such as vibration or operational stress. Salvatore Di Giorgio, Nexans Global Segment Manager for Shipbuilding and Offshore Top Side market, says: “The ability to withstand these environmental constraints is a major technical achievement, which will make it easier to safely develop Oil & Gas fields, shipping routes and processing plants in the High Arctic.” 


Related Information
Discover Nexans' offer for Shipbuilding & Navy
Discover Nexans' offer for Oil, gas and petrochemical

Related Document
  Nexans launches ICEFLEX®  (37.8kb)

Your Contact
Angéline Afanoukoe
Press relations
Phone + 33 1 73 23 84 12
Angeline.afanoukoe@nexans.com
Michel Gédéon
Investor Relations
Phone +33 (0)1 73 23 85 31
Michel.Gedeon@nexans.com

About
About Nexans
With energy as the basis of its development, Nexans, the worldwide leader in the cable industry, offers an extensive range of cables and cabling systems. The Group is a global player in the infrastructure, industry, building and Local Area Network markets. Nexans addresses a series of market segments from energy, transport and telecom networks to shipbuilding, oil and gas, nuclear power, automotive, electronics, aeronautics, handling and automation. With an industrial presence in 39 countries and commercial activities worldwide, Nexans employs 23,500 people and had sales in 2008 of 6.8 billion euros. Nexans is listed on NYSE Euronext Paris, compartment A. More information on www.nexans.com



Related Document
  Nexans launches ICEFLEX®  (37.8kb)


Related Information
Discover Nexans' offer for Shipbuilding & Navy
Discover Nexans' offer for Oil, gas and petrochemical


Nexans © copyright 2001 - 2012   Legal Notice | Contact Us | Site Map